Object Data Over CAN Users Guide

Table of Contents

Overview

This lab exercise demonstrates the ability of AWR1642 TI-mmWave sensor to estimate and track the position (in the azimuthal plane), the velocity of objects and sends the detections over CAN interface.

The mmWave sensor AWR1642BOOST ES 2.0 is used for lab demonstration.

Required Hardware

Getting Started

Flash Lab Binaries on AWR1642BOOST

* XDS110 Class Application/User UART (COM<sub>UART</sub>): Used for passing configuration data and firmware to the EVM
* XDS110 Class Auxiliary Data Port (COM<sub>AUX</sub>): Used to send processed radar data output

Run the Lab

CANBUS circuit:

Pin assignment on the PCAN-USBFD:

Note: The AWR1642BOOST has only 1 CANFD so there is no need to use the CANBUS circuit. The CAN lines can be connected directly to PCAN-USBFD. If there are multiple AWR1642BOOST then use the CANBUS circuit.