AWRL1432 KTO Users Guide
Table of Contents
Device Compatibility
⚠️ This lab is currently only compatible with the AWRL1432.
Overview
This lab demonstrates the use of TI AWRL1432 mmWave sensors for a kick-to-open system to allow for hands-free access to the trunk of a vehicle. As low power consumption is a key pain point for this use case, this lab implements two modes: “Low Power Mode” and “Gesture Mode.” While in “Low Power Mode,” the sensor consumes minimal power while searching for a presence to trigger a switch to “Gesture Mode.” In “Gesture Mode” the device uses range, velocity, and angle data to enable detection and classification of a kick gesture. This lab outputs what mode the sensor is in, the device’s power consumption, and whether or not a kick has been detected.
Quickstart
Prerequisites
Prerequisite 1 - Run mmWave Lab
Before continuing with this lab, users should run the mmw Demo for the AWRL1432 to gain familiarity with the sensor’s capabilities and the tools used in the Radar Toolbox.
Prerequisite 2 - XDS Firmware
If using an AWRL1432BOOST EVM, the latest XDS110 firmware is required. The XDS110 Firmware runs on the microcontroller onboard the AWRL1432BOOST, which provides the JTAG Emulation and serial port communication over the XDS110 USB port. Packet loss has been observed on the serial port (COM ports) with some versions of the XDS110 firmware which can cause the demo to fail.
The latest XDS110 firmware is installed with the latest version of Code Composer Studio. CCS version 12.2 or later required.
Prerequisite 3 - PC CPU and GPU Resources
The Kick-to-Open Visualizer requires sufficient GPU and CPU resources to process the incoming UART data every frame and run the demo smoothly. Users with insufficient PC resources may notice occasional visualizer lag or missed frames in the log file. The demo should still run on most PCs regardless of hardware resources, but performance might vary.
Requirements
Hardware Requirements
| Item | Details |
|---|---|
| AWRL1432 Evaluation Board | AWRL1432 Evaluation Board |
| Computer | PC with Windows 10. If a laptop is used, please use the ‘High Performance’ power plan in Windows. |
| Micro USB Cable | Due to the high mounting height of the EVM, a 15ft+ cable or USB extension cable is recommended. |
Software Requirements
| Tool | Version | Download Link |
|---|---|---|
| TI mmWave L SDK | 5.3.0.2 | TI mmWave SDK 5.3.0.2 |
| Uniflash | Latest | Uniflash tool is used for flashing TI mmWave Radar devices. Download offline tool or use the Cloud version |
| Code Composer Studio | CCS 12.2 or later | Code Composer Studio |
1. Configure the EVM for Flashing Mode
Follow the instructions for Hardware Setup of Flashing Mode
2. Flash the EVM using Uniflash
Flash the binary listed below using UniFlash. Follow the instructions for using UniFlash
- gesture_recognition_demo.Debug.appimage
The flashable binary can be found at: <RADAR_TOOLBOX_INSTALL_DIR>\source\ti\examples\AWRL1432_KTO\prebuilt_binaries\
3. Configure the EVM for Functional Mode
Follow the instructions for Hardware Setup of of Functional Mode
4. Run the Lab
1. Open Visualizer
Navigate to <RADAR_TOOLBOX_INSTALL_DIR>\tools\visualizers\Kick_To_Open_Visualizer. The visualizer software may be run from Python 3.7.3 or as a standalone executable. In general, running the visualizer from the Python source runs faster and results in fewer errors over long periods of time. If running Python directly from source, run the setUpEnvironment.bat script first to ensure all the correct packages and versions are installed. Then run the visualizer either directly from source with python gui_main.py, or as an executable by running the mmWave_Kick_To_Open_Visualizer.exe
2. Reset the AWRL1432BOOST EVM by pressing the RESET_SW button
3. Select the arrowed options as shown in the below graphic.
Set the Device to AWRL1432 as indicated by arrow 1
Set CLI COM to the appropriate COM port as indicated by arrow 2. If the AWRL1432BOOST EVM is plugged in when the visualizer is opened, then the COM ports filled in automatically. If they do not appear, check the Device Manager on Windows for the XDS110 Class Application/User UART port, and use this port number in the visualizer.
Select the AWRL1432 Kick-to-Open demo as indicated by arrow 3.
Press the “Connect” button as indicated by arrow 4
Press the “Select Configuration” button as indicated by arrow 5. Navigate to
<RADAR_TOOLBOX_INSTALL_DIR>\radar_toolbox\source\ti\examples\AWRL1432_KTO\chirp_configsand selectgesture_recognition.cfg.Press the “Start and Send Configuration” button as indicated by arrow 6.
4. Running the Demo
This utilizes two “modes:” a gesture recognition mode and a low power presence detection mode. While in presence detection mode, the device operates on minimal power searching for a person within roughly 2m. Once a person is detected, the device switches to gesture recognition mode in which the following features are supported:
- Detection/Classification of one gestures (at a range of 1m): Kick.
Perform the above gesture while standing at a distance of 1m from the radar sensor. The detected gestures will be displayed in the ‘Gesture Status’ box of the visualizer.
Once a person enters the presence detection range (roughly 3m), the device will switch from “Low Power Mode” to “Gesture Recognition Mode,” in which the frame rate is much higher. The device is now ready to recognize kick gestures. In the visualizer, the “Presence Threshold” plot will disappear and be replaced by the “Doppler Average” plot which shows the extracted feature being streamed from the device.
After a person exits and there is no presence found for about 10 seconds, the device will switch back to “Low Power Mode,” where it will once again wait for a presence to be detected.
This concludes the Quickstart section.
Developer’s Guide
Import Lab Project to CCS
To import the source code into your CCS workspace, a CCS project is provided in the lab at the path given below.
Start CCS and configure workspace as desired.
Import the project specified below to CCS.
<RADAR_TOOLBOX_INSTALL_DIR>\source\ti\examples\AWRL1432_KTO\src\xwrl1432\AWRL1432_KTO.projectspecVerify that the import occurred without error by checking that
AWRL1432_ktoshows up in the project explorer
🛑 Error during Import to IDE
If an error occurs, check that the software dependencies listed above have been installed. Errors will occur if necessary files are not installed in the correct location for importing.
Build the Lab
- Select the AWRL1432_kto in Project Explorer so that it is highlighted. Right click on the project and select Rebuild Project. The project will then build.
- On successful build, the following should appear:
- In
<PROJECT_WORKSPACE_DIR>\AWRL1432_kto→Debug- AWRL1432_kto.out (this is the binary used for CCS debug mode)
- gesture_recognition_demo.Debug.appimage (this is the flashable binary used for deployment mode)
- In
Selecting Rebuild instead of Build ensures that the project is always re-compiled. This is especially important in case the previous build failed with errors.
🛑 Build Fails with Errors
If the build fails with errors, please ensure that all the software requirements are installed as listed above and in the mmWave SDK release notes.
Execute the Lab
There are two ways to execute the compiled code on the EVM:
- Deployment mode: the EVM boots from flash and starts running the bin image at power-up
- Using Uniflash, flash the gesture_recognition_demo.Debug.appimage found at
<PROJECT_WORKSPACE_DIR>\AWRL1432_gesture_recognition\Debug - The same procedure for flashing can be used as detailed in the Flash the EVM section.
- Using Uniflash, flash the gesture_recognition_demo.Debug.appimage found at
- Debug mode: This mode is used for downloading and running the executable from CCS. This mode enables JTAG connection with CCS while the lab is running and is useful during development and debugging.
- Follow the CCS Debug Mode Guide ⚠️ JTAG connection is lost when power management framework is enabled in SDK. In order to do this, then lowPowerCfg must be set to 0 in cfg file; however, this will prevent the device from switching between presence detection mode and gesture recognition mode.
UART Output Data Format
This demo outputs data using a TLV (type-length-value) encoding scheme with little endian byte order. For every frame, a packet is sent consisting of a fixed sized Frame Header and then a variable number of TLVs depending on what was detected in that scene. The TLVs for this demo include the extracted features used for the neural network inference as well as the detected gesture for that frame.
Frame Header
Length: 40 Bytes
A Frame Header is sent at the start of each packet. Use the Magic Word to find the start of each packet.
| Value | Type | Bytes | Comments |
|---|---|---|---|
| Magic Word | uint64_t | 8 | syncPattern in hex is: ‘02 01 04 03 06 05 08 07’ |
| Version | uint32_t | 4 | Software Version |
| Total Packet Length | uint32_t | 4 | In bytes, including header |
| Platform | uint32_t | 4 | A6843 |
| Frame Number | uint32_t | 4 | Frame Number |
| Time [in CPU Cycles] | uint32_t | 4 | Message create time in cycles |
| Num Detected Obj | uint32_t | 4 | Number of detected points in this frame |
| Num TLVs | uint32_t | 4 | Number of TLVs in this frame |
| Subframe Number | uint32_t | 4 | Sub-Frame number |
TLV Header
Length: 8 Bytes
A TLV Header is sent at the start of each TLV. Following the header is the the TLV-type specific payload.
| Value | Type | Bytes | Comments |
|---|---|---|---|
| Type | uint32_t | 4 | TLV Type |
| Length [number of bytes] | uint32_t | 4 | In bytes |
TLVs
Gesture Features TLV
Size: sizeof (tlvHeaderStruct) + 56 Bytes
The Gesture Features TLV consists of an array of extracted features some of which are used as input to the neural network. Each extracted feature is defined as given below.
| Value | Type | Bytes | Comment |
|---|---|---|---|
| rangeAvg | float | 4 | range average feature from RD heatmap |
| dopplerAvg | float | 4 | doppler average feature from RD heatmap |
| dopplerAvgPos | float | 4 | doppler positive average feature from RD heatmap |
| dopplerAvgNeg | float | 4 | doppler negative average feature from RD heatmap |
| numPoints | float | 4 | number of detected points above a threshold in RD heatmap |
| azimWtMean | float | 4 | azimuth weighted mean from elevation-azimuth heatmap |
| elevWtMean | float | 4 | elevation weighted mean from elevation-azimuth heatmap |
| azimWtDisp | float | 4 | azimuth weighted displacement from elevation-azimuth heatmap |
| elevWtDisp | float | 4 | elevation weighted displacement from |
| dopAzimCorr | float | 4 | doppler azimuth correlation across n frames |
| dopElevCorr | float | 4 | doppler elevation correlation across n frames |
| dopPosNegCorr | float | 4 | doppler positive negative correlation across n frames |
| dopPosElevCorr | float | 4 | doppler positive elevation correlation across n frames |
| dopPosAzimCorr | float | 4 | doppler positive azimuth correlation across n frames |
Gesture Classifier Output TLV
Size: sizeof (tlvHeaderStruct) + sizeof(uint8_t)
The Gesture Classifier Output TLV consists of a single uint8_t indicating the detected gesture.
| Gesture | Identifier |
|---|---|
| No Gesture | 0 |
| Kick | 1 |
Presence Detection Output TLV
Type: MMWDEMO_OUTPUT_EXT_PRESENCE_OUTPUT = 352
Size: sizeof (tlvHeaderStruct) + sizeof(uint8_t)
The Presence Detection Output TLV consists of a single uint8_t indicating the detected presence. This TLV is not sent out in gesture-only mode.
| Status | Value |
|---|---|
| No Presence Detected | 0 |
| Presence Detected | 1 |
Presence Detection Threshold TLV
Type: MMWDEMO_OUTPUT_EXT_PRESENCE_DETECT_THRESHOLD = 353
Size: sizeof (tlvHeaderStruct) + sizeof(uint32_t)
This TLV contains the sum of magnitude across 2nd Doppler bin from range ‘x’ to range bin ‘y’ in the presence mode. The value in this TLV This TLV is not sent out in gesture-only mode.
Stats TLV
Type: MMWDEMO_OUTPUT_EXT_MSG_STATS = 354
Size: sizeof (tlvHeaderStruct) + sizeof(MmwDemo_output_message_stats)
| Value | Type | Bytes | Comment |
|---|---|---|---|
| interFrameProcessingTime | uint32_t | 4 | Interframe processing time in usec |
| transmitOutputTime | uint32_t | 4 | Transmission data transmit time in usec |
| powerMeasured[4] | uint16_t[4] | 8 | Power at 1.8V, 3.3V, 1.2V and 1.2V RF rails (1LSB = 100 uW) |
| tempReading[4] | int16_t[4] | 8 | Temperature: Rx, Tx, PM, DIG. (°C), 1LSB = 1°C |
Neural Network
This demo utilizes a neural network model which runs on the ARM core making predictions based on extracted features. A sliding window buffer of features, extracted from the data across a number of frames, is used as input to the neural network. The model outputs a set of probabilities, each represents the probability that the input data belongs to a specific gesture.
Features
The model is trained on following extracted features.
| Extracted Feature | Description |
|---|---|
| Doppler Average | Weighted average of the Doppler across the heatmap |
| Elevation Weighted Mean | Select the N cells of the heat-map with the highest magnitude and for each cell compute the elevation bin (via angle-FFT). The average elevation is the weighted average of all these elevation bin indices. |
| Azimuth Weighted Mean | Select the N cells of the heat-map with the highest magnitude and for each cell compute the azimuth bin (via angle-FFT). The average azimuth is the weighted average of all these azimuth bin indices. |
| Number of detected points | Number of cells in the heatmap that have a magnitude above a certain threshold |
| Range Average | Weighted average of the range across the heatmap. |
Retraining
Users may wish to retrain the neural network model for various reasons such as adding or removing certain gestures. The full process for retraining and deploying a model is not provided in this guide; however, one can save the extracted features which are output over UART and use the saved features as training data in the model building process.