3D People Tracking User Guide

Table of Contents

⚠️ Device Compatibility

This lab is only compatible with the xWRx843 family (IWR6843/AWR6843/IWR1843/AWR1843). For the people tracking offering on the IWLR6432, see the IWRL6432 People Tracking page

Overview

This lab demonstrates the use of TI mmWave sensors to track and count moving and stationary people using the IWR6843ISK, IWR6843ISK-ODS or IWR6843AOPEVM sensor module positioned in side-mount configuration (e.g. on a wall). Detection and tracking algorithms run onboard the IWR6843 mmWave sensor and are used to localize people and track their movement.

In this demonstration, localization and tracking is performed upon any moving object in the scene and the people or objects will continue being tracked until they leave the scene. This will even continue tracking people as they sit or lie down and remain stationary.

With the 3D people tracking software running on the IWR6843 chip, the mmWave sensor module outputs a data stream consisting of 3 dimensional point cloud information and a list of tracked objects which can be visualized using the PC based visualizer included in the toolbox.

This user guide covers the procedures to Flash, Run, and Compile the 3D People Tracking demo. For details regarding the demo software algorithms and implementation, please refer to the following documents available in the People Tracking Lab docs directory.


⚠️ IWR6843 ES2.0 Only

This lab is only compatible with ES2.0 version of IWR6843.

ISK or ODS

If using an IWR6843ISK or IWR6843ISKODS, check the device version on your IWR6843 using the on-chip device markings as shown below

  1. If line 4 reads 678A, you have an ES2 device. In this case, this lab is compatible with your EVM.
  2. If line 4 reads 60 GHZi, you have an older ES1 device. In this case, the lab is NOT compatible with your EVM. ES2 IWR6843ISK/IWR6843ISK-ODS boards are orderable from the EVM link above.

On AOP, the EVM must be Rev F or later. This can be distinguished by the shape of the EVM if it is as shown above.

AOP

The IWR6843AoP version of this lab is only compatible with ES2.0 silicon and the corresponding EVM. Please ensure your EVM is the same as in the below image.


Quickstart

Prerequisites

Prerequisite 1 - Run Out of Box Demo

Before continuing with this lab, users should first run the out of box demo for the EVM. This will enable users to gain familiarity with the sensor’s capabilities as well as the various tools used across all labs in the Radar Toolbox.


Prerequisite 2 - XDS Firmware

If using MMWAVEICBOOST, the latest XDS110 firmware is required. The XDS110 Firmware runs on the microcontroler onboard the MMWAVEICBOOST Carrier Card, which provides the JTAG Emulation and serial port communication over the XDS110 USB port. We have observed packet loss on the serial port (COM ports) with some versions of the XDS110 firmware which can cause the demo to fail.

The latest XDS110 firmware is installed with the latest version of Code Composer Studio. CCS version 10.1 or later required.


Prerequisite 3 - PC CPU and GPU Resources

The visualizer requires sufficient GPU and CPU resources to process the incoming UART data every frame and run the demo smoothly. Users with insufficent PC resources may notice occasional visualizer lag or missed frames in the log file. The demo should still run on most PCs regardless of hardware resources, but performance might be slightly different.


1. Hardware and Software Requirements

Hardware

Item Details
Device IWR6843ISK or IWR6843ISK-ODS or IWR6843AOP or IWR6843L optionally with mmWave Carrier Board.
Mounting Hardware The EVM needs to be mounted at a height of ~1.5-2.5m with a slight downtilt. An adjustable clamp style smartphone adapter mount for tripods and a 60-75” tripod can be used to clamp and elevate the EVM. This is only an example solution for mounting; other methods can be used so far as setup specifications are met.
Computer PC with Windows 7 or 10. If a laptop is used, please use the ‘High Performance’ power plan in Windows.
Micro USB Cable Due to the high mounting height of the EVM, an 8ft+ cable or USB extension cable is recommended.
Power Supply 5V, >3.0A with 2.1-mm barrel jack (center positive). The power supply can be wall adapter style or a battery pack with a USB to barrel jack cable.

Software

Tool Version Download Link
TI mmWave SDK 3.5.x.x Link to Latest mmWave SDK. To access a previous version of the mmWave SDK scroll to the bottom of the table and click the link under “MMWAVE-SDK previous release”. Repeat to continue stepping back to previous versions.
Uniflash Latest Uniflash tool is used for flashing TI mmWave Radar devices. Download offline tool or use the Cloud version
Silicon Labs CP210x USB to UART Bridge VCP Drivers
(only required in standalone mode)
Latest Latest SiLabs Driver

2. Flash the EVM

  1. Set the device in flashing mode:

    a. If using the EVM standalone module, follow the instructions for setting Modular EVM to flashing mode

    b. If using the EVM with ICBOOST, follow the instructions for Hardware Setup of ICB for Flashing Mode

  2. Follow the instruction to Flash the mmWave Device

    Image Location
    Meta Image 1/RadarSS <toolbox_install_dir>\source\ti\examples\people_tracking\3D_people_tracking\prebuilt_binaries\3D_people_track_68xx_demo.bin

3. Physical Setup

  1. Setup the device for functional mode

    a. If using ISK standalone, follow the instructions for setting Modular EVM to functional mode

    b. If using the ICBOOST, follow the instructions for Hardware Setup of ICB for Functional Mode

  2. For best results, the EVM should be positioned high enough to be above the top of tracked objects and with a slight down tilt. The aim is to position the EVM so that the antenna beam can encompass the area of interest. If the down tilt is too severe, noise from ground clutter would increase and the effective sensing area would decrease. If there is no down tilt, tracking performance would be worse for cases in which one person is in line with and shielded by another person.

📝 NOTE: More Information
For a more detailed discussion of the optimal placement and angle of the radar device, refer to TI’s Application Brief on the topic - Best Practices for Placement and Angle of mmWave Radar Devices

Setup Requirements:

Setup using suggested tripod and smartphone clamp mount:

  1. Screw on clamp mount to tripod
  2. Clamp EVM across its width below power barrel jack to attach EVM
  3. Adjust tripod head for ~10 degree down tilt (Tip: Bubble or level smartphone apps can be used to measure down tilt)
  4. Plug in micro-usb and power supply to EVM
  5. Extend tripod so that the EVM is elevated 1.5-2.5m from the ground
  6. Position EVM and tripod assembly in desired location of room. The EVM should be positioned so that the 120 degree FOV of the EVM antenna encompasses the area of interest and points to the region in which people are expected to enter the space.

4. Run the Lab

To run the lab, launch and configure the visualizer which displays the detection and tracked object data received via UART. See the instructions in the visualizer folder

Please ensure you use the default chirp for your device:

EVM Configuration File(s)
IWR6843ISK ISK_6m_default.cfg or ISK_14m_extended.cfg
IWR6843ISKODS ODS_6m_default.cfg
IWR6843AOPEVM AOP_6m_default.cfg
IWR6843LEVM ISK_6m_default.cfg or ISK_14m_extended.cfg

📝 Note - If using the IWR6843LEVM, maximum range may be limited compared
to the IWR6843ISKEVM. However, both EVMs should reach 14m range for
indoor applications.

⚠️ Warning
Device must be restarted before sending a new configuration.

Typical Chirp Parameters

Chirp Parameter (Units) Value
Start Frequency (GHz) 60.6
Slope (MHz/us) 54.725
Samples per chirp 96
Chirps per frame 288
Frame duration (ms) 50
Sampling rate (Msps) 2.950
Bandwidth (MHz) 2249
Range resolution (m) 0.084
Max Unambiguous Range (m) 7.2
Max Radial Velocity (m/s) 8.38
Velocity resolution (m/s) 0.17
Azimuth resolution (deg) 14.5
Elevation resolution (deg) 58
Number of Rx 4
Number of Tx 3

Developer’s Guide

Build the Firmware from Source Code

1. Software Requirements

Tool Version Download Link
TI mmWave SDK 3.5.x.x Link to Latest mmWave SDK. To access a previous version of the mmWave SDK scroll to the bottom of the table and click the link under “MMWAVE-SDK previous release”. Repeat to continue stepping back to previous versions.
Code Composer Studio Latest Code Composer Studio

2. Import Lab Project

For the People Tracking lab, there are two projects, the DSS for the C674x DSP core and the MSS project for the R4F core, that need to be imported to CCS and compiled to generate firmware for the xWR6843.

⚠️ WARNING
When importing projects to a workspace, a copy is created in the workspace. All modifications will only be implemented for the workspace copy. The original project downloaded from the Toolbox is not touched.

  1. Start CCS and setup workspace as desired.
  2. Import the project(s) specified below to CCS from the src/ folder. See instructions for importing here.
    • 3D_people_track_68xx_dss
    • 3D_people_track_68xx_mss
  3. Verify that the import occurred without error: in CCS Project Explorer, both 3D_ppltrack_68xx_mss and 3D_ppltrack_68xx_dss should appear.

3. Build the Lab

The DSS project must be built before the MSS project.

  1. Select the 3D_people_track_68xx_dss so it is highlighted. Right click on the project and select Rebuild Project. The DSS project will build.
  2. Select the 3D_people_track_68xx_mss so it is highlighted. Right click on the project and select Rebuild Project. The MSS project will build, the the lab binary will be constructed automatically.
  3. On successful build, the following should appear:
    • In 3D_people_track_68xx_dss → Debug, 3D_people_track_68xx_dss.xe674 (this is the C67x binary used for CCS debug mode)
    • In 3D_people_track_68xx_mss → Debug, 3D_people_track_68xx_mss.xer4f (this is the Cortex R4F binary used for CCS debug mode) and 3D_people_track_68xx_demo.bin (this is the flashable binary used for deployment mode)

⚠️ WARNING - Selecting Rebuild
Selecting Rebuild instead of Build ensures that the project is always re-compiled. This is especially important in case the previous build failed with errors.


⚠️ WARNING - Build Fails with Errors
If the build fails with errors, please ensure that all the software requirements are installed as listed above and in the mmWave SDK release notes.


📝 NOTE - Existing Binaries
As mentioned in the Quickstart section, pre-built binary files, both debug and deployment binaries are provided in the pre-compiled directory of the lab.


4. Execute the Lab

There are two ways to execute the compiled code on the EVM:

After executing the lab using either method, the lab can be visualized following the steps in Run the Lab section under Quickstart.

Customization

For detailed description of the configuration parameters and recommendations related to tuning the parameters, please refer to the following documents available in the People Tracking Lab docs directory.

Modifying the Configuration Files for the Physical Setup

The configuration files included a set of commands which are used to specify the scene boundaries (i.e. area of interest) in relation to the sensor position and may need to be modified accordingly. These commands and their respective parameters are listed below.

Modifying the Configuration File for Performance

The configuration file contains a number of commands that can be modified to optimize device performance. The commands inside the configuration file for the people tracking labs are described in detail in three locations, in the mmWave SDK User’s Guide (found at C:\ti$MMWAVE_SDK_DIRECTORY$\docs), the 3D People Tracking Demo Detection Layer Tuning Guide and the 3D People Tracking Demo Tracker Layer Tuning Guide.


📝 NOTE - Typical Configuration Challenges
Typical problems and solutions for first-time users working with the mmWave devices are documented in Section 4 of the 3D People Tracking Demo Detection Layer Tuning Guide and in Section 4 of the 3D People Tracking Demo Tracker Layer Tuning Guide. These scenarios include tuning the range and velocity, reducing noise, discerning true tracks from ghost tracks and more.

UART Output Data Format

The demo outputs the point cloud and tracking information using a TLV(type-length-value) encoding scheme with little endian byte order. For every frame, a packet is sent consisting of a fixed sized Frame Header and then a variable number of TLVs depending on what was detected in that scene. The TLVs can be of types representing the 3D point cloud, target list object, and associated points.


Frame Header

Length: 40 Bytes
A Frame Header is sent at the start of each packet. Use the Magic Word to find the start of each packet.

Value Type Bytes Comments
Magic Word uint64_t 8 syncPattern in hex is: ‘02 01 04 03 06 05 08 07’
Version unint32_t 4 Software Version
Total Packet Length unint32_t 4 In bytes, including header
Platform unint32_t 4 A6843
Frame Number unint32_t 4 Frame Number
Time [in CPU Cycles] unint32_t 4 Message create time in cycles
Num Detected Obj unint32_t 4 Number of detected points in this frame
Num TLVs unint32_t 4 Number of TLVs in this frame
Subframe Number unint32_t 4 Sub-Frame number

TLV Header

Length: 8 Bytes
A TLV Header is sent at the start of each TLV. Following the header, is the the TLV-type specific payload. The TLVs can be of type POINT CLOUD, TARGET LIST, TARGET INDEX, PRESENCE INDICATION or TARGET HEIGHT.

Value Type Bytes Comments
Type unint32_t 4 TLV Type: 1020 = Point Cloud, 1010 = Target object list, 1011 = Target Index, 1012 = Target Height, 1021 = Presence Indication
Length [number of bytes] unint32_t 4 In bytes

TLVs

Compressed Point Cloud TLV

Size: sizeof (tlvHeaderStruct) + sizeof(pointUnit) + sizeof (pointStruct) x numberOfPoints

Each Point Cloud TLV consists of an array of points. Each point is defined in 8 bytes. The pointUnit struct is used to uncompress each point to five floats (20 bytes).

Value Type Bytes Comments
elevationUnit float 4 Multiply each point by this value - used for compression
azimuthUnit float 4 Multiply each point by this value - used for compression
dopplerUnit float 4 Multiply each point by this value - used for compression
rangeUnit float 4 Multiply each point by this value - used for compression
snrUnit float 4 Multiply each point by this value - used for compression
Value Type Bytes Comments
elevation int8_t 1 Elevation in radians
azimuth int8_t 1 Azimuth, in radians
doppler int16_t 2 Doppler, in m/s
range int16_t 2 Range, in meters
snr int16_t 2 SNR, ratio

Target List TLV

Size: sizeof (tlvHeaderStruct) + sizeof (trackerProc_Target) x numberOfTargets The Target List TLV consists of an array of targets. Each target object is defined as given below.

Value Type Bytes Comments
tid uint32 4 Track ID
posX float 4 Target position in X dimension, meters
posY float 4 Target position in Y dimension, meters
posZ float 4 Target position in Z dimension, meters
velX float 4 Target velocity in X dimension, meters/s
velY float 4 Target velocity in Y dimension, meters/s
velZ float 4 Target velocity in Z dimension, meters/s
accX float 4 Target acceleration in X dimension, meters/s^2
accY float 4 Target acceleration in Y dimension, meters/s^2
accZ float 4 Target acceleration in Z dimension, meters/s^2
ec[16] float 16x4 Tracking error covariance matrix, [4x4] in range/azimuth/elevation/doppler coordinates
g float 4 Gating function gain
confidenceLevel float 4 Confidence Level

Target Index TLV

Size: sizeof (tlvHeaderStruct) + sizeof(uint8) x numberOfPoints (NOTE: here the number of points are for frame n-1)

The Target Index TLV consists of an array of target IDs. A targetID at index i is the target to which point i of the previous frame’s point cloud was associated. Valid IDs range from 0-249.

Value Type Bytes Comments
targetID uint8_t 1 Track ID

Other Target ID values:

Value Meaning
253 Point not associated, SNR too weak
254 Point not associated, located outside boundary of interest
255 Point not associated, considered as noise

Presence Indication TLV

Size: sizeof (tlvHeaderStruct) + sizeof(uint32)

The Presence Indication TLV consists of a single uint32 value to provide a binary indication of presence in the presence boundary box. A value of 1 represents presence detected and 0 represents no presence detected.


Target Height TLV

Size: sizeof(tlvHeaderStruct) + (sizeof(targetHeight)) x numberOfTargets

The Target Height TLV consists of a single uint8 corresponding to the track number it refers to, then the maximum Z estimate given as a float and the minimum Z estimate given as a float. For a more detailed explanation of the height estimation algorithm, see the 3D People Tracking Implementation Guide.

Value Type Bytes Comments
targetID uint8_t 1 Track ID
maxZ float 4 Target maxZ estimate
minZ float 4 Target minZ estimate

Need More Help?