Introduction
This workshop is an introduction to the TI Wi-SUN FAN part of the SimpleLink™ CC26x2 and CC13x2 Software Development Kits (SDK). The 4 tasks in this lab session are targeted to be completed within a 2-hour time frame. An intermediate level of knowledge of the C programming language and some experience with embedded software development is needed to be able to complete the tasks.
This lab session uses the SimpleLink CC13x2 wireless MCU LaunchPad development kit to demonstrate the tasks in this module.
In task one, you will learn how to set up a Border Router device and how to send commands over the pyspinel interface. In task two, set up a Router Node. In the third task the network is started and the connection is formed. In the fourth task, you learn how to send a ping over the network. The lab will take about one hour and a half to complete.
It is recommended to read the TI Wi-SUN FAN User's Guide alongside this lab for details and further information.
Prerequisites
Hardware
For this lab, you need one board to run the Border Router application. Supported development boards are:
- SimpleLink™ CC1312R7 LaunchPad
- SimpleLink™ CC1352P7-1 LaunchPad
In addition, you need one board to run the Router Node application. Supported development boards are:
- SimpleLink™ CC1312R7 LaunchPad
- SimpleLink™ CC1352P7-1 LaunchPad
You will also need a computer to act as the host to the network processor. You can use Windows or Linux. You will need git on your computer.
Software
- Python v.3.6.8 or later (including pip)
- CCS installed with support for CC13xx/CC26xx devices.
- SimpleLink™ CC13x2/26x2 SDK
- TI Wi-SUN FAN pySpinel GitHub repo
Recommended reading
Getting started – Desktop
Install the SDK
Open Resource Explorer via View → Resource Explorer and find the SDK you want to install.

On the right side, you will see a download icon. Click this to install the SDK and all its dependencies.

Download the off line installer from the SDK links above under
Prerequisites
Run the SimpleLink CC13X2-26X2 SDK installer:
simplelink_cc13x2_26x2_sdk_x_xx_xx_xx.exe
. These instructions assume you have installed to the default directory:C:\ti\
Install TI Clang
TI Wi-SUN FAN uses the TI Clang Compiler. This must be installed separately:
Download the package from here.
Install to the default location. This will give you
ti_ctg_armllvm_1.3.0.LTS
installed inC:\ti\
.Open Code Composer Studio and go to Window → Preferences → Build → Compilers. Check that TI Clang shows up on the list.
If TI Clang has not appeared on the list, press Refresh and install all discovered tools. Then restart CCS.
Install Python 3.x
Python 3.x is needed for the network processor interface. Python can be installed directly from www.python.org. If asked, make sure to include pip with the installation.
Install the TI Wi-SUN FAN pySpinel GitHub Repo
Within the tools folder of the SDK, there is a file called setup_pyspinel.bat. Running this file will automatically clone and setup the TI git repository that contains the NWP python files for your use.
Open the SDK and navigate to the tools folder
<SDK_INSTALL_DIR>\tools
.Run the file called setup_pyspinel.bat to setup the TI git repo. Click on the file to start running it, and the repository will be setup inside of the tools folder in your SDK.
In SimpleLink CC13x2/26x2 SDK 5.20, there is a small error in the bat file which will cause it to fail. After the file has ran, navigate to the
ti-wisunfan-pyspinel
folder (C:\ti\simplelink_cc13x2_26x2_sdk_5_20_00_52\tools\pyspinel_repo\ti-wisunfan-pyspinel
). Open a git bash. Check out theTI_WiSUN_STACK_01_00_00
tag:$ git checkout TI_WiSUN_STACK_01_00_00
Depending on your Python setup, running the
.bat
file may give you a pip error:If this happens, follow the recommendation to update pip and then install the requirements.
$ pip install --upgrade pip
Then install the requirements:
$ pip install -r requirements.txt
Yay!
All the components are ready and we can start setting up the network!
Wi-SUN Network
The Wi-SUN FAN mesh network consists of two types of logical devices: The Border Router (BR) device and the Router Node (RN) devices.
- Each PAN contains a BR providing WAN connectivity to the PAN. The BR maintains source routing tables for all nodes within its PAN, provides node authentication and key management services, and disseminates PAN wide information such as broadcast schedules.
- In addition there is one or more RNs, which provide upward and downward packet forwarding (within a PAN). An RN also provides services for relaying security and address management protocols.
Task 1 – Run the Border Router Project
A Note About Build Times
TI Wi-SUN FAN example project take a few minutes to build. This can be a bit inconvenient. For this reason try to make any alterations before you start building. This lab (except bonus task) will require you to build only once.
Luckily, the examples are available as network processors. This means that in most cases you will only need to build the project once. Most configurations can be made at runtime.
In the first task we will set up a Border Router device. This device will be the root of the network.
Import in Code Composer Studio
Open Code Composer Studio and import the BR project:
In CCS, open Project → Import CCS Projects...
Navigate to the
ns_br
folder for your development board and press Select Folder. The path is:<SDK_INSTALL_DIR>\examples\rtos\<DEVELOPMENT_BOARD>\ti_wisunfan\ns_br
Select the discovered project and press Finish.
The project will appear in your Project Explorer window as shown below.
Connect the LaunchPad
Start by making sure your kit is assembled, turned on, and connected to the PC via the USB cable.
When the LaunchPad is connected, the Windows Device Manager (Start → Control Panel → Device Manager, or Win+X, M on Windows 10) will show you the following devices connected:

The Application/User UART
serial port is used for application output in this
example.
If you are using a Linux computer, use the dmesg | grep tty
command to get a
chronological list of all devices. The second to last is the one we want to use
(e.g. /dev/ttyACM0).
Note down the COM or tty number, we will use it soon!
Build the Projects and Flash the Device
- Build the project by right-clicking on it and selecting
Build Project
.- Alternatively build all projects by pressing Ctrl + B.
- Program the project by right clicking on it and selecting Debug As → Code Composer Debug Session
- When the IDE is halted at the
main
function, terminate debugging session by clicking Ctrl + F2 or the square red stop icon.
Debugger Update
The first time you program your device, you may be prompted by CCS to update the debugger on the LaunchPad. You will need to do this in order to be able to program the device with CCS. Make sure you only run the update once at a time.
Connect the Network Processor Interface
We will use the spinel-cli.py
file to control the Border Router device. To run
a python script, open a command terminal or similar. Here, git bash is used.
Navigate to the location of
spinel-cli.py
,<SDK_INSTALL_DIR>\tools\pyspinel_repo\ti-wisunfan-pyspinel
$ cd /c/ti/simplelink_cc13x2_26x2_sdk_5_20_00_52/tools/pyspinel_repo/ti-wisunfan-pyspinel
Remember the USB port we found in the Section Connect the LaunchPad? We will use it now. Call the
spinel-cli.py
with the COM or tty port added as an argument:$ python spinel-cli.py -u COM4 spinel-cli >
$ python spinel-cli.py -u /dev/ttyACM0 spinel-cli >
If you have both pyserial and serial installed, you might get the following error:
$ python spinel-cli.py -u COM10
Couldn't open COM10 module 'serial' has no attribute 'Serial'
Traceback (most recent call last):
File "spinel-cli.py", line 1839, in <module>
main()
File "spinel-cli.py", line 1816, in main
options.baudrate, options.rtscts)
File "C:\ti\simplelink_cc13x2_26x2_sdk_5_20_00_52\tools\pyspinel_repo\ti-wisunfan-pyspinel\spinel\stream.py", line 185, in StreamOpen
return StreamSerial(dev, baudrate, rtscts)
File "C:\ti\simplelink_cc13x2_26x2_sdk_5_20_00_52\tools\pyspinel_repo\ti-wisunfan-pyspinel\spinel\stream.py", line 55, in __init__
self.serial = serial.Serial(port=dev,
AttributeError: module 'serial' has no attribute 'Serial'
If this happens, try uninstalling both pyserial and serial.
$ python -m pip uninstall serial pyserial
Then install only pyserial:
$ python -m pip install pyserial
Then try again running the spinel-cli.py
script.
When trying to open a port where you don't have the permission, you may get an error message.
$ python spinel-cli.py -u /dev/ttyACM0
Couldn’t open dev/ttyACM0 [Errno 13] could not open port dev/ttyACM0: [Errno 13] Permission denied: ‘dev/ttyACM0’
...
One way of getting this permission is using the following command:
$ sudo chmod 666 /dev/ttyACM0
You may need to repeat this every time you disconnect and reconnect the USB cable.
Another reason why you may get this error is that some other program has opened the port. If you're unsure whether this is the case, you can unplug and replug the USB cable.
Run Some Commands
Now that we have the network processor interface up and running, we can run some commands. For example, we can check the version of the image running on the LaunchPad:
spinel-cli > ncpversion
TIWISUNFAN/1.0.0; RELEASE; Jul 23 2021 13:54:01
Or we can ask for all available command to be displayed using help
:
spinel-cli > help
We have the BR running....
... Let's set up a peer device to keep it company!
Task 2 – Run the Router Node Project
In this task we will set up a Router Node to connect with the Border Router. Here we will set up one, but in a real mesh network there will be many of these devices. The steps for programming a launchpad are the same as for the BR project.
Import in Code Composer Studio
Open Code Composer Studio and import the RN project, ns_coap_node
.
The steps are the same as for the BR project, but the path is different:
<SDK_INSTALL_DIR>\examples\rtos\<DEVELOPMENT_BOARD>\ti_wisunfan\ns_coap_node
.
When you have imported the project, it will show up in CCS as follows:
Connect the LaunchPad
Connect your second LaunchPad to the laptop via USB. Again, you can check that it appears in Windows Device Manager.
When you have two launchPads connected to your laptop, it's important to make sure the correct one is programmed by CCS when you press the Debug button. If not, you risk that one LaunchPad is never programmed while the other one is overwritten each time you press the debug button. One way to avoid this is to assign a specific LaunchPad to each CCS project. Instructions for this is found here.
Build the Projects and Flash the Device
Build the project, program it and terminate the debug session using the same steps as for the BR device.
Run the Project
The ns_coap_node
project is a fully embedded implementation of the
Router Node. This means we don't need to connect through the network processor
interface. Instead, the CoAP node automatically looks for a Wi-SUN network to
join after booting. If it finds a network with matching network parameters it
will join it.
You will notice the green LED starts flashing when the CoAP node is running.
To see the connection status of the CoAP node, let's open a UART terminal.
Connect a Terminal Program
To see the serial output from the LaunchPad it is necessary to use a terminal emulator. There are several options. We will use PuTTy.
There are several options for terminal program:
- PuTTY
- Tera Term
- RealTerm
- Windows PowerShell
- Or even just going to the command prompt and typing for example
type COM10:
.- Type
help mode
to learn how to set the port parameters.
- Type
Set your terminal emulator settings to 115200
baud rate, 8
bit data, 1
stop
bit, no parity, and no flow control.
When you press the power button on the LaunchPad (next to the micro USB connector), you will see the following print out in your terminal:

Task 3 – Form the Connection
Let's start by starting the network from the Border Router device. We will start by checking the network name and PAN ID:
spinel-cli > networkname Wi-SUN Network Done
spinel-cli > panid 0xabcd Done
You can use these commands to change the network name and PAN ID. However, make sure you change these parameters on the Router Node side as well or it won't be able to connect!
Open SysConfig by double-clicking
ti_wisunfan_router_node.syscfg
.Select TI Wi-SUN FAN Stack and open the Network tab. Here you can select the PAN ID and Network name you wish.
Save the
.syscfg
file, rebuild the project and reprogram the device.Don't forget to set the same PAN ID and network name on the BR!
spinel-cli > networkname Best Network Best Network Done spinel-cli > panid 0xa1a1 Done
It's time to start the network. The first command we need is the
ifconfig up
command which brings up the network interface:spinel-cli > ifconfig up Done
The second command we need is
wisunstack
. This command tells you the status of the Wi-SUN FAN network. Call it with thestart
keyword to start the network.spinel-cli > wisunstack start Done spinel-cli > wisunstack start Done
Join time
It can take several minutes for the router node to join the network. This is because both the BR and the RN are frequency hopping.
From the BR side, we can use the
routerstate
command to check the join status of this device. For the BR, we expect this to be 5 when the network is operational.spinel-cli > routerstate 5 Successfully joined and operational Done
If the return status is something other than 5, the network has not yet started. For example if you get a 0 status.
In most cases this means you forgot to run the
ifconfig up
or thewisunstack start
command. Rerun these and retry!We can use
connecteddevices
to check if any devices are connected yet.spinel-cli > connecteddevices List of Connected Devices currently in routing table: No nodes currently in routing table.
After a few minutes the RN will join the network. The green LED will stop flashing. When this happens the RN will print out a message over UART.
On the BR, you can send the
connecteddevices
command:spinel-cli > connecteddevices List of Connected Devices currently in routing table: fd00:7283:7e00:0:212:4b00:14f7:d1b5 Done
We have a connection! At this point you can add more RNs to the network, or you can continue with the next task. If you choose to add more routers, you can use the
connecteddevices
command to get a list of all devices in the network.spinel-cli > connecteddevices List of Connected Devices currently in routing table: fd00:7283:7e00:0:212:4b00:1ca1:727a fd00:7283:7e00:0:212:4b00:1ca6:17ea Done
Task 4 – Ping the Router Node
In this task, we will send a ping from the Border Router, to the Router Node.
First we need to know the DHCP address of this RN. If we only have one RN in the network, we can use the
connecteddevices
command on the BR. This will print out the address of all connected devices.spinel-cli > connecteddevices List of Connected Devices currently in routing table: fd00:7283:7e00:0:212:4b00:14f7:d1b5 Done
If we have multiple RNs in the network, let's use the terminal display on the RN to see it's address. When the RN first connected to the network, it printed it's own address as the
CON_STATUS_LOCAL_UP
. Here, it'sfd00:7283:7e00:0:212:4b00:14f7:d1b5
.Now we can use the
ping
command from the BR:spinel-cli > ping fd00:7283:7e00:0:212:4b00:14f7:d1b5 56 bytes from fd00:7283:7e00:0:212:4b00:14f7:d1b5: icmp_seq=50089 hlim=64 time=118ms
In the return message you can even see the turnaround time.
That's ok.... but maybe there's a command we can use and see the effect on the RN side as well? A good starting point would be to check the pyspinel command documentation. You can find it in the README file in the TI Wi-SUN FAN pySpinel GitHub repo.
If you search for CoAP in the README you will find the coap specific command:
spinel-cli > coap fdde:ad00:beef:0:558:f56b:d688:799 get con led
CoAP packet received from fe80::212:4b00:10:50d4: type: 2 (Acknowledgement), token len: 0, code: 2.05 (Content), msg_id: 1
CoAP options: Content-Format (12): b''
RLED state: Off, GLED state: On
spinel-cli > coap fdde:ad00:beef:0:558:f56b:d688:799 post con led --led_state r 1
CoAP packet received from fe80::212:4b00:10:50d4: type: 2 (Acknowledgement), token len: 0, code: 2.04 (Changed), msg_id: 2
CoAP options: Content-Format (12): b''
No CoAP payload
spinel-cli > coap fdde:ad00:beef:0:558:f56b:d688:799 get non led
CoAP packet received from fe80::212:4b00:10:50d4: type: 2 (Acknowledgement), token len: 0, code: 2.04 (Changed), msg_id: 2
CoAP options: Content-Format (12): b''
No CoAP payload
For example, we can light the red LED on our RN by sending the command with --led_state r 1
.
spinel-cli > coap fd00:7283:7e00:0:212:4b00:14f7:d1b5 post con led --led_state r 1
spinel-cli >
CoAP packet received from fd00:7283:7e00:0:212:4b00:14f7:d1b5: type: 2 (Acknowledgement), token len: 0, code: 2.04 (Changed), msg_id: 0
CoAP options: Content-Format (12): b''
No CoAP payload
Bonus Task – Set up a Sniffer
A sniffer log can be very useful for debugging, or if you're just curious about what's going over the air. In short, a sniffer will observe all the packets going back and forth in the network.
In this task we will set up a sniffer to keep track of the network. You will need one additional LaunchPad. The following are supported:
We will keep the Border Router and Router Node(s) running, but some configuration is required.
To set up the sniffer, follow the steps in the TI Wi-SUN FAN User's Guide → Debugging → Packet Sniffer.
Pay attention to the final section, Application Setup
. Here you can find the
specific application changes needed.
That's it!
Very well done!
References
TI Wi-SUN FAN pySpinel GitHub repo

This work is licensed under a Creative Commons Attribution-NonCommercial-NoDerivatives 4.0 International License.