Bluetooth Low Energy - Over the Air Download (OAD) Fundamentals#
Introduction#
This module covers the basics of the Over the Air Download (OAD) feature of the TI BLE5-Stack. The estimated time to complete this lab is 3 hours. It is assumed that the reader has a basic knowledge of embedded C tool chains and general C programming concepts. This lab is intended as a starting point for users who want to get familiar with OAD concepts and running a basic update demo.
OAD refers to the ability to perform a device firmware update over-the-air using the BLE5 protocol stack. A number of software components are involved in this process and TI uses OAD to refer to all of them as a software system.
During this lab, the following topics will be covered:
Understanding the OAD fundamental components.
Setting up the environment to enable OAD.
Running the OAD demo using BTool and SimpleLink™ Connect Mobile Application.
Debugging an OAD project.
Moreover, the guide will split some tasks between On-Chip, Off-Chip and Dual-Image OAD. These sections will be accessible following an interface as the one presented below. Please select the desired application by clicking on one of the tabs.
This content will be related to On-Chip OAD use case.
This content will be related to Off-Chip OAD use case.
This content will be related to Dual-Image OAD use case.
Warning
Do not mix the information and files given for each of the OAD projects (On-Chip, Off-Chip and Dual-Image OAD) as this will lead to incorrect and unknown behavior.
Prerequisites#
Hardware#
For this lab, you need two Bluetooth-enabled development boards. Supported devices are:
Software for Development#
Software#
SIMPLELINK-LOWPOWER-F3-SDK Software Development Kit (SDK)
Code Composer Studio CCS / CCS Cloud or IAR
See Dependencies section of SDK release notes for required version.
-
See Dependencies section of SDK release notes for required version.
Readings#
It is recommended to review the OAD Chapter of the BLE5-Stack User’s Guide before starting this lab.
Getting Started#
The following installation steps can be started in the background while reading the next chapter: Anatomy of an OAD.
Installing the Software#
Import Software Projects#
The following software projects will be used in this lab. They can be imported and compiled now.
Basic BLE OAD On-Chip
The basic_ble_oad_onchip example project contains what would be the user application
functionality and implements the OAD reset service. The project can be
found inside the ble5stack examples folder:
<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\ble5stack\basic_ble_oad_onchip\
Persistent App
The basic_persistent example project is required for on-chip OAD as well. This is a
lightweight application that implements the OAD profile and is responsible of
storing the new image. The project can be found inside the ble5stack example
folder:
<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\ble5stack\basic_persistent\
MCUboot Secure Bootloader
The MCUboot is a secured open source bootloader that verifies and boots into the new image once downloaded.
There is a pre-compiled binary available within the examples folder:
<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\ble5stack\hexfiles\mcuboot_onchip_<BOARD_NAME>_nortos_ticlang.hex
Basic BLE OAD Off-Chip
The basic_ble_oad_offchip example project contains what would be the user application
functionality and implements the OAD reset service. The project can be found
in the ble5stack examples folder:
<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\ble5stack\basic_ble_oad_offchip\
MCUboot Secure Bootloader
The MCUboot is a secured open source bootloader that verifies and boots into the new image once downloaded.
There is a pre-compiled binary available within the examples folder:
<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\ble5stack\hexfiles\mcuboot_offchip_<BOARD_NAME>_nortos_ticlang.hex
Basic BLE Dual-Image
The basic_dual_image example project contains what would be the user application
functionality and implements the OAD reset service. The project can be found in the
ble5stack examples folder:
<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\ble5stack\basic_dual_image\
MCUboot Secure Bootloader
The MCUboot is a secured open source bootloader that verifies and boots into the new image once downloaded.
There is a pre-compiled binary available within the examples folder:
<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\hexfiles\mcuboot_dual_image_<BOARD_NAME>_nortos_ticlang.hex
Note
The device’s MCUboot project included in the workspace must also be flashed to the device when using on-chip/off-chip OAD or the device will not function correctly.
As detailed in the introduction, the following sections will cover some of the primary topics related to OAD using the BLE5-Stack.
Anatomy of an OAD#
This section explains various components involved in an OAD image from a high-level perspective. Each software component is treated as a building block that is added to an unmodified BLE5-Stack application without OAD (for instance, basic_ble). These BLE5-Stack images are used to build an OAD image.
Default Non OAD Image#
We will begin with the template for a standard BLE5-stack image that does not have OAD enabled.
Image without OAD#
There are three main components of this image:
The instructions/constants that implement the compiled form of the program (application code)
The reset vectors in the ARM Cortex M format: ARM Cortex M0+ Vector Table
The CCFG, which contains chip configuration parameters, see the Technical Reference Manual Section 8.2.1 CCFG.
OAD’s goal is to update a device’s software image wirelessly. In order to achieve this goal, a few software components must be (used/included).
Image Fragmentation and Image Header#
An entire image cannot be sent over in a single BLE packet due to the largest payload size supported by the Bluetooth Low Energy Specification. Therefore, the image to be sent over-the-air must be fragmented into a size that will fit into Bluetooth LE GATT payloads. The figure below pictures fragmentation of the new image into GATT payloads.
Image fragmentation#
As seen in the figure above, it will take many GATT packets to send a complete image over-the-air using the Bluetooth LE protocol. Each packet containing OAD image data is referred to as an OAD block.
However, there is no way for the receiving device to know information about the incoming image. This problem is solved by using the OAD Image Header. The OAD Image Header contains metadata describing the image and is used by the application and MCUboot secure bootloader to determine the suitability of an image for downloading or loading. Other benefits of the OAD Image Header are:
Image metadata is bundled as part of the image.
A running image can query knowledge about itself by reading the header.
Bootloader software can read the header to determine which image(s) are present and active.
Information about the incoming image is available to the target early in the OAD process.
Now, that we are sold on the benefits of an image header in an OAD system, here is an updated version of the previous drawing with an image header added.
Image with Header#
Warning
When comparing images with a header and images without the header one must keep in
mind that the header itself takes up space. The space available to the code section
of the image is shrunk to accommodate the header, and the reset vectors are pushed
back to accommodate the header. These changes are specified in the linker script
(shrinking app space) and the RTOS .cfg file (relocating reset vectors).
MCUboot Secure Bootloader#
A running image cannot update itself. This means that an incoming OAD image must be stored in a temporary location while it is being received. This temporarily location can be a reserved location in internal flash outside of the executable area covered in the first image (On-chip OAD and Dual-Image OAD applications). Alternatively, the temporary location can be in an external flash chip (Off-chip OAD applications).
In addition, after the download is complete, someone has to execute the logic to evaluate the new image and assess if the current image should be overwritten, and later executing the new image.
MCUboot is an open source project that supports hardware-independent secure bootloader for 32-bit MCUs. In the context of OAD, MCUboot serves the same purpose as the Boot Image Manager (BIM), which is to verify and boot into the new image once downloaded. Implementation details can be found in the public MCUboot Documentation. The code is maintained on the MCUboot GitHub Repository.
MCUboot is intended to permanently remain on the device, meaning it persists through many OADs and cannot be updated.
MCUboot will run every time the device boots and determine if a new image should be loaded and run (based on image header).
Furthermore, the MCUboot and CCFG structure are tied together, because both are required for a successful device boot.
The CCFG is needed by the boot ROM and startup firmware for device trim and to
determine where the program execution is to start from. By default, the boot ROM will
jump to address 0x00000000 and look for a vector table, but this region is
now occupied by the image header. A custom CCFG must be used to instruct the
device to jump directly to the MCUboot.
From there the MCUboot will perform device trim based on the CCFG settings, and determine and load the optimal image based on the OAD image header.
The MCUboot code will require more space to be reserved in our system. See below for the memory map after MCUboot has been added to the last image.
Image with Header and MCUboot#
Warning
MCUboot is responsible for linking and defining the CCFG structure, instead of the application as in the non OAD case. Therefore, the CCFG section cannot be modified by OAD and will be removed by the toolchain if it is defined.
OAD Memory Layout#
The final memory structure depends on the type of OAD in use.
This section will describe the method for placing images in internal flash when using on-chip OAD.
Requirements and Constraints for On-chip OAD
In order to perform an On-chip OAD, the target system must have:
The user application must be sufficiently small in order to fit into the flash layout system described below.
User app functionality is lost while performing OAD (Persistent app is running).
Only one user application image may be stored in flash at any time.
Internal Flash Memory Layout
The internal flash of the device contains the active user application, the user application’s stack, the persistent application, the persistent application’s stack, and the MCUboot. Each application’s role is defined below.
As we have assumed the stack-library approach, the stack images referenced below are a part of each application image (i.e. the user and persistent apps have their own dedicated stack).
MCUboot Secure Bootloader
Search for the proper image in FLASH.
Copy new user image.
Ensure validity and optionally security of image before running.
Persistent Application
Providing lightweight application that implements the OAD profile.
Stack
BLE5-Stack protocol implementation.
User Application
User defined application code.
Must implement OAD reset service.
On-Chip OAD Image#
The user application (referred to as Primary Slot) pictured above is responsible
for the following:
Implementing the protocol stack definition of the OAD reset service
Implementing customer defined behavior
The persistent application (referred to as Secondary Slot) pictured above is
responsible for the following:
Implementing the protocol stack definition of the OAD service This image is permanently resident on the device
The location of the persistent application varies depending on the flash size
available for the selected device variant. This is done to maximize the user’s
application space. Refer to the linker cmd file define IMG_A_FLASH_START to
further determine where precisely the persistent application is located.
This section will describe the method for placing images in internal and external flash when using off-chip OAD.
Requirements and Constraints for Off-chip OAD
Internal flash refers to the flash memory inside the device and external flash refers to an external SPI flash memory connected to the device.
In order to perform an Off-chip OAD the target system must have:
An off-chip flash storage as large as the application size + one external flash page to store the external flash image header. (default example will use 1MB of external flash)
A serial connection (SPI) is used to communicate with the off-chip flash component.
Free GPIO pins to interface to the external memory (i.e. 4 wires for SPI)
Enough free code space to reserve the entire contents of the last 1-2 flash page(s) for MCUboot.
The following software limitations exist on the external flash:
The maximum number of simultaneously stored OAD images is 256.
The OAD images’ headers shall be stored in the first 1 MBytes of the external flash addressable space.
The total size of the stored images should not exceed 4 GBytes.
Note
Off-chip OAD using the BLE5-Stack has only be tested using a 1 MBytes external flash. The out-of-the-box software do not allow larger external flash size.
Internal Flash Memory Layout
The internal flash of the device contains the active user application and the MCUboot. Off-chip OAD maximizes the available flash space to the user application because of its ability to store the incoming image in external flash during the download process.
Off-Chip OAD Image Internal#
The user application pictured above is responsible for the following:
Implementing the protocol stack specific implementation of the OAD transport
Finding a suitable location in external flash for the image and storing its image header in the table.
External Flash Memory Layout
The off-chip flash memory on the SimpleLink™ device LaunchPad contains the image
header vector table and the user applications. The memory map layout of the
external flash part is defined in ext_flash_layout.h. The amount of space
reserved for each application is dynamically sized by the user application’s
implementation of the OAD protocol. The size of the image in external flash can
be determined once the image header vector is sent over-the-air.
The application will round up as necessary according to the equation below:
Off-Chip OAD Image External Formula#
The memory partition of the application for Off-chip OAD is depicted in below.
Off-Chip OAD Image External#
The size of the image header table is scalable and can be changed in the user application implementation of the OAD protocol.
This section will describe the method for placing images in internal flash when using dual image OAD.
Requirements and Constraints for Dual-Image OAD
In order to perform an On-chip OAD the target system must have:
The user application must be sufficiently small in order to fit into the flash layout system described below.
Only one operational user application image may be stored in flash at any time.
Internal Flash Memory Layout
The internal flash of the device contains the following:
MCUboot: search for the proper image in flash and ensure validity and security of image before running.
Download application: memory area equivalent to the active application flash which is available for storage once the over-the-air download begins.
Active application: implements customer defined behavior in addition to the OAD reset service.
Dual-Image OAD Internal Flash Memory Layout#
OAD Protocol/ Bluetooth LE Profile#
Currently we have covered all the necessary building blocks for updating an image local to the target device. The only missing piece is a vehicle for sending the OAD blocks over-the-air and storing them on the target device.
This functionality is implemented by the BLE5-Stack OAD profile. The GATT profile is the vehicle for sending data over Bluetooth LE. At a high level, the BLE5-Stack OAD profile is responsible for receiving the following:
Determining if the candidate image should be accepted for download.
Receiving and unpacking image blocks and storing them.
Writing the received blocks to non-volatile storage.
Verifying the received image post download.
OAD Service#
The OAD service is responsible for receiving and storing an OAD image. This service is implemented in the basic_ble_oad_offchip, basic_dual_image and basic_persistent projects. See OAD service description in the BLE5-Stack User’s Guide for more information on the OAD service.
Name |
UUID |
Description |
|---|---|---|
OAD Service |
0xFFC0 |
OAD service declaration |
Image Identify |
0xFFC1 |
Used to send image header over-the-air |
Image Block Request/Response |
0xFFC2 |
Actual block of image data along with offset into the image |
Extended Control |
0xFFC5 |
Controls various aspects of OAD process |
OAD Reset Service#
The OAD reset service is only used by basic_ble_oad_onchip project. It implements a method for switching/invalidating the currently running image and resetting the device. This must occur because in on-chip solutions the currently running image cannot update itself.
See OAD reset service description in the BLE5-Stack User’s Guide for more information on the OAD reset service.
Name |
UUID |
Description |
|---|---|---|
OAD Reset Service |
0xFFD0 |
OAD reset service declaration |
OAD Start/Reset Characteristic |
0xFFD1 |
Responsible for starting the OAD process or resetting the target device |
Task 1 – Setting up the OAD Environment#
The OAD environment requires a two-step setup:
Flash the OAD Distributor with
host_testand connecting it withBTool.Flash the OAD Target with the bootloader image and the application image. This example will use the
basic_ble_oad_offchipandbasic_ble_oad_onchipprojects. For On-Chip OAD projects, thepersistent appwill also need to be flashed onto the OAD Target.
OAD Environment: Distributor and Target.#
Note
The OAD Distributor: refers to the device responsible for accepting an OAD enabled image from the compiler and transferring it over-the-air to the OAD Target device for a firmware update.
OAD Distributor Setup#
The OAD Distributor is the device responsible for fragmenting an OAD enabled image into chunks of OAD blocks and sending each block over to the OAD Target device as they are requested.
During this training we will use two different OAD Distributors: 1) SimpleLink™ Connect mobile
application, and 2) another SimpleLink™ device LaunchPad running host_test in combination with BTool.
BTool is a PC tool that is capable of interfacing to host_test and performing
various Bluetooth LE operations through HCI functions in addition to OAD. For
more information, refer to the host_test README file or the BTool User’s
Guide. In addition, in this session we will also use
Flashing the host_test Image#
See below for the steps to setup the host_test image on a CC23xx.
Navigate to
hexfilesfolder within the BLE5-Stack and select the filehost_test_app.hex<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\ble5stack\hexfiles\host_test_app.hexFlash the above hexfile using UNIFLASH.
Flashing host_test with UNIFLASH#
Warning
Please power-cycle the SimpleLink™ device after flashing it before you open the COM port in BTool.
Connecting BTool to host_test#
BTool and host_test communicate via USB through the XDS110 UART back channel.
See below for a diagram:
OAD Toolchain#
Find the port used by the UART backchannel of the SimpleLink™ LaunchPad running
host_test. This is the one with the nameXDS110 Class Application/User UART.Open BTool (see the BTool executable in the tools folder of the BLE5-Stack).
Use the following serial port settings, select OK.
Port:
<PORT_FROM_ABOVE_STEP>Baud Rate: 115200
Data length: 8 bits
Parity: None
Stop bits: 1 bit
Flow Control: None
This will open and initialize the
host_testdevice.Press the scan button and a list of discovered devices will populated in the BTOOL log.
A screen shot of a properly initialized BTool session is shown below
BTool Init Success#
OAD Target Setup#
As we learned in the section Anatomy of an OAD, the target device requires three images (On-Chip) or two images (Off-Chip and Dual-Image) to be flashed.
Note
Use a second LaunchPad for the following steps and do not flash the host_test
board again.
The first image is the MCUboot. In this lab we will be using the secure release version that is available as a precompiled .hex file:
<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\ble5stack\hexfiles\mcuboot_onchip_<BOARD_NAME>_nortos_ticlang.hex
Both persistent and user applications cannot be directly flashed as a .hex file
as image header data is required by the MCUboot to accept the image after startup.
Instead we will be using the generated image *_oad.bin. This is automatically
generated in CCS as a pre-build step that runs the OAD Image Tool. This
applies to OAD enabled projects that have SECURITY defined, which is the
default setting for OAD projects in the SDK.
The application image for on-chip OAD is split into two parts: Persistent app and user app. Exact project and file names may differ depending on the hardware and IDE used.
Compile the Persistent App project. The
Releasefolder should now contain the OAD binarybasic_persistent_<BOARD_NAME>_freertos_ticlang.binCompile the Basic BLE OAD On-Chip project. The
Releasefolder should now contain the OAD binarybasic_ble_oad_onchip_<BOARD_NAME>_freertos_ticlang_v1.binFlash all three images using UNIFLASH. You can flash them in one run, see below screenshot. Note the start address of
0x0006000for the persistent app and0x00032000for the OAD image application. To understand the reason behind the addresses values please refer to the OAD Memory Layout section.
Flashing On-Chip MCUboot and application images.#
The first image is the MCUboot. In this lab we will be using the secure release version that is available as a precompiled .hex file (or use the compiled .hex file from your MCUboot project):
<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\ble5stack\hexfiles\mcuboot_offchip_<BOARD_NAME>_nortos_ticlang.hex
The application cannot be directly flashed as a .hex file as image header data
is required for the MCUboot to accept the image after startup. Instead we will be
using the generated image *_oad.bin. This is automatically generated in CCS as
a pre-build step that runs the OAD Image Tool.
After compiling the project. The folder Release will contain the file
basic_ble_oad_offchip_<BOARD_NAME>_freertos_ticlang_v1.bin. You can flash them in one run, see
below screenshot. Note the start address of 0x0006000 for the persistent app. To understand the reason behind
the address value please refer to the OAD Memory Layout
section.
Flashing Off-Chip MCUboot and application image.#
The first image is the MCUboot. In this lab we will be using the secure release version that is available as a precompiled .hex file (or use the compiled .hex file from your MCUboot project):
<SDK_INSTALL_DIR>\examples\rtos\<BOARD_NAME>\ble5stack\hexfiles\mcuboot_dual_image_<BOARD_NAME>_nortos_ticlang.hex
The application cannot be directly flashed as a .hex file as image header data
is required for the MCUboot to accept the image after startup. Instead we will be
using the generated image *_oad.bin. This is automatically generated in CCS as
a pre-build step that runs the OAD Image Tool.
After compiling the project. The folder Release will contain the file
basic_dual_image_<BOARD_NAME>_freertos_ticlang_v1.bin. You can flash them in one run, see
below screenshot. Note the start address of 0x0006000 for the persistent app. To understand the reason behind
the address value please refer to the OAD Memory Layout
section.
Flashing Dual-Image MCUboot and application image.#
Warning
Once the OAD Target is set up, please power-cycle the SimpleLink™ device after flashing. At this point, you should see the application menu on a serial terminal.
Task 2 – Running the OAD Demo#
Now that the OAD environment is ready, we will learn how to download a new image over BLE using BTool and the SimpleLink™ Connect Mobile Application.
Modifying the Image Version#
Modifying the image version is a quick and easy way to verify that the OAD has completed. Some sample apps, like our out-of-the-box examples, will display their image version in the terminal window.
Open the project
Propertiesby doing right click on the OAD project.Go to
Build→Steps→Post-build steps.Modify the software version.
Build the application project and generate a new binary
*_vX.bin.
Project Properties - Modifying the Image Version#
OAD using BTool#
Read the OAD Target address. To do this, you can connect the OAD Distributor to a Serial Terminal. The program is prepared to display the device address when initializing.
Now switch back to the OAD Distributor. Use BTool to scan for Bluetooth LE addresses and perform an OAD with the new version of our application. After scanning, look for the OAD Target address discovered in the previous step and connect to it as shown in the image below.
BTool Establish Connection#
Once connected, switch to the OAD tab and load an OAD image (with
.binextension) into BTool by clicking atRead Image File.
Note
Make sure to use a new version of the image.
The
Securecheckbox is read-only and indicates whether the currently loaded OAD image has security enabled in its header.If using on-chip OAD, be sure to un-check the box
OAD to external flash.If using dual-image OAD, be sure to un-check the box
OAD to external flash.If using off-chip OAD, be sure to check the box
OAD to external flash.The OAD process begins once the image identify is accepted.
While intermittent blocks are being sent BTool will display:
Write Block Number = x of y.The OAD process will continue until BTool displays
OAD Download Successful.
BTool OAD Process#
For secure OAD configurations, BTool uses the default public/private key pair. To change the security keys used by the embedded device, see Generating New Security Keys (Embedded) in the BLE5-Stack User’s Guide. To change the security keys used by BTool please see the next section of this chapter.
After some delay (verification process done by the MCUboot secure bootloader), the new image should boot up and will be active.
On the OAD Target device, a new image version number should be observed on the terminal display. If the version displayed on the terminal matches the one that was send from the OAD Distributor device, then the download has completed successfully.
OAD Distributor Serial Terminal - New image version displayed.#
BTool Image Header Dialog#
A good way to inspect and parse the fields in the OAD Image Header for a given image is to use BTool. In this view, BTool will parse the various fields in the image header and present them in a human readable format. This can also be used to manually change various fields of the image header and then resign/recalculate the CRC. The image header dialog can be used to modify the image version number in order to simulate upgrading to a new version of the firmware via OAD.
You can access the OAD Image Header dialog using the following steps:
Open BTool.
Navigate to the
Over The Air Downloadpanel.Select read image file, point this to the candidate image ending with _oad.bin.
Load an OAD image (with .bin extension) by clicking at
Read Image File.
BTool - OAD Image Header#
OAD Speed Optimization#
The time required to accomplish the OAD process through BTool can be reduced by turning off the following settings at the User Interface. To this end, do right-click on the output panel at the right and turn off (un-check) the following features:
Display RX Dumps
Display TX Dumps
Display RX Packets
Display TX Packets
Auto Scroll Lock
BTool - OAD Speed Optimization#
Further steps to improve the OAD speed are:
Increase the baud-rate of BTool and host-test (requires modification and re-compiling of the host-test project)
Select the highest possible packet length.
Ensure the fastest possible connection interval of 7.5 ms. For on-chip OAD, the target connection interval may be changed by the persistent app.
SysConfig - Reduce Connection Interval.#
Note
The overall OAD performance on BTool is depending on the available processing power of the computer executing BTool. Running other software in parallel can have a noticeable impact in the time required for the OAD process.
OAD using SimpleLink™ Connect Mobile Application.#
Note
For a first experience with the TI SimpleLink™ Connect App, please go through our training lab: TI SimpleLink™ Connect App
Enable Bluetooth at the phone settings.
Open the SimpleLink™ Connect Application.
Click on
Enable Bluetooth LE scanto start discovering devices.Look for the advertising generated by the OAD Target device.
SimpleLink™ Connect Application - Select OAD Target device#
Connect to the OAD Target device and click on
TI OAD Resetservice.
SimpleLink™ Connect Application - Select OAD related Service.#
Inside the
Firmware Updatewindow, select the new image to be downloaded to the OAD Target device and click onUpdate.
SimpleLink™ Connect Application - Select Firmware and initiate OAD.#
It is also possible to modify the repository from where the image is being downloaded by first clicking at
Change to Service Specific Viewand then on the settings symbol.
SimpleLink™ Connect Application - Select new firmware to be updated from own repository.#
You can also load a local image from the device by first clicking at
Change to Service Specific Viewand then clicking at theAdd local file.
SimpleLink™ Connect Application - Select new firmware to be updated from local file.#
Wait until the download process is finished and the device resets to click on
Done.
SimpleLink™ Connect Application - Wait for OAD to finish.#
Debug an OAD Project#
The following are recommended steps to debug the basic_persistent application (similar steps can be applied for basic_ble_oad_on_chip, basic_ble_oad_off_chip, etc).
Build the image, flash the device and connect the debugger.
Build the basic_persistent app.
Click the
Debugbutton – This leads the debugger to erase the device’s flash then download the newly built image.This is going to lead to a JTAG Communication Error: (Error -615 @ 0x0). This is due to MCUboot image not being programmed leading the code at address 0x0 to be invalid.
In the
Debugwindow, right click onTexas Instruments XDS110 USB Debug ProbethenConnect Target.
Code Composer Studios - Connect to Target#
Enable the
Memory BrowserandRegistersviews.Click
View.Then select
Memory Browser.Click again
Viewand selectRegisters.
Code Composer Studios - Inspect Memory Browser#
Force the device to execute the image you want to debug.
In the memory browser, find the entry point of the image. You can leverage the map file (see the green square) if you are not sure of the address.
In all the cases, you should find the
resetVectorssymbol at the entry point of the image.For the
basic_ble_persistentapp, the entry point is at 0x6100. It is worth mentioning that the section 0x6000-0x60FF contains the image header.In the
Registersview, update the value of theCore Registers→SP registerwith the first value of theresetVectors(0x20009000 in this example).In the
Registersview, update the value of theCore Registers→PC registerwith the second value of theresetVectors(0x2C66D in this example).In the
Registersview, update the value of theSCB→VTOR registerwith the address of theresetVectors(which is also the entry point of the app, i.e. 0x6100 in this example).Setup a breakpoint in the
basic_persistentapplication (e.g. on the call toBLEAppUtil_init()in the functionappMain()inapp_main.c) and click theRun button.
Code Composer Studios - Inspect Memory vector values.#
Note
The steps provided here only leads to flash one app (which is the recommended approach for app debugging). In case multiple apps have to be flashed at the same time, Uniflash should be used. Then the step to connect the Debugger to a Running Target described in the Debugger Guide should be followed. And, eventually, the steps in (1) and (2) should be applied.