Over the Air Download (OAD)¶
This section serves as a guide to the Texas Instruments Over-the-Air Download (OAD) ecosystem. OAD is a device firmware upgrade method that allows the firmware image running on a device to be updated over the air using a proprietary RF connection while providing power loss protection.
The OAD guide section will cover:
OAD theory of operation and architecture
How to run the OAD examples included in the SimpleLink CC13x0 SDK
How to add OAD to an existing sample application
The supported development kit for OAD is a launchpad. To follow the procedures listed in this guide, two launchpad development kits are required.
Table of contents