CC2640R2 to CC26x2¶
Table of Contents¶
Introduction¶
This section describes the main differences an Application Developer must be aware of between the CC2640R2 and the CC26x2 along with a porting guide to demonstrate the migration effort.
Features and Benefits¶
Increased Processing Power and Scalability¶
The CC26x2 is a wireless MCU with a dedicated Arm Cortex-M4F application processor that is pin-to-pin compatible to the CC2640R2 in the 7x7mm QFN package.
More memory is available with an increase of non-volatile memory from 275kB to 608kB. This breaks down into 352kB Flash memory + 256 KB ROM. RAM has also increased from 28 kB to 80 kB. The availability of this increased memory provides support for Over-the-Air Downloads (OAD), larger applications, and more simultaneous connections.
Other improvements include an additional UART and a 70% reduction in current consumption in the Sensor Controller.
Bluetooth 5.1 Enabled¶
If your project wasn’t already on a BLE5 platform, the CC26x2 will provide the ability to support the new features of Bluetooth 5 and BLuetooth 5.1. This includes features such as higher throughput, longer range, advertising extensions, and improved coexistence with other wireless technology.
Enhanced Security¶
With additional hardware security accelerators for AES-128/256, SHA-256, and ECC, CC26x2 saves five times the processing time and current consumption for implementing security algorithms. This is critical to enable strong network security.
CC26x2 LaunchPad Support¶
All example applications are compatible with the CC26x2 LaunchPad development kit. These features allow for a unified development experience and empowers developers to rapidly release to market.
Compatibility Notes¶
Application Build Configuration¶
Depending on the example project, the available application build configurations
now are FlashROM_Release
, FlashROM_Debug
, and FlashROM_RCOSC_Release
.
The FlashROM_Debug
provides debug feature improvements and is user
configurable in the ble_debug.cfg
file found in the project’s Tools
folder. In contrast, FlashROM_Release
and FlashROM_RCOSC_Release
have
debug features turned off but they are still configurable in the
ble_release.cfg
file found in the project’s Tools
folder.
By default, the project’s build configuration is FlashROM_Release
.
Refer to the application’s README
file for additional application specific
information.
Stack Build Configuration¶
All application configurations use the stack library configuration,
FlashROM_Library
. This build configuration will yield additional flash
footprint optimizations by the linker since the application and stack can share
contiguous flash pages. This configuration is further discussed in the
Stack Library Configuration section of this
User’s Guide.
The build_config.opt
specifies which stack components will
be utilized, and thus which library files should be used during
the Stack Project build process. This file is located in the Tools
folder of the stack project.
BLE5 features cannot be removed from the stack. BLE5-Stack 1.02.00 now comes with BLE 5.0 features always enabled.
Predefined Symbols¶
The predefined symbols have been moved from the project properties into the
project’s Tools/defines
folder. Select the .opt
file that is
relevant to the project’s current build configuration (Debug, Release, etc.).
Heap Configuration¶
Previously, the heap configuration was handled in the application’s
app_ble.cfg
file found in the project’s Tools
folder. This is now part
of the TI RTOS configuration file (ble_debug.cfg
or ble_release.cfg
)
that is described earlier in the Application Build Configuration section.
GAP Role Removal¶
All GAP Roles source and header files (peripheral.c
, peripheral.h
,
central.c
, central.h
, etc.) have been removed. Functionality relating
to specific roles was moved into GAP Bond Manager. With the GAP Role changes,
GAP events are being handled differently. GAP events are now returned to the
application directly as RTOS events.
Further discussion of this is in Porting BLE-Stack to BLE5-Stack.
Host Privacy¶
The design of the Host Privacy in BLE5 1.02.00 is a complete redesign of the existing one. In BLE5-Stack 1.02.00 the Host is responsible for the following tasks:
- Configuring the privacy mode and own address type to conduct desired privacy operations on the controller
- Performing pairing procedure to exchange device identity information including IRK, identity address, and address type
- Updating peer device’s address information in the link DB after acquiring the identity information through pairing process
- Managing resolving list by adding/removing resolving list entries or clearing
- Storing resolving list to NV and restore it from, so that the privacy information is persistent across power cycles
Porting BLE-Stack to BLE5-Stack¶
This section will describe how to port from a BLEStack project to a BLE5Stack project.
Note
This example is specifically for CC2640R2 BLE-Stack 3.01.01/BLE5-Stack to to CC26x2 BLE5-Stack 1.02.00 but the steps are similar for all cases. Individual differences can be found in the relevant :ref:’Porting Guides’
This guide will describe a way to port a project from CC2640R2 SDK 1.50 (BLE-Stack 3.01.01)/SDK 1.40 (BLE5-Stack 1.00.01) to a CC26x2 SDK 2.10 (BLE5-Stack 1.02.00) BLE5-Stack 1.02.00 project. If your project is from BLE-Stack 3.01.01, please note that this won’t show how to add BLE5 features. However porting your project will allow the use of BLE5 features that are contained in the BLE5-Stack 1.02.00.
See the following tables for API replacements:
Porting Steps¶
To minimize project configuration differences, start with an example project in
the CC26x2 SDK 2.10 (BLE5-Stack 1.02.00). For example, if your base project
was simple_peripheral
in BLE-Stack 3.01.01, use simple_peripheral
in BLE5-Stack 1.02.00 as the project base to implement application-level
modifications on. In other words, no modifications will be made to the original
project. All application specific code will be inserted into the BLE5-Stack
1.02.00 project.
Some of these application-level modifications are due to various API changes. To aid in this, the guide provides an API translation table: GAP Changes.
Be sure to utilize the IDE and Tools recommended by the SDK’s release notes. For API Descriptions see BLE Stack API Reference. Additional information on this process can be found in the CC26x2 Wiki Porting Page
Choose a BLE5-Stack 1.02.00 example project and open it in the preferred supported IDE
We’re going to use
simple_peripheral
as the starting BLE5-Stack 1.02.00 sample project to provide context.Transfer any additional app specific predefined symbols into the example project
The predefined symbols have moved from the project properties into the project’s
Tools/defines
folder. Select the.opt
file that is relevant to the project’s current build configuration (Debug, Release, etc.). The default build configuration selected isRelease
. Further information about these configurations can be found in the README of the example project.Transfer modified application files into the example project
Modify
main.c
in the BLE5-Stack 1.02.00 example to create or rename any tasks that were added or modified in the original project. Note thatGAPRole_createTask()
should not be brought over tomain.c
.In this example, the following files from the original project were moved into
simple_peripheral
BLE5-Stack 1.02.00 example:two_btn_menu.c
andtwo_btn_menu.h
simple_peripheral.c
andsimple_peripheral.h
simple_peripheral_menu.c
andsimple_peripheral_menu.h
simple_gatt_profile.c
andsimple_gatt_profile.h
Adjust the Application for the GAP Role Removal
All GAP Roles source and header files (
peripheral.c
,peripheral.h
,central.c
,central.h
, etc.) have been removed in BLE5-Stack 1.02.00. These files will produce build errors and should not be included in your app. This change will introduce a structure change in the application.The functionality of the roles have been broken into distinct GAP functions: Scanner, Advertiser, and Initiator.
These functions of GAP can be independently controlled to allow the device to function as a desired GAP Role such as peripheral or central. For additional information about using these roles, it is suggested to refer to the GAP Roles section of the User Guide. If coming from BLE-Stack 3.01.01, this section provides information about the legacy features that exist in your current application.
Utilize the GAP Changes table to port application GAP functionality. For example, in this table you’ll find information such as
TGAP_LIM_DISC_ADV_INT_MIN
is now replaced withGAP_ADV_PARAM_PRIMARY_INTERVAL_MIN
,GAPROLE_ADVERT_ENABLED
is now done withGapAdv_enable()
or thatGAPRole_StartDevice()
is replaced byGAP_DeviceInit()
to start the GAP module.It is suggested to look at an existing example in the SDK, such as
simple_peripheral
orsimple_central
, may need to be used to assist in the porting process of the application. For example, the initialization of GAP Advertiser can be found insimple_peripheral
.After using the GAP Changes table and using a relevant BLE5-Stack 1.02.00 SDK example project as a guide, such as
simple_peripheral
, the structure and changes will become clearer.In the context of
simple_peripheral
and using the rest of the guide, the following table provides an example of changes to understand and implement when porting: Sample Simple Peripheral App Changes.Adjust the Application for the GAP Bond Manager Changes
During the removal of GAP Roles source files, functionality relating to specific roles was moved into GAP Bond Manager. One particular change is the handling of passcodes. These are now handled via call back - see
simple_peripheral
orsimple_central
for implementation details (search forpasscodeCb
).See GAP Bond Manager Changes for additional changes.
Include
icall_ble_api.h
if Stack/ICall APIs are used. Add the following #include AFTER all other includes for source files using Stack/ICall APIs.In this example, add:
#include "icall_ble_api.h"
into the following files AFTER all other includes. In for the
simple_peripheral
port, add this into these files:simple_peripheral.c
simple_gatt_profile.c
For more information regarding
icall_ble_api.h
see ICall Translation and Include.Warning
All Stack/ICall APIs are listed in
icall_ble_api.h
. If any APIs are used withouticall_ble_api.h
, build and or link errors may occur with erratic runtime behaviors!
Replace GAP Event processing
In addition to the GAP Role changes, GAP events are being handled differently. This used to be received by GAP Role (ie. SimpleBLEPeripheral_processStateChangeEvt), which would then call GAPBondMgr, and then translate the event to GAPRole specific events and pass it to the application through a callback (ie. SimpleBLEPeripheral_gapRoleCBs).
GAP events are now returned to the application directly as RTOS events. If the GAPBondMgr is present, they will first be received by the GAPBondMgr to do some processing but it will still be received the same in the application. This is now configured with
GAP_DeviceInit
. GAP events are received by the application (when the bond manager exists) as stack messages of typeGAP_MSG_EVENT
.See the example for
simple_peripheral
from BLE5-Stack 1.02.00 in the snippets below:// Address mode of the local device #define DEFAULT_ADDRESS_MODE ADDRMODE_PUBLIC //... // Entity ID globally used to check for source and/or destination of messages static ICall_EntityID selfEntity; //... // Event globally used to post local events and pend on system and // local events. static ICall_SyncHandle syncEvent; //... // Address mode static GAP_Addr_Modes_t addrMode = DEFAULT_ADDRESS_MODE; //... static void SimplePeripheral_init(void) { // Register the current thread as an ICall dispatcher application // so that the application can send and receive messages. ICall_registerApp(&selfEntity, &syncEvent); //... //Initialize GAP layer for Peripheral role, pass taskID and register to receive GAP events GAP_DeviceInit(GAP_PROFILE_PERIPHERAL, selfEntity, addrMode, NULL); }
static void SimplePeripheral_processGapMessage(gapEventHdr_t *pMsg); // function definition to handle GAP messages static uint8_t SimplePeripheral_processStackMsg(ICall_Hdr *pMsg) { // Always dealloc pMsg unless set otherwise uint8_t safeToDealloc = TRUE; switch (pMsg->event) { case GAP_MSG_EVENT: SimplePeripheral_processGapMessage((gapEventHdr_t*) pMsg); break; //... } } //... static void SimplePeripheral_processGapMessage(gapEventHdr_t *pMsg) { switch(pMsg->opcode) { case GAP_DEVICE_INIT_DONE_EVENT: { //... etc.
Adjust the Application for the GATT Profile Changes
Due to changes in LinkDB defines (
linkdb.h
), custom GATT profiles may need to be modified in order to account for the new definitions.Prepend
LINKDB_
to all constants starting withCONNHANDLE_
, for example insimple_gatt_profile.c
:// Initialize Client Characteristic Configuration attributes GATTServApp_InitCharCfg( LINKDB_CONNHANDLE_INVALID, simpleProfileChar4Config );
See GAP GATT Server Changes and Link Database Changes for additional changes as required.
Note that additional return parameters have been added to
HCI_EXT_ConnEventNoticeCmd()
:/** * Report describing connection event Returned via a @ref pfnGapConnEvtCB_t. */ typedef struct { GAP_ConnEvtStat_t status; //!< status of connection event uint16_t handle; //!< connection handle uint8_t channel; //!< BLE RF channel index (0-39) GAP_ConnEvtPhy_t phy; //!< PHY of connection event int8_t lastRssi; //!< RSSI of last packet received /// Number of packets received for this connection event uint16_t packets; /// Total number of CRC errors for the entire connection uint16_t errors; /// Type of next BLE task GAP_ConnEvtTaskType_t nextTaskType; /// Time to next BLE task (in us). 0xFFFFFFFF if there is no next task. uint32_t nextTaskTime; } Gap_ConnEventRpt_t; /** @} End GAP_Structs */
Note that additional parameter (signalIdentifier) has been added to GAP_UpdateLinkParamReq:
/** * Establish Link Request parameters * * This is used by @ref GAP_UpdateLinkParamReq */ typedef struct { uint16_t connectionHandle; //!< Connection handle of the update uint16_t intervalMin; //!< Minimum Connection Interval uint16_t intervalMax; //!< Maximum Connection Interval uint16_t connLatency; //!< Connection Latency uint16_t connTimeout; //!< Connection Timeout uint8_t signalIdentifier; //!< L2CAP Signal Identifier. Must be 0 for LL Update } gapUpdateLinkParamReq_t;
HCI_EXT_ConnEventNoticeCmd()
has been replaced withGap_RegisterConnEventCb()
. Seegap.h
for the API description.
API Translation Tables¶
These tables describe BLE5Stack API replacements for BLEStack API’s.
Previous Implementation | New/Current implementation | |
---|---|---|
Type | Name | Description / API / Parameter |
GAP EVENT | GAP_ADV_DATA_UPDATE_DONE_EVENT | Check return status of GapAdv_loadByHandle() or GapAdv_loadByBuffer() |
GAP EVENT | GAP_DEVICE_DISCOVERY_EVENT |
|
GAP EVENT | GAP_DEVICE_INFO_EVENT | GAP_EVT_ADV_REPORT or GAP_EVT_ADV_REPORT_FULL |
GAP EVENT | GAP_END_DISCOVERABLE_DONE_EVENT | Check return status of GapAdv_disable() to see that advertising is successfully being cancelled. The GAP_EVT_ADV_END_AFTER_DISABLE will be sent after the last advertisement ends. |
GAP EVENT | GAP_MAKE_DISCOVERABLE_DONE_EVENT | Check return status of GapAdv_enable() to see that advertising is successfully being started. The GAP_EVT_ADV_START_AFTER_ENABLE will be sent after the first advertisement starts. |
GAP EVENT | GAP_RANDOM_ADDR_CHANGED_EVENT | Obsolete - Address Resolution is done controller |
GAP PARAM | TGAP_GEN_DISC_ADV_MIN | Configured by durationOrMaxEvents parameter of GapAdv_enable() |
GAP PARAM | TGAP_LIM_ADV_TIMEOUT | Configured by durationOrMaxEvents parameter of GapAdv_enable() |
GAP PARAM | TGAP_GEN_DISC_SCAN | Configured by parameters of GapScan_enable() |
GAP PARAM | TGAP_LIM_DISC_SCAN | Configured by parameters of GapScan_enable() |
GAP PARAM | TGAP_GEN_DISC_SCAN_INT | Configured by interval parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_GEN_DISC_SCAN_WIND | Configured by window parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_LIM_DISC_SCAN_INT | Configured by interval parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_LIM_DISC_SCAN_WIND | Configured by window parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_CONN_EST_ADV_TIMEOUT | Configured by durationOrMaxEvents parameter of GapAdv_enable() |
GAP PARAM | TGAP_CONN_PARAM_TIMEOUT | GAP_SetParamValue() with GAP_PARAM_CONN_PARAM_TIMEOUT |
GAP PARAM | TGAP_LIM_DISC_ADV_INT_MIN | GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN |
GAP PARAM | TGAP_LIM_DISC_ADV_INT_MAX | GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX |
GAP PARAM | TGAP_GEN_DISC_ADV_INT_MIN | GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN |
GAP PARAM | TGAP_GEN_DISC_ADV_INT_MAX | GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX |
GAP PARAM | TGAP_CONN_ADV_INT_MIN | GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN |
GAP PARAM | TGAP_CONN_ADV_INT_MAX | GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX |
GAP PARAM | TGAP_CONN_SCAN_INT | Configured by interval parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_CONN_SCAN_WIND | Configured by window parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_CONN_HIGH_SCAN_INT | Configured by interval parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_CONN_HIGH_SCAN_WIND | Configured by window parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_GEN_DISC_SCAN_INT | Configured by interval parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_GEN_DISC_SCAN_WIND | Configured by window parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_LIM_DISC_SCAN_INT | Configured by interval parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_LIM_DISC_SCAN_WIND | Configured by window parameter of GapScan_setPhyParams() |
GAP PARAM | TGAP_CONN_EST_INT_MIN | GapInit_setPhyParam() with INIT_PHYPARAM_CONN_INT_MIN |
GAP PARAM | TGAP_CONN_EST_INT_MAX | GapInit_setPhyParam() with INIT_PHYPARAM_CONN_INT_MAX |
GAP PARAM | TGAP_CONN_EST_SCAN_INT | GapInit_setPhyParam() with INIT_PHYPARAM_SCAN_INTERVAL |
GAP PARAM | TGAP_CONN_EST_SCAN_WIND | GapInit_setPhyParam() with INIT_PHYPARAM_SCAN_WINDOW |
GAP PARAM | TGAP_CONN_EST_SUPERV_TIMEOUT | GapInit_setPhyParam() with INIT_PHYPARAM_SUP_TIMEOUT |
GAP PARAM | TGAP_CONN_EST_LATENCY | GapInit_setPhyParam() with INIT_PHYPARAM_CONN_LATENCY |
GAP PARAM | TGAP_CONN_EST_MIN_CE_LEN | Obsolete - Not Used by Controller |
GAP PARAM | TGAP_CONN_EST_MAX_CE_LEN | Obsolete - Not Used by Controller |
GAP PARAM | TGAP_PRIVATE_ADDR_INT | GAP_SetParamValue() with GAP_PARAM_PRIVATE_ADDR_INT |
GAP PARAM | TGAP_CONN_PAUSE_CENTRAL | Obsolete - Not Used by Controller |
GAP PARAM | TGAP_CONN_PAUSE_PERIPHERAL | GAP_UpdateLinkParamReq() |
GAP PARAM | TGAP_SM_TIMEOUT | GAP_SetParamValue() with GAP_PARAM_SM_TIMEOUT |
GAP PARAM | TGAP_SM_MIN_KEY_LEN | GAP_SetParamValue() with GAP_PARAM_SM_MIN_KEY_LEN |
GAP PARAM | TGAP_SM_MAX_KEY_LEN | GAP_SetParamValue() with GAP_PARAM_SM_MAX_KEY_LEN |
GAP PARAM | TGAP_FILTER_ADV_REPORTS | Obsolete - Duplicate Filtering done in Controller |
GAP PARAM | TGAP_SCAN_RSP_RSSI_MIN | GapScan_setParam() with SCAN_PARAM_FLT_MIN_RSSI |
GAP PARAM | TGAP_REJECT_CONN_PARAMS | GAP_SetParamValue() with GAP_PARAM_LINK_UPDATE_DECISION |
GAP PARAM | TGAP_AUTH_TASK_ID | GAP_SetParamValue() with GAP_PARAM_AUTH_TASK_ID |
GAP PARAM | TGAP_VERIFY_CAR | DEPRECATED |
GAP PARAM | TGAP_GGS_PARAMS | GAP_SetParamValue() with GAP_PARAM_GGS_PARAMS |
GAP PARAM | GAPROLE_IRK, GAPCENTRALROLE_IRK | GapConfig_SetParameter() with GAP_CONFIG_PARAM_IRK |
GAP PARAM | GAPROLE_SRK, GAPCENTRALROLE_SRK | GapConfig_SetParameter() with GAP_CONFIG_PARAM_SRK |
GAP PARAM | GAPROLE_BD_ADDR, GAPCENTRALROLE_BD_ADDR | HCI_ReadBDADDRCmd() |
GAP PARAM | GAPROLE_ADVERT_ENABLED, GAPROLE_ADV_NONCONN_ENABLED | GapAdv_enable() and GapAdv_disable() |
GAP PARAM | GAPROLE_ADVERT_OFF_TIME | Configured by durationOrMaxEvents parameter of GapAdv_enable() |
GAP PARAM | GAPROLE_ADVERT_DATA | |
GAP PARAM | GAPROLE_SCAN_RSP_DATA | |
GAP PARAM | GAPROLE_ADV_EVENT_TYPE | GapAdv_setParam() or GapAdv_getParam() with GAP_ADV_PARAM_PROPS |
GAP PARAM | GAPROLE_ADV_DIRECT_TYPE | GapAdv_setParam() or GapAdv_getParam() with GAP_ADV_PARAM_PEER_ADDRESS_TYPE |
GAP PARAM | GAPROLE_ADV_DIRECT_ADDR | GapAdv_setParam() or GapAdv_getParam() with GAP_ADV_PARAM_PEER_ADDRESS |
GAP PARAM | GAPROLE_ADV_CHANNEL_MAP | GapAdv_setParam() or GapAdv_getParam() with GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP |
GAP PARAM | GAPROLE_ADV_FILTER_POLICY | GapAdv_setParam() or GapAdv_getParam() with GAP_ADV_PARAM_FILTER_POLICY |
GAP PARAM | GAPROLE_CONNHANDLE | Returned for each GAP event |
GAP PARAM | GAPROLE_RSSI_READ_RATE | RSSI can be received by HCI_ReadRssiCmd() |
GAP PARAM | GAPROLE_PARAM_UPDATE_ENABLE | GAP_UpdateLinkParamReq() can be called as desired |
GAP PARAM | GAPROLE_MIN_CONN_INTERVAL | pParams.intervalMin parameter of GAP_UpdateLinkParamReq() |
GAP PARAM | GAPROLE_MAX_CONN_INTERVAL | pParams.intervalMax parameter of GAP_UpdateLinkParamReq() |
GAP PARAM | GAPROLE_SLAVE_LATENCY | pParams.connLatency parameter of GAP_UpdateLinkParamReq() |
GAP PARAM | GAPROLE_TIMEOUT_MULTIPLIER | pParams.connTimeout parameter of GAP_UpdateLinkParamReq() |
GAP PARAM | GAPROLE_STATE | Obsolete - GAP changes remove the need for this |
GAP PARAM | GAPROLE_CONN_BD_ADDR, GAPROLE_BD_ADDR_TYPE | Returned in GAP_LINK_ESTABLISHED_EVENT, contained in stack message, gapEstLinkReqEvent_t when the link is established Or use linkDB_GetInfo() at any time during the connection |
GAP PARAM | GAPROLE_CONN_INTERVAL | Returned from linkDB_GetInfo(), as linkDBInfo_t.connInterval |
GAP PARAM | GAPROLE_CONN_LATENCY | Returned from linkDB_GetInfo(), as linkDBInfo_t.connLatency |
GAP PARAM | GAPROLE_CONN_TIMEOUT | Returned from linkDB_GetInfo(), as linkDBInfo_t.connTimeout |
GAP PARAM | GAPCENTRALROLE_MAX_SCAN_RES | Configured by maxNumReport parameter of GapScan_enable() |
GAP PARAM | GAPCENTRALROLE_LINK_PARAM_UPDATE_REQ_REPLY | GAP_SetParamValue() with GAP_PARAM_LINK_UPDATE_DECISION |
GAP API | GAP_DeviceInit, GAPRole_StartDevice, GAPCentralRole_StartDevice |
|
GAP API | GAPRole_RegisterAppCBs | Obsolete - Functionality moved to GAPBondMgr_Register() |
GAP API | GAP_SetAdvToken | Obsolete - Advertisement Sets are Used |
GAP API | GAP_GetAdvToken | Obsolete - Advertisement Sets are Used |
GAP API | GAP_RemoveAdvToken | Obsolete - Advertisement Sets are Used |
GAP API | GAP_UpdateAdvTokens | Obsolete - Advertisement Sets are Used |
GAP API | GAPRole_SendUpdateParam, GAPCentralRole_UpdateLink | GAP_UpdateLinkParamReq() |
GAP API | GAP_MakeDiscoverable | GapAdv_enable() |
GAP API | GAP_UpdateAdvertisingData | |
GAP API | GAP_EndDiscoverable | GapAdv_disable() |
GAP API | GAP_DeviceDiscoveryRequest, GAPCentralRole_StartDiscovery | GapScan_enable() |
GAP API | GAP_DeviceDiscoveryCancel, GAPCentralRole_CancelDiscovery | GapScan_disable() |
GAP API | GAP_ResolvePrivateAddr | Obsolete - Address Resolution is done controller |
GAP API | GAP_EstablishLinkReq, GAPCentralRole_EstablishLink | GapInit_connect(), or GapInit_connectWl() to use Filter Accept List |
GAP API | GAP_TerminateLinkReq, GAPRole_TerminateConnection, GAPCentralRole_TerminateLink | GapInit_cancelConnect() for connection request, GAP_TerminateLinkReq() otherwise |
GAP API | GAP_ConfigDeviceAddr | Obsolete - Only way to configure the device address is as parameters in GAP_DeviceInit() |
GAP CB | gapRolesParamUpdateCB_t, paramUpdateAppDecision_t, passThroughToApp_t | These are handled through GAP_UPDATE_LINK_PARAM_REQ_EVENT, applies to the L2CAP Parameter Update Procedure as well. |
GAP CB | gapRolesStateNotify_t, pfnGapCentralRoleEventCB_t | Moved into GAP Bond Manager callbacks, gapBondCBs_t |
Previous Implementation | New/Current implementation | |
---|---|---|
Type | Name | Description / API / Parameter |
GAPBOND PARAM | GAPBOND_DEFAULT_PASSCODE | Use pfnPasscodeCB_t, shared default passcode defined in bcomdef.h B_APP_DEFAULT_PASSCODE |
GAPBOND PARAM | GAPBOND_REMOTE_OOB_SC_ENABLED | Obsolete |
GAPBOND PARAM | GAPBOND_REMOTE_OOB_SC_DATA | Obsolete |
GAPBOND PARAM | GAPBOND_LOCAL_OOB_SC_ENABLED | Obsolete |
GAPBOND PARAM | GAPBOND_LOCAL_OOB_SC_DATA | Obsolete |
GAPBOND STATE | GAPBOND_PAIRING_STATE_BONDED | GAPBOND_PAIRING_STATE_ENCRYPTED |
GAPBOND DEF | GBM_QUEUE_PAIRINGS | Removed, is now default behavior |
GAPBOND DEF | GBM_GATT_NO_CLIENT | Configured by GATT_NO_CLIENT |
GAPBOND DEF | SNP_SECURITY | Configured by GAPBONDMGR_NO_SIGNING |
GAPBOND API | GAPBondMgr_LinkEst | Removed Application Access to API Handled Internally |
GAPBOND API | GAPBondMgr_LinkTerm | Removed Application Access to API Handled Internally |
GAPBOND API | GAPBondMgr_SlaveReqSecurity | GAPBondMgr_Pair(), allowing both Centrals and Peripherals to request pairing |
GAPBOND API | GAPBondMgr_UpdateCharCfg | Removed Application Access to API Handled Internally |
GAPBOND API | GAPBondMgr_ReadGattChar | Removed Application Access to API Handled Internally |
GAPBOND API | GAPBondMgr_SupportsEnhancedPriv | Removed Application Access to API Handled Internally |
GAPBOND API | GAPBondMgr_CheckNVLen | Removed Application Access to API Handled Internally |
GAPBOND API | GAPBondMgr_syncResolvingList | Removed Application Access to API Handled Internally |
Previous Implementation | New/Current implementation | |
---|---|---|
Type | Name | Description / API / Parameter |
GGS PARAM | GGS_PERI_PRIVACY_FLAG_ATT | Obsolete |
GGS PARAM | GGS_RECONNCT_ADDR_ATT | Obsolete |
GGS PARAM | GGS_PERI_PRIVACY_FLAG_PROPS | Obsolete |
GGS PARAM | GGS_W_PERMIT_PRIVACY_FLAG_ATT | Obsolete |
GGS PARAM | GGS_TESTMODE_W_PERMIT_PRIVACY_FLAG | Obsolete |
Previous Implementation | New/Current implementation | |
---|---|---|
Type | Name | Description / API / Parameter |
LinkDB API | linkDB_Remove | API now accepts linkDBInfo_t in addition to connection handle |
Previous Implementation | BLE5-Stack 1.02.00 Implementation |
---|---|
SimpleBLEPeripheral_processStateChangeEvt | See SimplePeripheral_processGapMessage |
SimpleBLEPeripheral_processAppMsg | Different events are now being handled. See SimplePeripheral_processAppMsg |
SimpleBLEPeripheral_processStackMsg |
|
SimpleBLEPeripheral_stateChangeCB gapRolesCBs_t SimpleBLEPeripheral_gapRoleCBs |
|
GAP_SetParamValue(TGAP_CONN_PAUSE_PERIPHERAL, DEFAULT_CONN_PAUSE_PERIPHERAL) | GAP_UpdateLinkParamReq() |
GAPRole_SetParameter(GAPROLE_ADVERT_ENABLED, sizeof(uint8_t),&initialAdvertEnable) | In SimplePeripheral_processGapMessage by GapAdv_enable() |
GAPRole_SetParameter(GAPROLE_ADVERT_OFF_TIME, sizeof(uint16_t),&advertOffTime) | In SimplePeripheral_processGapMessage by GapAdv_enable().
Configured by the third parameter durationOrMaxEvents |
GAPRole_SetParameter(GAPROLE_SCAN_RSP_DATA, sizeof(scanRspData),scanRspData) | In SimplePeripheral_processGapMessage by GapAdv_loadByHandle().
with GAP_ADV_DATA_TYPE_SCAN_RSP set as the data type |
GAPRole_SetParameter(GAPROLE_ADVERT_DATA, sizeof(advertData), advertData) | In SimplePeripheral_processGapMessage by GapAdv_loadByHandle()
with GAP_ADV_DATA_TYPE_ADV set as the data type |
GAPRole_SetParameter(GAPROLE_PARAM_UPDATE_ENABLE, sizeof(uint8_t), &enableUpdateRequest) | In SimplePeripheral_processGapMessage ,
parameter updates from a central device are
handled in GAP_UPDATE_LINK_PARAM_REQ_EVENT and
uses GAP_UpdateLinkParamReqReply() |
GAPRole_SetParameter(GAPROLE_MIN_CONN_INTERVAL, sizeof(uint16_t), &desiredMinInterval) | In SimplePeripheral_processParamUpdate ,
set as DEFAULT_DESIRED_MIN_CONN_INTERVAL
and applied with GAP_UpdateLinkParamReq() |
GAPRole_SetParameter(GAPROLE_MAX_CONN_INTERVAL, sizeof(uint16_t), &desiredMaxInterval) | In SimplePeripheral_processParamUpdate ,
set as DEFAULT_DESIRED_MAX_CONN_INTERVAL
and applied with GAP_UpdateLinkParamReq() |
GAPRole_SetParameter(GAPROLE_SLAVE_LATENCY, sizeof(uint16_t), &desiredSlaveLatency) | In SimplePeripheral_processParamUpdate ,
set as DEFAULT_DESIRED_SLAVE_LATENCY
and applied with GAP_UpdateLinkParamReq() |
GAPRole_SetParameter(GAPROLE_TIMEOUT_MULTIPLIER, sizeof(uint16_t), &desiredConnTimeout) | In SimplePeripheral_processParamUpdate ,
set as DEFAULT_DESIRED_CONN_TIMEOUT
and applied with GAP_UpdateLinkParamReq() |
GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MIN, advInt) GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MIN, advInt) | GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN |
GAP_SetParamValue(TGAP_LIM_DISC_ADV_INT_MAX, advInt) GAP_SetParamValue(TGAP_GEN_DISC_ADV_INT_MAX, advInt) | GapAdv_setParam() with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX |
GAPBondMgr_SetParameter(GAPBOND_DEFAULT_PASSCODE, sizeof(uint32_t), &passkey) | Use pfnPasscodeCB_t, shared default passcode defined in bcomdef.h B_APP_DEFAULT_PASSCODE |
GAPROLE_STATE | Obsolete - GAP changes remove the need for this |
GAPROLE_CONNHANDLE | Returned for each GAP event |