233 #ifndef ti_drivers_AESCTRDRBG__include 234 #define ti_drivers_AESCTRDRBG__include 260 #define AESCTRDRBG_STATUS_RESERVED (-32) 268 #define AESCTRDRBG_STATUS_SUCCESS (0) 276 #define AESCTRDRBG_STATUS_ERROR (-1) 286 #define AESCTRDRBG_STATUS_RESOURCE_UNAVAILABLE (-2) 294 #define AESCTRDRBG_STATUS_RESEED_REQUIRED (-3) 299 #define AESCTRDRBG_AES_BLOCK_SIZE_BYTES 16 505 const void *additionalData,
506 size_t additionalDataLength);
ADC_Params params
Definition: Driver_Init.h:11
The CryptoKey type is an opaque representation of a cryptographic key.
AESCTRDRBG_AES_KEY_LENGTH
Length in bytes of the internal AES key used by an instance.
Definition: AESCTRDRBG.h:304
#define AESCTRDRBG_AES_BLOCK_SIZE_BYTES
The AES block size in bytes.
Definition: AESCTRDRBG.h:299
void AESCTRDRBG_close(AESCTRDRBG_Handle handle)
Function to close an AESCTRDRBG peripheral specified by the AESCTRDRBG_Handle.
Definition: AESCTRDRBG.h:347
Definition: AESCTRDRBG.h:342
const AESCTRDRBG_Params AESCTRDRBG_defaultParams
Default AESCTRDRBG_Params structure.
void AESCTRDRBG_init(void)
This function initializes the AESCTRDRBG driver.
void * object
Definition: AESCTRDRBG.h:363
CryptoKey datastructure.
Definition: CryptoKey.h:209
AESCTRDRBG Global configuration.
Definition: AESCTRDRBG.h:361
AESCTRDRBG_SEED_LENGTH
Length in bytes of seed used to instantiate or reseed instance.
Definition: AESCTRDRBG.h:312
Definition: AESCTRDRBG.h:314
Definition: AESCTRDRBG.h:313
AESCTRDRBG_Handle AESCTRDRBG_construct(AESCTRDRBG_Config *config, const AESCTRDRBG_Params *params)
Constructs a new AESCTRDRBG object.
AESCTRDRBG Parameters.
Definition: AESCTRDRBG.h:382
void const * hwAttrs
Definition: AESCTRDRBG.h:366
AESCTRDRBG_ReturnBehavior
The way in which AESCTRDRBG function calls return after generating the requested entropy.
Definition: AESCTRDRBG.h:337
Definition: AESCTRDRBG.h:305
const void * seed
Definition: AESCTRDRBG.h:390
void * custom
Definition: AESCTRDRBG.h:410
uint32_t reseedInterval
Definition: AESCTRDRBG.h:386
AESCTRDRBG_Config * AESCTRDRBG_Handle
A handle that is returned from an AESCTRDRBG_open() call.
Definition: AESCTRDRBG.h:372
AESCTRDRBG_AES_KEY_LENGTH keyLength
Definition: AESCTRDRBG.h:383
int_fast16_t AESCTRDRBG_reseed(AESCTRDRBG_Handle handle, const void *seed, const void *additionalData, size_t additionalDataLength)
Reseed an AESCTRDRBG instance.
AESCTRDRBG_Handle AESCTRDRBG_open(uint_least8_t index, const AESCTRDRBG_Params *params)
This function opens a given AESCTRDRBG instance.
int_fast16_t AESCTRDRBG_getBytes(AESCTRDRBG_Handle handle, CryptoKey *randomBytes)
Generate a requested number of random bytes.
AESCTRDRBG_ReturnBehavior returnBehavior
Definition: AESCTRDRBG.h:403
void AESCTRDRBG_Params_init(AESCTRDRBG_Params *params)
Function to initialize the AESCTRDRBG_Params struct to its defaults.
size_t personalizationDataLength
Definition: AESCTRDRBG.h:399
Definition: AESCTRDRBG.h:306
const void * personalizationData
Definition: AESCTRDRBG.h:395