ADC driver's custom configuration structure.
Definition: ADC.h:346
ADC_Params params
Definition: Driver_Init.h:11
ADC Parameters used with ADC_open().
Definition: ADC.h:258
uint32_t ADC_convertToMicroVolts(ADC_Handle handle, uint16_t adcValue)
Function to convert a raw ADC sample into microvolts.
void ADC_Params_init(ADC_Params *params)
Initialize an ADC_Params structure to its default values.
Analog to Digital Conversion (ADC) Input Driver.
ADC_Handle ADC_open(uint_least8_t index, ADC_Params *params)
Function to initialize the ADC peripheral.
ADC_convert(adcHandle, &result)
ADC_Handle adcHandle
Definition: Driver_Init.h:15
resultUv
Definition: Driver_Init.h:21
ADC_init()
Function to initialize the ADC driver.
#define ADC_INSTANCE
Definition: Driver_Init.h:5