Z-Stack 3.6.0+ to Z-Stack 4.3.0

This section will describe a way to migrate a projects Z-Stack 3.6.0 and later to a Z-Stack 4.3.0 project.

Note

Z-Stack 3.6.0 is the last 3.x version, the next being Z-Stack 4.1.0 and since then following the same SimpleLink CC13xx/CC26xx SDK version naming convention.

For this guide, zc_light from Z-Stack 3.6.0 will be compared with Z-Stack 4.3.0. New features and updates that have occurred in between include:

  • Project pre-definition changes
  • Renaming of several ZCL definitions
  • Revised callbacks and API names/parameters
  • LED handling

The recommended approach is to start with a Z-Stack 4.3.0 project that contains the same base application as the porting target project and merge any custom functionality.

  1. Choose a Z-Stack 4.3.0 example project that contains your target project’s base functionality. For reference and use in this example, zc_light from C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\examples\rtos\CC13xx or CC26xx_LAUNCHXL\zstack is chosen as a starting point.
  2. Multiple application predefinitions have changed, including (but not limited to) USE_ZCL_SAMPLEAPP_UI to CUI_DISABLE and OTA_CLIENT to OTA_CLIENT_INTEGRATED. The list of current preprocessor definitions are available in Application Preprocessor Configuration and developers must take caution to modify their project settings and application files accordingly. For example, instances of #ifdef USE_ZCL_SAMPLEAPP_UI should become ifndef CUI_DISABLE in zcl_sample*.[c/h].
  3. As SysConfig has been upgraded to version 1.6.0, developers must modify their Z-Stack settings (and thus the definitions generated for ti_zstack_config.h) in the new .syscfg file from the Z-Stack 4.3.0 project. Refer to the directions in Zigbee Configuration for more information.
  4. Several ZCL files inside C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\source\ti\zstack\stack\zcl have renamed definitions for cluster IDs, attributes, and commands. For example, ZCL_CLUSTER_ID_GEN_BASIC from zcl.h is now ZCL_CLUSTER_ID_GENERAL_BASIC. Several changes have been made to other common zcl*.h files including zcl_general.h and zcl_ha.h, among others. Affected definitions range from ZCL_*, COMMAND_*, ATTRID_*, and more. Developers must be sure to update the zcl_sample*_data.c and zcl_sample*.c files accordingly for consistency. Other clusters, attributes, or simple descriptors which were added or altered in the previous Z-Stack project should also be migrated accordingly.

The following items specifically concern zcl_samplelight.c:

  1. DMM functionality for related projects has been modified slightly, thus instances of if USE_DMM are replaced with #if defined(USE_DMM) && defined(BLE_START).

  2. static void zclSampleLight_LevelControlMoveToClosestFrequencyCB( zclLCMoveFreq_t *pCmd ); has been added and is placed in the zclGeneral_AppCallbacks_t zclSampleLight_CmdCallbacks table:

    static zclGeneral_AppCallbacks_t zclSampleLight_CmdCallbacks =
    {
    ...
    #ifdef ZCL_LEVEL_CTRL
      zclSampleLight_LevelControlMoveToLevelCB,             // Level Control Move to Level command
      zclSampleLight_LevelControlMoveCB,                    // Level Control Move command
      zclSampleLight_LevelControlStepCB,                    // Level Control Step command
      zclSampleLight_LevelControlStopCB,                    // Level Control Stop command
      zclSampleLight_LevelControlMoveToClosestFrequencyCB,  // Level Control Stop command
    #endif
    ...
    };
    

    Also, zclSampleLight_LevelControlStopCB now has parameter zclLCStop_t *pCmd instead of void.

  3. Key and button handling have been modified:

      #include <ti/drivers/apps/Button.h>
      #include <ti/drivers/apps/LED.h>
      ...
      ##ifndef CUI_DISABLE
      CONST char zclSampleLight_appStr[] = APP_TITLE_STR;
      CUI_clientHandle_t gCuiHandle;
      static LED_Handle gRedLedHandle;
      static uint32_t gSampleLightInfoLine;
      #endif
      ...
      #ifndef CUI_DISABLE
      static void zclSampleLight_processKey(uint8_t key, Button_EventMask buttonEvents);
      static void zclSampleLight_RemoveAppNvmData(void);
      static void zclSampleLight_InitializeStatusLine(CUI_clientHandle_t gCuiHandle);
      static void zclSampleLight_UpdateStatusLine(void);
      #endif
      ...
        //Request the Red LED for App
        LED_Params ledParams;
        LED_Params_init(&ledParams);
        gRedLedHandle = LED_open(CONFIG_LED_RED, &ledParams);
    
        //Initialize the sampleLight UI status line
    zclSampleLight_InitializeStatusLine(gCuiHandle);
      ...
      static void zclSampleLight_UpdateLedState(void)
      {
    
      #ifndef CUI_DISABLE
        // set the LED1 based on light (on or off)
        if ( LIGHT_ON == zclSampleLight_getOnOffAttribute())
        {
      #ifdef ZCL_LEVEL_CTRL
          uint8_t lightLevel = zclSampleLight_getCurrentLevelAttribute();
    
          // lightLevel is a value from 0-255. We must map this to a percentage (0-100%)
          LED_stopBlinking(gRedLedHandle);
          LED_setOn(gRedLedHandle, (lightLevel * 100) / 255);
      #else
          LED_stopBlinking(gRedLedHandle);
          LED_setOn(gRedLedHandle, LED_BRIGHTNESS_MAX);
          #endif
        }
        else
        {
          LED_stopBlinking(gRedLedHandle);
          LED_setOff(gRedLedHandle);
        }
      #endif
    
      }
      ...
      static void zclSampleLight_processKey(uint8_t key, Button_EventMask buttonEvents)
      {
          if (buttonEvents & Button_EV_CLICKED)
          {
              if(key == CONFIG_BTN_LEFT)
              {
                  zstack_bdbStartCommissioningReq_t zstack_bdbStartCommissioningReq;
    
                  zstack_bdbStartCommissioningReq.commissioning_mode = zclSampleLight_BdbCommissioningModes;
                  Zstackapi_bdbStartCommissioningReq(appServiceTaskId, &zstack_bdbStartCommissioningReq);
              }
              if(key == CONFIG_BTN_RIGHT)
              {
    
              }
          }
      }
    

    The CUI_led* APIs are no longer used.

  4. zclport_registerZclHandleExternal now includes an endpoint as the first parameter, zclport_registerZclHandleExternal(SAMPLELIGHT_ENDPOINT, zclSampleLight_ProcessIncomingMsg);.

  5. All Timer_* APIs have become UtilTimer_*.

  6. Updated third parameter for CUI_statusLineResourceRequest, const bool _refreshInd set to false in the default application.

  7. Any other Z-Stack 3.6.0+ application changes to the Z-Stack 4.3.0 file, if not pertaining to the items listed above, should be added accordingly.

Note

Difference comparison software is recommended for discerning all differences between software stacks.