51 #include <openthread/thread.h> 203 Button_EventMask _buttonEvents);
229 extern void tiopCUIReset(
const char _input,
char* _pLines[3],
void processMenuUpdateFn(void)
Handles CUI Menu update events for examples.
Definition: LP_CC2674R10_FPGA/thread/door_lock/tiop_ui.h:60
void tiopCUINwkReset(const char _input, char *_pLines[3], CUI_cursorInfo_t *_pCurInfo)
Reset the OpenThread Instance as well as clear out the previous network data. CUI function type that ...
void uiActionJoin(const int32_t _itemEntry)
Handles join menu option event for examples.
cuiConn
Definition: LP_CC2674R10_FPGA/thread/door_lock/tiop_ui.h:56
void tiopCUIUpdateConnStatus(cuiConn status)
Update connection status CUI output line.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:409
Definition: LP_CC2674R10_FPGA/thread/door_lock/tiop_ui.h:58
void uiActionAttach(const int32_t _itemEntry)
Handles attach menu option event for examples.
void processKeyChangeCB(Button_Handle _buttonHandle, Button_EventMask _buttonEvents)
Handles the key pressed events for examples.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/doorlock.c:351
void tiopCUIUpdateChannel(uint8_t ch)
Update channel CUI output.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:302
void tiopCUIInit(char *appString, Button_Handle *rightButtonHandle)
Initialize example CUI functionality.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:106
void tiopCUIUpdateShortAddr(otShortAddress s)
Update short address CUI output.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:316
void tiopCUIUpdateExtPANID(otExtendedPanId extPan)
Update Extended panid CUI output.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:259
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/cui.h:748
void tiopCUIUpdateApp(char *appInfo)
Update Application specific CUI output line.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:447
Definition: LP_CC2674R10_FPGA/thread/door_lock/tiop_ui.h:61
void uiActionProcessConfigureChannel(const char _input, char *_pLines[3], CUI_cursorInfo_t *_pCurInfo)
Handle reading user input into the channel configuration in CUI.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:584
void tiopCUIUpdateRole(otDeviceRole role)
Update device role CUI output line.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:328
cuiConn
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.h:56
void uiActionProcessConfigurePanId(const char _input, char *_pLines[3], CUI_cursorInfo_t *_pCurInfo)
Handle reading user input into the panid configuration in CUI.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:455
Definition: LP_CC2674R10_FPGA/thread/door_lock/tiop_ui.h:59
static Button_Handle rightButtonHandle
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/doorlock.c:184
void tiopCUIUpdateNwkName(const char *name)
Update network name CUI output.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:244
void tiopCUIUpdateMasterkey(otMasterKey key)
Update masterkey CUI output.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:274
void tiopCUIReset(const char _input, char *_pLines[3], CUI_cursorInfo_t *_pCurInfo)
Reset the OpenThread Instance without clearing out previous network data. CUI function type that is c...
void tiopCUIUpdateDeviceInfo(void)
Update device info CUI output line.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:230
void tiopCUIUpdatePANID(otPanId pan)
Update panid CUI output.
Definition: CC1352P_2_LAUNCHXL/thread/door_lock/tiop_ui.c:290