40 #ifndef ti_drivers_TimerSupport__include 41 #define ti_drivers_TimerSupport__include bool TimerSupport_timerFullWidth(Timer_Handle handle)
Function to determine if timer is full-width.
void TimerSupport_timerEnable(Timer_Handle handle)
Function to enable the timer peripheral.
Timer Global configuration.
Definition: Timer.h:385
void TimerSupport_timerDisable(Timer_Handle handle)
Function to disable the timer peripheral.
void TimerSupport_timerLoad(Timer_Handle handle)
Function to load timer peripheral.