CPU_TPIU

Instance: CPU_TPIU
Component: CPU_TPIU
Base address: 0xE0040000


Cortex-M's Trace Port Interface Unit (TPIU)

TOP:CPU_TPIU Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

SSPSR

RO

32

0x0000 000B

0x0000 0000

0xE004 0000

CSPSR

RW

32

0x0000 0001

0x0000 0004

0xE004 0004

ACPR

RW

32

0x0000 0000

0x0000 0010

0xE004 0010

SPPR

RW

32

0x0000 0001

0x0000 00F0

0xE004 00F0

FFSR

RO

32

0x0000 0008

0x0000 0300

0xE004 0300

FFCR

RW

32

0x0000 0102

0x0000 0304

0xE004 0304

FSCR

RO

32

0x0000 0000

0x0000 0308

0xE004 0308

CLAIMMASK

RO

32

0x0000 000F

0x0000 0FA0

0xE004 0FA0

CLAIMSET

WO

32

0x0000 000F

0x0000 0FA0

0xE004 0FA0

CLAIMTAG

RO

32

0x0000 0000

0x0000 0FA4

0xE004 0FA4

CLAIMCLR

WO

32

0x0000 0000

0x0000 0FA4

0xE004 0FA4

DEVID

RO

32

0x0000 0CA0

0x0000 0FC8

0xE004 0FC8

TOP:CPU_TPIU Register Descriptions

TOP:CPU_TPIU:SSPSR

Address Offset 0x0000 0000
Physical Address 0xE004 0000 Instance 0xE004 0000
Description Supported Sync Port Sizes
This register represents a single port size that is supported on the device, that is, 4, 2 or 1. This is to ensure that tools do not attempt to select a port width that an attached TPA cannot capture.
Type RO
Bits Field Name Description Type Reset
31:4 RESERVED4 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x000 0000
3 FOUR 4-bit port size support

0x0: Not supported
0x1: Supported
RO 1
2 THREE 3-bit port size support

0x0: Not supported
0x1: Supported
RO 0
1 TWO 2-bit port size support

0x0: Not supported
0x1: Supported
RO 1
0 ONE 1-bit port size support

0x0: Not supported
0x1: Supported
RO 1

TOP:CPU_TPIU:CSPSR

Address Offset 0x0000 0004
Physical Address 0xE004 0004 Instance 0xE004 0004
Description Current Sync Port Size
This register has the same format as SSPSR but only one bit can be set, and all others must be zero. Writing values with more than one bit set, or setting a bit that is not indicated as supported can cause Unpredictable behavior. On reset this defaults to the smallest possible port size, 1 bit.
Type RW
Bits Field Name Description Type Reset
31:4 RESERVED4 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0x000 0000
3 FOUR 4-bit port enable
Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior.
RW 0
2 THREE 3-bit port enable
Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior.
RW 0
1 TWO 2-bit port enable
Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior.
RW 0
0 ONE 1-bit port enable
Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior.
RW 1

TOP:CPU_TPIU:ACPR

Address Offset 0x0000 0010
Physical Address 0xE004 0010 Instance 0xE004 0010
Description Async Clock Prescaler
This register scales the baud rate of the asynchronous output.
Type RW
Bits Field Name Description Type Reset
31:13 RESERVED13 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b000 0000 0000 0000 0000
12:0 PRESCALER Divisor for input trace clock is (PRESCALER + 1). RW 0b0 0000 0000 0000

TOP:CPU_TPIU:SPPR

Address Offset 0x0000 00F0
Physical Address 0xE004 00F0 Instance 0xE004 00F0
Description Selected Pin Protocol
This register selects the protocol to be used for trace output.
Note: If this register is changed while trace data is being output, data corruption occurs.
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000 0000 0000 0000 0000 0000 0000
1:0 PROTOCOL Trace output protocol
Value ENUM Name Description
0x0 TRACEPORT TracePort mode
0x1 SWO_MANCHESTER SerialWire Output (Manchester). This is the reset value.
0x2 SWO_NRZ SerialWire Output (NRZ)
RW 0b01

TOP:CPU_TPIU:FFSR

Address Offset 0x0000 0300
Physical Address 0xE004 0300 Instance 0xE004 0300
Description Formatter and Flush Status
Type RO
Bits Field Name Description Type Reset
31:4 RESERVED4 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x000 0000
3 FTNONSTOP 0: Formatter can be stopped
1: Formatter cannot be stopped
RO 1
2:0 RESERVED0 This field always reads as zero RO 0b000

TOP:CPU_TPIU:FFCR

Address Offset 0x0000 0304
Physical Address 0xE004 0304 Instance 0xE004 0304
Description Formatter and Flush Control
When one of the two single wire output (SWO) modes is selected, ENFCONT enables the formatter to be bypassed. If the formatter is bypassed, only the ITM/DWT trace source (ATDATA2) passes through. The TPIU accepts and discards data that is presented on the ETM port (ATDATA1). This function is intended to be used when it is necessary to connect a device containing an ETM to a trace capture device that is only able to capture Serial Wire Output (SWO) data. Enabling or disabling the formatter causes momentary data corruption.
Note: If the selected pin protocol register (SPPR.PROTOCOL) is set to 0x00 (TracePort mode), this register always reads 0x102, because the formatter is automatically enabled. If one of the serial wire modes is then selected, the register reverts to its previously programmed value.
Type RW
Bits Field Name Description Type Reset
31:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b000 0000 0000 0000 0000 0000
8 TRIGIN Indicates that triggers are inserted when a trigger pin is asserted. RW 1
7:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000
1 ENFCONT Enable continuous formatting:

0: Continuous formatting disabled
1: Continuous formatting enabled
RW 1
0 RESERVED0 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0

TOP:CPU_TPIU:FSCR

Address Offset 0x0000 0308
Physical Address 0xE004 0308 Instance 0xE004 0308
Description Formatter Synchronization Counter
Type RO
Bits Field Name Description Type Reset
31:0 FSCR The global synchronization trigger is generated by the Program Counter (PC) Sampler block. This means that there is no synchronization counter in the TPIU. RO 0x0000 0000

TOP:CPU_TPIU:CLAIMMASK

Address Offset 0x0000 0FA0
Physical Address 0xE004 0FA0 Instance 0xE004 0FA0
Description Claim Tag Mask
Type RO
Bits Field Name Description Type Reset
31:0 CLAIMMASK This register forms one half of the Claim Tag value. When reading this register returns the number of bits that can be set (each bit is considered separately):

0: This claim tag bit is not implemented
1: This claim tag bit is implemented

The behavior when writing to this register is described in CLAIMSET.
RO 0x0000 000F

TOP:CPU_TPIU:CLAIMSET

Address Offset 0x0000 0FA0
Physical Address 0xE004 0FA0 Instance 0xE004 0FA0
Description Claim Tag Set
Type WO
Bits Field Name Description Type Reset
31:0 CLAIMSET This register forms one half of the Claim Tag value. Writing to this location allows individual bits to be set (each bit is considered separately):

0: No effect
1: Set this bit in the claim tag

The behavior when reading from this location is described in CLAIMMASK.
WO 0x0000 000F

TOP:CPU_TPIU:CLAIMTAG

Address Offset 0x0000 0FA4
Physical Address 0xE004 0FA4 Instance 0xE004 0FA4
Description Current Claim Tag
Type RO
Bits Field Name Description Type Reset
31:0 CLAIMTAG This register forms one half of the Claim Tag value. Reading this register returns the current Claim Tag value.
Reading CLAIMMASK determines how many bits from this register must be used.

The behavior when writing to this register is described in CLAIMCLR.
RO 0x0000 0000

TOP:CPU_TPIU:CLAIMCLR

Address Offset 0x0000 0FA4
Physical Address 0xE004 0FA4 Instance 0xE004 0FA4
Description Claim Tag Clear
Type WO
Bits Field Name Description Type Reset
31:0 CLAIMCLR This register forms one half of the Claim Tag value. Writing to this location enables individual bits to be cleared (each bit is considered separately):

0: No effect
1: Clear this bit in the claim tag.

The behavior when reading from this location is described in CLAIMTAG.
WO 0x0000 0000

TOP:CPU_TPIU:DEVID

Address Offset 0x0000 0FC8
Physical Address 0xE004 0FC8 Instance 0xE004 0FC8
Description Device ID
Type RO
Bits Field Name Description Type Reset
31:0 DEVID This field returns: 0xCA1 if there is an ETM present. 0xCA0 if there is no ETM present. RO 0x0000 0CA0