Hardware Architecture¶
System Core¶
The system core is designed to run the wireless protocol stack from the link layer up to the user application.
For CC13x1 and CC26x1 devices the system core is ARM Cortex M4
For CC13x2 and CC26x2 devices the system core is ARM Cortex M4F
For CC13x4 and CC2674 devices the system core is ARM Cortex M33
You can read more about ARM Cortex in the Arm Cortex User Guide.
The link layer interfaces to the radio core through a software module called the RF driver, which sits above the RF doorbell software layer. The RF driver runs on the system core and acts as an interface to the radio on the CC13xx or CC26xx, and also manages the power domains of the radio hardware and radio core. Documentation for the RF driver can be found at the TI Drivers API Reference.
Radio Core (Arm Cortex-M0)¶
The Cortex-M0 (CM0) core within the CC13xx or CC26xx is responsible for both interfacing to the radio hardware, and translating complex instructions from the system core into bits that are sent over the air using the radio. For TI 15.4-Stack, the CM0 implements the PHY layer of the protocol stack. The CM0 is able to operate autonomously, which frees up the system core for higher-level protocol and application-layer processing.
The system core communicates with the CM0 through a hardware interface called the RF doorbell, which is documented in the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual. The radio core firmware is not intended to be used or modified by the application developer.
Flash, RAM, and Peripherals¶
The following in-system programmable flash memory and SRAM options are available for the CC13xx or CC26xx. For a full memory of your device, please refer to the CC13xx or CC26xx datasheet.
Device |
Flash (kB) |
SRAM (kB) |
---|---|---|
CC13x1x3 or CC26x1x3 |
352 |
40 |
CC13x2x1 or CC26x2x1 |
352 |
80 |
CC13x2x7 or CC26x2x7 |
704 |
144 |
CC13x4x10 or CC26x4x10 |
1024 |
256 |
Devices outside of the CC13x1x3 or CC26x1x3 also contain 8 kB of cache SRAM that can be utilized to extend RAM capacity or can function as a normal cache to increase application performance. The CC13xx or CC26xx also hosts a full range of peripherals including UART, I2C, I2S, AES, TRNG, temperature and battery monitors, 4x 32-bit timers, 2x SSI, and an integrated and autonomous sensor controller. See Sensor Controller for more information on the sensor controller.
Below is a sample device block diagram. Please check the datasheet for an accurate block diagram of your device.
CC13x1x3 and CC26x1x3¶
The CC13x1x3 or CC26x1x3 are cost-optimized devices with a reduced feature set, as such the following changes have taken effect:
Features and peripherals which have been removed
IEEE 754-compliant single-precision Floating Point Unit (FPU)
Memory Protection Unit (MPU)
AES 256-bit crypto accelerator
ECC and RSA Public Key Hardware Accelerator
SHA2 Accelerator
Sensor Controller with 4KB of SRAM
Further peripheral modifications
1x UART
1x SSI (SPI, MICROWIRE, TI)
32KB + 8KB GP cache SRAM, parity removed
40 KB ROM
Note
One implication of SRAM reduction is that Dynamic Multiprotocol Management (DMM) is not possible for common use cases with CC13x1x3 or CC26x1x3 devices.
Programming Internal Flash With the ROM Bootloader¶
The CC13xx or CC26xx internal flash memory can be programmed using the bootloader located in device ROM. Both UART and SPI protocols are supported. See the Bootloader chapter of the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual for more details on the programming protocol and requirements.
Note
Because the ROM bootloader uses predefined DIO pins for internal flash programming, allocate these pins in the board layout. The CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual has more details on the pins allocated to the bootloader based on the chip package type.
Startup Sequence¶
For a complete description of the CC13xx or CC26xx reset sequence, see the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
Resets¶
Reset the device using only hard resets. From the software, this reset can be accomplished using:
HAL_SYSTEM_RESET();
In CCS, select Board Reset (automatic) from the reset menu (see Figure 11.). Then you can press the reset button to reset the device.