TI Bluetooth Mesh Host PC Tool

This section describes the functionality of the Bluetooth Mesh Host PC Tool features and provides a list of APIs eRPC uses to interface with Bluetooth Mesh.

Overview

The PC host application is a Python based tool created using the Embedded Remote Procedure Call (eRPC) system which is an open source Remote Procedure Call system. This application acts as the host processor with the goal of providing the option of getting started and performing the operations of the BLE Mesh examples.

Running Bluetooth Mesh Host PC Tool

This section covers the required libraries and installations prior to running the Host PC tool. In addition, it covers the steps on how to get the Host PC tool running on a PC.

Installation

  1. Install Python version 3.7.6.

    1. Download Python installer from: https://www.python.org/downloads/release/python-376/

    Note

    Utilize the Windows x86-64 executable installer.

  2. Install eRPC.

    1. Navigate to <SDK_ROOT>/source/third_party/erpc/erpc_python

    2. Install Python library enum34 using the following command:

      pip install enum34

    3. Install Python library pyserial using the following command:

      pip install pyserial

    4. Install the eRPC packages by using the following command:

      python setup.py install

Running Tool

  1. Navigate to the location of the Host PC tool at <SDK_ROOT>/examples/rtos/ CC26X2R1_LAUNCHXL/ble5stack/mesh_app_python.

  2. Run the ble_mesh_erpc_app script.

    1. Open up a terminal such as Git Bash.

    2. Run the ble_mesh_erpc_app script using the following command:

      python ble_mesh_erpc_app.py

    3. At this moment, if not already running, flash a CC26x2 device with the simple_mesh_node example project. ERPC uses UART2 on the device side. Ensure that simple_mesh_node is compiled with “Network Processor Mode” enabled in SysConfig as seen in Figure 157. in order to work with the host.

      ../_images/ble_mesh_erpc_enable_nwp_syscfg.png

      Figure 157. Enabling Network Processor Mode in SysConfig

    4. Determine the COM port the simple_mesh_node device is connected to. Enter the COM port when prompted as seen in Figure 158.

      ../_images/ble_mesh_erpc_com_port.png

      Figure 158. Providing Device COM Port

    Note

    When entering the device serial port name, include the phrase “COM”. For example, for a simple_mesh_node device connected to COM port 13, enter “COM13”.

    1. Utilize the command menu seen in Figure 159. to select the proper commands needed.

      ../_images/ble_mesh_erpc_command_menu.png

      Figure 159. Host PC Tool Command Menu

Using Menu Commands

The commands should be run in the following order upon start-up to function successfully:

  1. Run one of the following menu commands to initialize Mesh:

    • Mesh init and unprovisioned beacon

    • Mesh init and static provisioning

    • Mesh init and load from NV

Only one of these commands needs to be called when initializing Mesh. Each command should be called in different scenarios. The Mesh init and unprovisioned beacon command should be used when the purpose is to initialize the Mesh data and start advertising unprovisioned beacon. The Mesh init and static provisioning command should be used when the purpose is to initialize Mesh data and perform static provisioning. Finally, the Mesh init and load from NV should be used when the purpose is to initialize the Mesh data and load previous provisioning data from NV. For instance, if the device reset after povisioning, this command should be used to return to a provisioned state without performing the provisioning process again.

Host PC Tool APIs

This section describes the APIs available on the Host PC Tool and the mapping of the APIs to the ones provided on the Bluetooth Mesh project. Upon the Host PC Tool startup and connecting to the correct device serial port, the following menu Figure 159. will appear in the terminal. Table 33. details these command descriptions.

Table 33. eRPC Commands and Bluetooth API Mapping

Command

API Description

Bluetooth API Mapping

Mesh init and unprovisioned beacon

Initialize Mesh data and call mesh_prov_enable to enable specific provisioning bearers

bt_mesh_prov_raw_init bt_mesh_init_comp_raw_init bt_mesh_init_elem_raw_init bt_mesh_cfg_srv_raw_init bt_mesh_health_srv_raw_init bt_mesh_init_model_raw_init bt_mesh_init bt_mesh_prov_enable

Mesh Init and static provisioning

Initialize Mesh data and do static provisioning

bt_mesh_prov_raw_init bt_mesh_init_comp_raw_init bt_mesh_init_elem_raw_init bt_mesh_cfg_srv_raw_init bt_mesh_cfg_cli_raw_init bt_mesh_health_srv_raw_init bt_mesh_init_model_raw_init bt_mesh_init bt_mesh_provision

Mesh Init and load from NV

Initialize the Mesh data and load from NV

bt_mesh_prov_raw_init bt_mesh_init_comp_raw_init bt_mesh_init_elem_raw_init bt_mesh_cfg_srv_raw_init bt_mesh_health_srv_raw_init bt_mesh_init_model_raw_init bt_mesh_init settings_load

Mesh load provisioning information from NV

Call the Zephyr settings module load API settings_load

settings_load

Mesh is provisioned

Check if the local node has been provisioned by calling bt_mesh_is_provisioned

bt_mesh_is_provisioned

Mesh Prov Enable

Enable specific porivisoning bearers by calling bt_mesh_prov_enable ADV and GATT bearers.

bt_mesh_prov_enable

Mesh Reset

Reset the state of the local Mesh node by calling bt_mesh_reset

bt_mesh_reset

Mesh Generic OnOff Client Menu

Initialize and start the generic on/off client Menu Screen

This command opens additional menu. For Bluetooth API mapping, please see the Generic OnOff Menu Commands and Bluetooth APIs table

Mesh VND Model Menu

Initialize and start the VND model example Menu Screen

This command opens additional menu. For Bluetooth API mapping, please see the VND Menu Commands and Bluetooth APIs table

Mesh find model index

Find a SIG model in a specific element

bt_mesh_model_find

Mesh find vnd model index

Find a VND model in a specific element

bt_mesh_model_find_vnd

Mesh LPN set

Toggle the Low Power feature of the local device

bt_mesh_lpn_set

Mesh LPN poll

Send out a Friend Poll message

bt_mesh_lpn_poll

Mesh PROXY Identity enable

Enable advertising with Node Identity

bt_mesh_proxy_identity_enable

Generate Fault on Health server (for testing only)

Used for adding a new fault to the fault array of the health server model, only used for testing purposes

bt_mesh_fault_update

Quit

Exit menu application

Figure 160. will appear when choosing command 8. Mesh Generic OnOff Client Menu on the main menu. Table 34. details the these command descriptions.

../_images/ble_mesh_erpc_gen_onoff_menu.png

Figure 160. Host PC Tool Generic OnOff Command Sub-Menu

Table 34. Generic OnOff Menu Commands and Bluetooth APIs

Command

API Description

Bluetooth API Mapping

Mesh Generic OnOff Client get msg

Get Gen OnOff State

bt_mesh_model_send_data

Mesh Generic OnOff Client set msg

Set Gen OnOff State

bt_mesh_model_send_data

Mesh Generic OnOff Client set msg with transition

Set Gen OnOff State with Transition

bt_mesh_model_send_data

Mesh Generic OnOff Client set unack msg

Set Gen OnOff Unacknowledged State

bt_mesh_model_send_data

Mesh Generic OnOff Client set unack msg with transition

Set Gen OnOff Unacknowledged State with Transition

bt_mesh_model_send_data

Back

Return to upper menu screen

Figure 161. will appear when choosing command 9. Mesh VND Model Menu. Table 35. details the these command descriptions.

../_images/ble_mesh_erpc_vnd_menu.png

Figure 161. Host PC Tool Generic OnOff Command Sub-Menu

Table 35. VND Menu Commands and Bluetooth APIs

Command

API Description

Bluetooth API Mapping

Mesh VND LED ON

Call VND Model API led_on

led_on

Mesh VND LED OFF

Call VND Model API led_off

led_off

Mesh VND Notify LED Status

Call VND Model API notify_led_status

notify_led_status

Mesh VND Get LED Status

Call VND Model API get_led_status

get_led_status

Mesh VND Send Large MSG

Call VND Model API vnd_large_msg

vnd_large_msg

Back

Return to upper menu screen