52 #ifndef ti_drivers_power_PowerCC26XX_ 53 #define ti_drivers_power_PowerCC26XX_ 55 #include <ti/drivers/dpl/HwiP.h> 56 #include <ti/drivers/dpl/ClockP.h> 59 #include <ti/devices/DeviceFamily.h> 66 typedef uint8_t PowerCC26XX_Resource;
70 #define PowerCC26XX_RESUMETIMESTANDBY 750 73 #define PowerCC26XX_TOTALTIMESTANDBY 1000 76 #define PowerCC26XX_WAKEDELAYSTANDBY 240 79 #define PowerCC26XX_INITIALWAITRCOSC_LF 1000 82 #define PowerCC26XX_RETRYWAITRCOSC_LF 1000 85 #define PowerCC26XX_INITIALWAITXOSC_HF 50 88 #define PowerCC26XX_RETRYWAITXOSC_HF 50 91 #define PowerCC26XX_INITIALWAITXOSC_LF 10000 94 #define PowerCC26XX_RETRYWAITXOSC_LF 5000 100 #define PowerCC26XX_PERIPH_GPT0 0 103 #define PowerCC26XX_PERIPH_GPT1 1 106 #define PowerCC26XX_PERIPH_GPT2 2 109 #define PowerCC26XX_PERIPH_GPT3 3 112 #define PowerCC26XX_PERIPH_SSI0 4 113 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X4_CC26X3_CC26X4) 115 #define PowerCC26XX_PERIPH_SPI0 PowerCC26XX_PERIPH_SSI0 119 #define PowerCC26XX_PERIPH_UART0 5 122 #define PowerCC26XX_PERIPH_I2C0 6 125 #define PowerCC26XX_PERIPH_TRNG 7 128 #define PowerCC26XX_PERIPH_GPIO 8 131 #define PowerCC26XX_PERIPH_UDMA 9 134 #define PowerCC26XX_PERIPH_CRYPTO 10 137 #define PowerCC26XX_PERIPH_I2S 11 140 #define PowerCC26XX_PERIPH_RFCORE 12 143 #define PowerCC26XX_XOSC_HF 13 146 #define PowerCC26XX_DOMAIN_PERIPH 14 149 #define PowerCC26XX_DOMAIN_SERIAL 15 152 #define PowerCC26XX_DOMAIN_RFCORE 16 155 #define PowerCC26XX_DOMAIN_SYSBUS 17 158 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X2_CC26X2 || \ 159 DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X4_CC26X3_CC26X4) 162 #define PowerCC26XX_PERIPH_PKA 18 165 #define PowerCC26XX_PERIPH_UART1 19 168 #define PowerCC26XX_PERIPH_SSI1 20 169 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X4_CC26X3_CC26X4) 171 #define PowerCC26XX_PERIPH_SPI1 PowerCC26XX_PERIPH_SSI1 176 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X4_CC26X3_CC26X4) 179 #define PowerCC26XX_PERIPH_UART2 21 182 #define PowerCC26XX_PERIPH_UART3 22 185 #define PowerCC26XX_PERIPH_SPI2 23 187 #define PowerCC26XX_PERIPH_SSI2 PowerCC26XX_PERIPH_SPI2 190 #define PowerCC26XX_PERIPH_SPI3 24 192 #define PowerCC26XX_PERIPH_SSI3 PowerCC26XX_PERIPH_SPI3 195 #define PowerCC26XX_PERIPH_I2C1 25 199 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X0_CC26X0) 200 #define PowerCC26XX_NUMRESOURCES 19 201 #elif (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X1_CC26X1) 202 #define PowerCC26XX_NUMRESOURCES 19 203 #elif (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X2_CC26X2) 204 #define PowerCC26XX_NUMRESOURCES 21 205 #elif (DeviceFamily_PARENT == DeviceFamily_PARENT_CC13X4_CC26X3_CC26X4) 206 #define PowerCC26XX_NUMRESOURCES 26 212 #define PowerCC26XX_PERIPH 0x80 213 #define PowerCC26XX_SPECIAL 0x40 214 #define PowerCC26XX_DOMAIN 0x00 215 #define PowerCC26XX_PARENTMASK 0x3F 216 #define PowerCC26XX_NOPARENT 0x3F 220 #define PowerCC26XX_STANDBY 0x1 223 #define PowerCC26XX_ENABLE 1 224 #define PowerCC26XX_DISABLE 0 229 #define PowerCC26XX_RETAIN_VIMS_CACHE_IN_STANDBY 0 232 #define PowerCC26XX_DISALLOW_SHUTDOWN 1 235 #define PowerCC26XX_DISALLOW_STANDBY 2 238 #define PowerCC26XX_DISALLOW_IDLE 3 241 #define PowerCC26XX_NEED_FLASH_IN_IDLE 4 254 #define PowerCC26XX_SWITCH_XOSC_HF_MANUALLY 5 263 #define PowerCC26XX_DISALLOW_XOSC_HF_SWITCHING 6 266 #define PowerCC26XX_NUMCONSTRAINTS 7 271 #define PowerCC26XX_SD_DISALLOW PowerCC26XX_DISALLOW_SHUTDOWN 272 #define PowerCC26XX_SB_DISALLOW PowerCC26XX_DISALLOW_STANDBY 273 #define PowerCC26XX_IDLE_PD_DISALLOW PowerCC26XX_DISALLOW_IDLE 274 #define PowerCC26XX_XOSC_HF_SWITCHING_DISALLOW PowerCC26XX_DISALLOW_XOSC_HF_SWITCHING 275 #define PowerCC26XX_SB_VIMS_CACHE_RETAIN PowerCC26XX_RETAIN_VIMS_CACHE_IN_STANDBY 285 #define PowerCC26XX_ENTERING_STANDBY 0x1 288 #define PowerCC26XX_ENTERING_SHUTDOWN 0x2 291 #define PowerCC26XX_AWAKE_STANDBY 0x4 295 #define PowerCC26XX_AWAKE_STANDBY_LATE 0x8 298 #define PowerCC26XX_XOSC_HF_SWITCHED 0x10 310 #define PowerCC26XX_SCLK_LF_SWITCHED 0x20 380 #define PowerCC26XX_JTAG_PD_TURNED_ON 0x40 383 #define PowerCC26XX_NUMEVENTS 6 390 #define PowerCC26XX_SETUP_CALIBRATE 1 391 #define PowerCC26XX_INITIATE_CALIBRATE 2 392 #define PowerCC26XX_DO_CALIBRATE 3 400 uint16_t driverlibID;
401 } PowerCC26XX_ResourceRecord;
447 bool (*calibrateFxn)(
unsigned int arg);
571 #if defined(DeviceFamily_CC26X0R2) 572 bool emulatorAttached;
574 uint8_t constraintCounts[PowerCC26XX_NUMCONSTRAINTS];
576 uint8_t resourceCounts[PowerCC26XX_NUMRESOURCES];
578 unsigned int (*resourceHandlers[3])(
unsigned int arg);
725 #define Power_getPerformanceLevel(void) 0 726 #define Power_setPerformanceLevel(level) Power_EFAIL bool calLF
Definition: PowerCC26XX.h:564
void PowerCC26XX_doWFI(void)
The Wait for interrupt (WFI) policy.
int32_t nDeltaFreqNew
Definition: PowerCC26XX.h:560
bool xoscPending
Definition: PowerCC26XX.h:563
bool bRefine
Definition: PowerCC26XX.h:561
bool PowerCC26XX_calibrate(unsigned int arg)
The RC Oscillator (RCOSC) calibration function.
uint32_t constraintMask
Definition: PowerCC26XX.h:547
bool calibrateRCOSC_LF
Boolean specifying whether the low frequency RC oscillator (RCOSC_LF) should be calibrated.
Definition: PowerCC26XX.h:526
bool enableMaxStandbyDuration
Boolean that enables limiting the duration spent in standby.
Definition: PowerCC26XX.h:504
Power_PolicyInitFxn policyInitFxn
The Power Policy's initialization function.
Definition: PowerCC26XX.h:413
void(* Power_PolicyInitFxn)(void)
Power policy initialization function pointer.
Definition: Power.h:402
uint16_t vddrRechargeMargin
Margin in SCLK_LF periods subtracted from previous longest VDDR recharge period.
Definition: PowerCC26XX.h:491
HwiP_Struct hwiStruct
Definition: PowerCC26XX.h:552
uint32_t maxStandbyDuration
Time in system ticks that specifies the maximum duration the device may spend in standby.
Definition: PowerCC26XX.h:474
bool enablePolicy
Boolean specifying if the Power Policy function is enabled.
Definition: PowerCC26XX.h:517
int32_t nCtrimFractNew
Definition: PowerCC26XX.h:557
Power_PolicyFxn policyFxn
The Power Policy function.
Definition: PowerCC26XX.h:435
bool initialized
Definition: PowerCC26XX.h:570
int32_t nRtrimNew
Definition: PowerCC26XX.h:558
int32_t nCtrimNew
Definition: PowerCC26XX.h:556
void PowerCC26XX_schedulerDisable(void)
ClockP_Handle PowerCC26XX_getClockHandle(void)
Get the handle of the Clock object used for scheduling device wakeups.
void(* Power_PolicyFxn)(void)
Power policy function pointer.
Definition: Power.h:407
uint32_t state
Definition: PowerCC26XX.h:562
bool busyCal
Definition: PowerCC26XX.h:566
void PowerCC26XX_standbyPolicy(void)
The STANDBY Power Policy.
void PowerCC26XX_switchXOSC_HF(void)
Switch the HF clock source to XOSC_HF.
bool calibrateRCOSC_HF
Boolean specifying whether the high frequency RC oscillator (RCOSC_HF) should be calibrated.
Definition: PowerCC26XX.h:535
Power_PolicyFxn policyFxn
Definition: PowerCC26XX.h:580
uint32_t PowerCC26XX_getXoscStartupTime(uint32_t timeUntilWakeupInMs)
Get the estimated HF crystal oscillator (XOSC_HF) startup delay, for a given delay from now...
int32_t nCtrimCurr
Definition: PowerCC26XX.h:554
PowerCC26XX_ModuleState.
Definition: PowerCC26XX.h:544
uint8_t calStep
Definition: PowerCC26XX.h:567
ClockP_Struct calClockStruct
Definition: PowerCC26XX.h:551
Global configuration structure.
Definition: PowerCC26XX.h:405
bool PowerCC26XX_injectCalibration(void)
Explicitly trigger RC oscillator calibration.
int32_t nCtrimFractCurr
Definition: PowerCC26XX.h:555
int32_t nDeltaFreqCurr
Definition: PowerCC26XX.h:553
bool PowerCC26XX_noCalibrate(unsigned int arg)
Function to specify when RCOSC calibration is to be disabled.
bool firstLF
Definition: PowerCC26XX.h:568
int32_t nRtrimCurr
Definition: PowerCC26XX.h:559
ClockP_Struct xoscClockObj
Definition: PowerCC26XX.h:549
ClockP_Struct clockObj
Definition: PowerCC26XX.h:548
bool enablePolicy
Definition: PowerCC26XX.h:569
ClockP_Struct lfClockObj
Definition: PowerCC26XX.h:550
void PowerCC26XX_schedulerRestore(void)
uint8_t hwiState
Definition: PowerCC26XX.h:565
List_List notifyList
Definition: PowerCC26XX.h:546
bool PowerCC26XX_isStableXOSC_HF(void)
Check if the XOSC_HF is stable and ready to be switched to.