![]() |
![]() |
Data Structures | |
| union | ECC_NISTP256_Param |
| Union to access ECC_NISTP256 curve params in bytes or words. More... | |
Macros | |
| #define | ECCParams_NISTP256_LENGTH 32 |
| Length of NIST P256 curve parameters in bytes. More... | |
| #define | ECC_NISTP256_PARAM_LENGTH_WITH_PREFIX_BYTES (ECCParams_NISTP256_LENGTH + ECC_LENGTH_PREFIX_BYTES) |
| Length in bytes of NISTP256 curve parameters including the prepended length word. More... | |
Variables | |
| const ECC_NISTP256_Param | ECC_NISTP256_generatorX |
| X coordinate of the generator point of the ECC_NISTP256 curve. More... | |
| const ECC_NISTP256_Param | ECC_NISTP256_generatorY |
| Y coordinate of the generator point of the ECC_NISTP256 curve. More... | |
| const ECC_NISTP256_Param | ECC_NISTP256_prime |
| Prime of the generator point of the ECC_NISTP256 curve. More... | |
| const ECC_NISTP256_Param | ECC_NISTP256_a |
| 'a' constant of the ECC_NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More... | |
| const ECC_NISTP256_Param | ECC_NISTP256_b |
| 'b' constant of the ECC_NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b). More... | |
| const ECC_NISTP256_Param | ECC_NISTP256_order |
| Order of the generator point of the ECC_NISTP256 curve. More... | |
| const ECC_NISTP256_Param | ECC_NISTP256_k_mont |
| 'k' in Montgomery domain of the ECC_NISTP256 curve. More... | |
| const ECC_NISTP256_Param | ECC_NISTP256_a_mont |
| 'a' in Montgomery domain of the ECC_NISTP256 curve. More... | |
| const ECC_NISTP256_Param | ECC_NISTP256_b_mont |
| 'b' in Montgomery domain of the ECC_NISTP256 curve. More... | |
Note: CC26X1 uses NIST P256 curve params defined in driverlib/rom_ecc.h
| #define ECCParams_NISTP256_LENGTH 32 |
Length of NIST P256 curve parameters in bytes.
| #define ECC_NISTP256_PARAM_LENGTH_WITH_PREFIX_BYTES (ECCParams_NISTP256_LENGTH + ECC_LENGTH_PREFIX_BYTES) |
Length in bytes of NISTP256 curve parameters including the prepended length word.
| const ECC_NISTP256_Param ECC_NISTP256_generatorX |
X coordinate of the generator point of the ECC_NISTP256 curve.
| const ECC_NISTP256_Param ECC_NISTP256_generatorY |
Y coordinate of the generator point of the ECC_NISTP256 curve.
| const ECC_NISTP256_Param ECC_NISTP256_prime |
Prime of the generator point of the ECC_NISTP256 curve.
| const ECC_NISTP256_Param ECC_NISTP256_a |
'a' constant of the ECC_NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b).
| const ECC_NISTP256_Param ECC_NISTP256_b |
'b' constant of the ECC_NISTP256 curve when expressed in short Weierstrass form (y^3 = x^2 + a*x + b).
| const ECC_NISTP256_Param ECC_NISTP256_order |
Order of the generator point of the ECC_NISTP256 curve.
| const ECC_NISTP256_Param ECC_NISTP256_k_mont |
'k' in Montgomery domain of the ECC_NISTP256 curve.
| const ECC_NISTP256_Param ECC_NISTP256_a_mont |
'a' in Montgomery domain of the ECC_NISTP256 curve.
| const ECC_NISTP256_Param ECC_NISTP256_b_mont |
'b' in Montgomery domain of the ECC_NISTP256 curve.