Project Zero

Table of Contents

Introduction

The project_zero project implements a simple Bluetooth low energy peripheral device with GATT services and demonstrates how to integrate Over the Air Download and three custom services. This project can be a framework for developing many different peripheral-role applications.

This project has the following app configurations available:

App Build Configuration Description
FlashROM_Release (default) All TI-RTOS debug features disabled but application-logging to UART remains enabled.
The application uses the config file ble_release.cfg and the defines are in <app name>_FlashROM_Release.opt.
FlashROM_Debug All TI-RTOS debug features enabled.
The application uses the config file ble_debug.cfg and the defines are in <app name>_FlashROM_Debug.opt.

All application configurations use the stack library configuration, FlashROM_Library. This build configuration will yield additional flash footprint optimizations by the linker since the application and stack can share contiguous flash pages. This configuration is further discussed in the Stack Library Configuration section of the BLE5-Stack User's Guide provided in the SDK.

OAD feature can be disabled by adding the 'EXCLUDE_OAD' flag to the project. The OAD feature is not supported on CC1354P10 platforms, so the 'EXCLUDE_OAD' flag is defined by default on the related projects.

Note on the Boot Image Manager
If "EXCLUDE_OAD" is not defined, This project is configured to be managed and launched by the BIM or Boot Image Manager example app. This means that this project does not include a CCFG section to configure the device at boot, and therefore requires that the BIM project is programmed into the device first.

The application supports secure OAD i.e. Image authentication needs to be done before executing the newly transferred image. This is done by the BIM example app. A security header is added to this application image in order to support this.

If BIM is not present in the device internal Flash, the project can usually be started from the IDE but will not be executed after a pin reset. Read more about BIM and OAD in the BLE5-Stack User's Guide.

Hardware Prerequisites

The default Project Zero board configuration uses the device's LaunchPad development kit. This hardware configuration is shown in the below image:

For custom hardware, see the Running the SDK on Custom Boards section of the BLE5-Stack User's Guide.

Software Prerequisites

For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the Release Notes file provided in the SDK. For information on how to import this project into your IDE workspace and build/run, please refer to the device's Platform section in the BLE5-Stack User's Guide.

Service/Profile Table

This project contains 3 services in addition to GAP, GATT, Device Information and OAD(if "EXCLUDE_OAD" is not defined).

LED Service

This service exposes two readable and writable characteristics, LED0 and LED1 which both expect 1 byte of data. Writing 0 to either of the characteristic value attributes will turn off the corresponding LED on the Launchpad. Writing anything other than 0 will turn the LED on.

Description UUID Format Properties
LED Service F0001110-0451-4000-B000-000000000000 Service declaration Read
LED0 State F0001111-0451-4000-B000-000000000000 1 byte uint8_t Read/Write
LED1 State F0001112-0451-4000-B000-000000000000 1 byte uint8_t Read/Write

Button Service

This service exposes to readable and notifiable characteristics, BUTTON0 and BUTTON1 which correspond to the hardware switches BTN-1 and BTN-2 respectively. The state of each is updated when the hardware switch is pressed, and this can be read out via BLE. If notifications are enabled on these characteristics the button states will be sent out as notifications.

Description UUID Format Properties
Button Service F0001120-0451-4000-B000-000000000000 Service declaration Read
BUTTON0 State F0001121-0451-4000-B000-000000000000 1 byte uint8_t Read/Notify
BUTTON1 State F0001122-0451-4000-B000-000000000000 1 byte uint8_t Read/Notify

Data Service

This service exposes a long (longer than legacy MTU size) characteristic String char and a characteristic that is meant to exemplify streaming, Stream char. In order to read the entire contents of String char, a client must either have negotiated a longer MTU size than the default 27 bytes, or must use the GATT Long Read procedure.

Description UUID Format Properties
Data Service F0001130-0451-4000-B000-000000000000 Service declaration Read
String char F0001131-0451-4000-B000-000000000000 Up to 40 byte uint8_t Read/Write/WriteNoRsp
Stream char F0001132-0451-4000-B000-000000000000 Up to 20 byte uint8_t WriteNoRsp/Notify

Usage

This application uses the UART peripheral to provide an interface for the application. The UART is only used for display messages.

We recommend that you use a terminal program that can parse ANSI/VT100 color codes such Tera Term, PuTTY, Code Composer Studio Terminal, etc. to to monitor the LaunchPad UART output.

To interact with the application over Bluetooth you may use any device that is able to act as a BLE Central device, such as

Please see the Readme for simple_peripheral for an example of how to connect with a smartphone.

The following default parameters are used for the UART peripheral for display:

UART Param Default Values
Baud Rate 115200
Data length 8 bits
Parity None
Stop bits 1 bit
Flow Control None

Booting

Once the Project Zero sample application starts, the output to the terminal will report its address and the fact that it is advertising, as shown below:

The following section is relevant when "EXCLUDE_OAD" is not defined.

During boot/application init some activities related to Boot Image Mananger (BIM) and the external flash also take place:

After application init both buttons will operate normally. If the buttons are released during the 5 second timeout, the device will continue booting normally.

NOTE: After erasing the external flash it is not recommended to perform the BTN-1 + Reset revert procedure as this leave the Boot Image Manager with no valid image in internal Flash and no factory image in external Flash. At this point a debugger like the on-board XDS110 must be used to download a new internal image to the device. Pressing only Reset after erasing external Flash will invoke the OAD_open self-backup functionality on boot and revert will function normally again.

Connecting

When a device connects, the address of the device will be shown in the console. After a while you will see the automatic parameter update request sent from the device being applied.