Stack Configurations¶
Most projects are using SysConfig to configure the BLE-Stack. See Checking if SysConfig is used for BLE for steps on how to check if SysConfig is enabled for BLE. Based on the selected SysConfig settings, only the necessary precompiled libraries will be linked to the project.
Caution
Note that the following section applies only to example applications that are not configuring the BLE-Stack via SysConfig. For information about configuring the BLE-Stack with SysConfig see BLE5-Stack SysConfig Features.
Configuring Bluetooth Low Energy Protocol Stack Features¶
The Bluetooth Low Energy protocol stack can be configured to include
or exclude certain Bluetooth Low Energy features by changing the
library configuration. The available Bluetooth
Low Energy features are defined in the build_config.opt file in
the Tools folder of the stack project within the IDE. Based on the features
selected in the build_config.opt file, the respective precompiled libraries
will be selected during the build process of the stack project.
Run-Time Bluetooth Low Energy Protocol Stack Configuration¶
The Bluetooth Low Energy protocol stack can be configured with
various parameters that control its runtime behavior and RF antenna
layout. The available configuration parameters are described in
the ble_user_config.h file in the ICallBLE IDE folder of the
application. During initialization, these parameters are supplied to the
Bluetooth Low Energy protocol stack by the user0Cfg structure, declared in
main.c.
#include "ble_user_config.h"
// BLE user defined configuration
bleUserCfg_t user0Cfg = BLE_USER_CFG;
Because the ble_user_config.h file is shared filed between the Bluetooth
Low Energy projects within the SDK, TI recommends defining configuration
parameters in the .opt files found under TOOLS\defines. The .opt
files contain preprocessor symbols of the application when the default value
isn’t sufficient. For example, to change the maximum PDU size from the default
27 to 162, set the preprocessor symbol MAX_PDU_SIZE=162 in the
preprocessor symbols for the application project. Increasing certain
parameters may increase heap memory use by the protocol stack;
adjust the HEAPMGR_SIZE as required (if not using auto sized heap).
Table 21. and Table 22.
list the available configuration parameters.
Configurable? |
Define |
Description |
|---|---|---|
Y |
BOARD_DISPLAY_USE_LCD |
0 or 1 determines if the Display driver should use LCD |
Y |
BOARD_DISPLAY_USE_UART |
0 or 1 determines if the Display driver should use UART |
Y |
BOARD_DISPLAY_USE_UART_ANSI |
0 or 1 determines if the Display driver should use UART ANSI |
N |
CC26X2 |
This selects the chipset |
Y |
CC26X2R1_LAUNCHXL |
This define may be changed when migrating to a custom development board |
N |
CC26XX |
This selects the chipset |
N |
DeviceFamily_CC26X2 |
This selects the chipset |
Y |
Display_DISABLE_ALL |
If set, the Display module will be disabled. |
Y |
EXT_HAL_ASSERT |
Defining this assert will forward ble5stack asserts to the application |
Y |
EXTENDED_STACK_SETTINGS |
Bitmask of extended stack settings that are passed to the stack via ble_user_config. Options are defined in build_components.opt. |
Y |
HEAPMGR_METRICS |
Defining this will enable heap profiling. |
N |
ICALL_EVENTS |
This define is used with ICALL - do not modify |
N |
ICALL_JT |
This define is used with ICALL - do not modify |
N |
ICALL_LITE |
This define is used with ICALL - do not modify |
Y |
ICALL_MAX_NUM_ENTITIES |
This Maximum number of entities that use ICall, including service entities and application entities. |
Y |
ICALL_MAX_NUM_TASKS |
Defines the max number of ICall enabled tasks. Must be the same as OSAL_MAX_NUM_PROXY_TASKS + 1. Default is 2. |
Y |
L2CAP_NUM_CO_CHANNELS |
Maximum number of L2CAP Connection-Oriented (CO) Channels. Default is 3. |
Y |
L2CAP_NUM_PSM |
Maximum number of L2CAP Protocol/Service Multiplexers (PSM). Default is 3. |
Y |
MAX_NUM_BLE_CONNS |
This is the maximum number of simultaneous Bluetooth Low Energy collections allowed. Adding more connections uses more RAM and may require increasing HEAPMGR_SIZE. Profile heap usage accordingly |
Y |
MAX_NUM_PDU |
Maximum number of Bluetooth Low Energy HCI PDUs. Default is 5. If the maximum number of connections is set to 0, then this number should also be set to 0. |
Y |
MAX_PDU_SIZE |
Maximum size in bytes of the Bluetooth Low Energy HCI PDU. Default is 27. Valid range is 27 to 255. The maximum ATT_MTU is MAX_PDU_SIZE - 4. See Configuring for Larger MTU Values. |
Y |
NPI_SPI_CONFIG |
When NPI_USE_API is defined, this will allows you to choose which SPI driver instance NPI will be used. |
Y |
NPI_USE_SPI |
Configure NPI to use SPI. Do not define NPI_USE_UART and NPI_USE_SPI at the same time. |
Y |
NPI_USE_UART |
Configure NPI to use UART. Do not define NPI_USE_SPI and NPI_USE_UART at the same time. |
Y |
PM_STARTUP_MARGIN |
Defines time in microseconds (us) the system will wake up before the start of the connection event. Default is 300. This value is optimized for the example projects. |
Y |
POWER_SAVING |
Power management is enabled when defined, and disabled when not defined. Requires same option in stack project |
Y |
PTM_MODE |
Define this will enable PTM mode. |
Y |
SC_HOST_DEBUG |
Define this will make the LE Secure Connection use the debug keys specified by the Bluetooth Core Specification, therefore it’s easy to decrypt the link and follow the over the air traffic. |
N |
STACK_LIBRARY |
Build/Use the build configuration where the stack is built as a library |
Y |
TBM_ACTIVE_ITEMS_ONLY |
When using the Two Button Menu, Only active items will be displayed |
N |
USE_ICALL |
This define is used with ICALL - do not modify |
Y |
USE_RCOSC |
This define will make the software to operate the CC13xx or CC26xx in a 32kHz crystal-less mode. |
Configurable? |
Define |
Description |
|---|---|---|
Y |
ATT_DELAYED_REQ |
Allows to reply to a Read Att Request at a later stage, if the request cannot be processed when received (see also Delaying an ATT Read Request) |
Y |
BROADCASTER_CFG |
Used to include the GAP Broadcaster Role support |
N |
CC26X2 |
This selects the chipset |
N |
CC26XX |
This selects the chipset |
Y |
CENTRAL_CFG |
Used to include the GAP Central Role support |
N |
DeviceFamily_CC26X2 |
This selects the chipset |
Y |
EXT_HAL_ASSERT |
Defining this assert will forward ble5stack asserts to the application |
Y |
GATT_NO_CLIENT |
Should only be done for devices that do not wish to discover the RPAO characteristic |
Y |
GATT_NO_SERVICE_CHANGED |
Used to exclude service changed characteristic from GATT Service |
Y |
HEAPMGR_METRICS |
Defining this will enable heap profiling. |
N |
ICALL_EVENTS |
This define is used with ICALL - do not modify |
N |
ICALL_JT |
This define is used with ICALL - do not modify |
N |
ICALL_LITE |
This define is used with ICALL - do not modify |
N |
ICALL_STACK0_ADDR |
This define is used with ICALL - do not modify |
Y |
L2CAP_COC_CFG |
Enable L2CAP Connection Oriented Channels |
Y |
OBSERVER_CFG |
Used to include the GAP Observer Role support |
Y |
PERIPHERAL_CFG |
Used to include the GAP Peripheral Role support |
Y |
POWER_SAVING |
Used to allow the device to go to standby |
N |
STACK_LIBRARY |
Build/Use the build configuration where the stack is built as a library |
Y |
USE_DMM |
Required if DMM functionalities are used |
N |
USE_ICALL |
This define is used with ICALL - do not modify |
Y |
USE_RTLS |
Required if RTLS functionalities are used |
Y |
RTLS_CTE |
Required if RTLS functionalities are used |
Y |
RTLS_CTE_TEST |
Required if RTLS test mode functionalities are used |
Y |
USE_PERIODIC_ADV |
Required to send periodic advertisements |
Y |
USE_PERIODIC_SCAN |
Required to synchronize with periodic advertisements |
N |
SYSCFG |
Set when BLE module is added in the sysconfig |
Y |
NPI_FLOW_CTRL |
Defining this will enable NPI flow control |
Y |
USE_COEX |
Defining this will enable coexistence |
Y |
GAP_BOND_MGR |
Defining this will enable Gap Bond Manager |
N |
OSAL_CBTIMER_NUM_TASKS |
Internal symbol - do not modify |
N |
ONE_BLE_LIB_SIZE_OPTIMIZATION |
Internal symbol - do not modify |
N |
HCI_TL_NONE |
Internal symbol - do not modify |
N |
HOST_CONFIG |
Internal symbol - do not modify |