Instance: DDI_0_OSC
Component: DDI_0_OSC
Base address: 0x400CA000
This is the DDI for the digital block that controls all the analog clock oscillators (OSC_DIG) and performs qualification of the clocks generated.
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x400C A000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x400C A004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0x400C A008 |
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0x400C A00C |
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0x400C A010 |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0x400C A014 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0x400C A018 |
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0x400C A01C |
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0x400C A020 |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x400C A024 |
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0x400C A028 |
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0x400C A02C |
|
RW |
32 |
0x0000 0000 |
0x0000 0030 |
0x400C A030 |
|
RW |
32 |
0x0000 0000 |
0x0000 0034 |
0x400C A034 |
|
RO |
32 |
0x0000 0000 |
0x0000 003C |
0x400C A03C |
|
RO |
32 |
0x0000 0000 |
0x0000 0040 |
0x400C A040 |
|
RO |
32 |
0x0000 0000 |
0x0000 0044 |
0x400C A044 |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x400C A000 | Instance | 0x400C A000 |
Description | Control 0 Controls clock source selects |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31 | XTAL_IS_24M | Set based on the accurate high frequency XTAL.
|
RW | 0 | |||||||||||||||||
30 | RESERVED30 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | |||||||||||||||||
29 | BYPASS_XOSC_LF_CLK_QUAL | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
28 | BYPASS_RCOSC_LF_CLK_QUAL | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
27:26 | DOUBLER_START_DURATION | Internal. Only to be used through TI provided API. | RW | 0b00 | |||||||||||||||||
25 | DOUBLER_RESET_DURATION | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
24 | CLK_DCDC_SRC_SEL | Select DCDC clock source. 0: CLK_DCDC is 48 MHz clock from RCOSC or XOSC / HPOSC 1: CLK_DCDC is always 48 MHz clock from RCOSC |
RW | 0 | |||||||||||||||||
23:15 | RESERVED15 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 0000 | |||||||||||||||||
14 | HPOSC_MODE_EN | 0: HPOSC mode is not enabled. The 48 MHz crystal is required for radio operation. 1: Enables HPOSC mode. The internal HPOSC can be used as HF system clock and for radio operation. |
RW | 0 | |||||||||||||||||
13 | RESERVED13 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | |||||||||||||||||
12 | RCOSC_LF_TRIMMED | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
11 | XOSC_HF_POWER_MODE | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
10 | XOSC_LF_DIG_BYPASS | Bypass XOSC_LF and use the digital input clock from AON for the xosc_lf clock. 0: Use 32kHz XOSC as xosc_lf clock source 1: Use digital input (from AON) as xosc_lf clock source. This bit will only have effect when SCLK_LF_SRC_SEL is selecting the xosc_lf as the sclk_lf source. The muxing performed by this bit is not glitch free. The following procedure must be followed when changing this field to avoid glitches on sclk_lf. 1) Set SCLK_LF_SRC_SEL to select any source other than the xosc_lf clock source. 2) Set or clear this bit to bypass or not bypass the xosc_lf. 3) Set SCLK_LF_SRC_SEL to use xosc_lf. It is recommended that either the rcosc_hf or xosc_hf (whichever is currently active) be selected as the source in step 1 above. This provides a faster clock change. |
RW | 0 | |||||||||||||||||
9 | CLK_LOSS_EN | Enable clock loss detection and hence the indicators to the system controller. Checks both SCLK_HF, SCLK_MF and SCLK_LF clock loss indicators. 0: Disable 1: Enable Clock loss detection must be disabled when changing the sclk_lf source. STAT0.SCLK_LF_SRC can be polled to determine when a change to a new sclk_lf source has completed. |
RW | 0 | |||||||||||||||||
8:7 | ACLK_TDC_SRC_SEL | Source select for aclk_tdc. 00: RCOSC_HF (48MHz) 01: RCOSC_HF (24MHz) 10: XOSC_HF (24MHz) 11: Not used |
RW | 0b00 | |||||||||||||||||
6:4 | ACLK_REF_SRC_SEL | Source select for aclk_ref 000: RCOSC_HF derived (31.25kHz) 001: XOSC_HF derived (31.25kHz) 010: RCOSC_LF (32kHz) 011: XOSC_LF (32.768kHz) 100: RCOSC_MF (2MHz) 101-111: Not used |
RW | 0b000 | |||||||||||||||||
3:2 | SCLK_LF_SRC_SEL | Source select for sclk_lf
|
RW | 0b00 | |||||||||||||||||
1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | |||||||||||||||||
0 | SCLK_HF_SRC_SEL | Source select for sclk_hf.
|
RW | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x400C A004 | Instance | 0x400C A004 |
Description | Control 1 This register contains OSC_DIG configuration |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:23 | RESERVED23 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 0000 | ||
22:18 | RCOSCHFCTRIMFRACT | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | ||
17 | RCOSCHFCTRIMFRACT_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
16:2 | SPARE2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b000 0000 0000 0000 | ||
1:0 | XOSC_HF_FAST_START | Internal. Only to be used through TI provided API. | RW | 0b00 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x400C A008 | Instance | 0x400C A008 |
Description | RADC External Configuration | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:22 | HPM_IBIAS_WAIT_CNT | Internal. Only to be used through TI provided API. | RW | 0b00 0000 0000 | ||
21:16 | LPM_IBIAS_WAIT_CNT | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
15:12 | IDAC_STEP | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
11:6 | RADC_DAC_TH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
5 | RADC_MODE_IS_SAR | Internal. Only to be used through TI provided API. | RW | 0 | ||
4:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 |
Address Offset | 0x0000 000C | ||
Physical Address | 0x400C A00C | Instance | 0x400C A00C |
Description | Amplitude Compensation Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31 | SPARE31 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | |||||||||||||||||
30 | AMPCOMP_REQ_MODE | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
29:28 | AMPCOMP_FSM_UPDATE_RATE | Internal. Only to be used through TI provided API.
|
RW | 0b00 | |||||||||||||||||
27 | AMPCOMP_SW_CTRL | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
26 | AMPCOMP_SW_EN | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
25:24 | RESERVED24 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | |||||||||||||||||
23:20 | IBIAS_OFFSET | Internal. Only to be used through TI provided API. | RW | 0x0 | |||||||||||||||||
19:16 | IBIAS_INIT | Internal. Only to be used through TI provided API. | RW | 0x0 | |||||||||||||||||
15:8 | LPM_IBIAS_WAIT_CNT_FINAL | Internal. Only to be used through TI provided API. | RW | 0x00 | |||||||||||||||||
7:4 | CAP_STEP | Internal. Only to be used through TI provided API. | RW | 0x0 | |||||||||||||||||
3:0 | IBIASCAP_HPTOLP_OL_CNT | Internal. Only to be used through TI provided API. | RW | 0x0 |
Address Offset | 0x0000 0010 | ||
Physical Address | 0x400C A010 | Instance | 0x400C A010 |
Description | Amplitude Compensation Threshold 1 This register contains threshold values for amplitude compensation algorithm |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:24 | SPARE24 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 | ||
23:18 | HPMRAMP3_LTH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
17:16 | SPARE16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
15:10 | HPMRAMP3_HTH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
9:6 | IBIASCAP_LPTOHP_OL_CNT | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
5:0 | HPMRAMP1_TH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0x400C A014 | Instance | 0x400C A014 |
Description | Amplitude Compensation Threshold 2 This register contains threshold values for amplitude compensation algorithm. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:26 | LPMUPDATE_LTH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
25:24 | SPARE24 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
23:18 | LPMUPDATE_HTH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
17:16 | SPARE16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
15:10 | ADC_COMP_AMPTH_LPM | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
9:8 | SPARE8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
7:2 | ADC_COMP_AMPTH_HPM | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
1:0 | SPARE0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0x400C A018 | Instance | 0x400C A018 |
Description | Analog Bypass Values 1 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:20 | RESERVED20 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x000 | ||
19:16 | XOSC_HF_ROW_Q12 | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
15:0 | XOSC_HF_COLUMN_Q12 | Internal. Only to be used through TI provided API. | RW | 0x0000 |
Address Offset | 0x0000 001C | ||
Physical Address | 0x400C A01C | Instance | 0x400C A01C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:14 | RESERVED14 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 0000 0000 0000 | ||
13:0 | XOSC_HF_IBIASTHERM | Internal. Only to be used through TI provided API. | RW | 0b00 0000 0000 0000 |
Address Offset | 0x0000 0020 | ||
Physical Address | 0x400C A020 | Instance | 0x400C A020 |
Description | Analog Test Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31 | SCLK_LF_AUX_EN | Enable 32 kHz clock to AUX_COMPB. | RW | 0 | ||
30:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b000 0000 0000 0000 | ||
15:14 | TEST_RCOSCMF | Test mode control for RCOSC_MF 0x0: test modes disabled 0x1: boosted bias current into self biased inverter 0x2: clock qualification disabled 0x3: boosted bias current into self biased inverter + clock qualification disabled |
RW | 0b00 | ||
13:12 | ATEST_RCOSCMF | ATEST control for RCOSC_MF 0x0: ATEST disabled 0x1: ATEST enabled, VDD_LOCAL connected, ATEST internal to **RCOSC_MF* enabled to send out 2MHz clock. 0x2: ATEST disabled 0x3: ATEST enabled, bias current connected, ATEST internal to **RCOSC_MF* enabled to send out 2MHz clock. |
RW | 0b00 | ||
11:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x000 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0x400C A024 | Instance | 0x400C A024 |
Description | ADC Doubler Nanoamp Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b000 0000 | ||
24 | NANOAMP_BIAS_ENABLE | Internal. Only to be used through TI provided API. | RW | 0 | ||
23 | SPARE23 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior | RW | 0 | ||
22:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 0000 0000 0000 | ||
5 | ADC_SH_MODE_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
4 | ADC_SH_VBUF_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
1:0 | ADC_IREF_CTRL | Internal. Only to be used through TI provided API. | RW | 0b00 |
Address Offset | 0x0000 0028 | ||
Physical Address | 0x400C A028 | Instance | 0x400C A028 |
Description | XOSCHF Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:14 | SPARE14 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 0000 0000 0000 | ||
13 | TCXO_MODE_XOSC_HF_EN | If this register is 1 when TCXO_MODE is 1, then the XOSC_HF is enabled, turning on the XOSC_HF bias current allowing a DC bias point to be provided to the clipped-sine wave clock signal on external input. | RW | 0 | ||
12 | TCXO_MODE | If this register is 1 when BYPASS is 1, this will enable clock qualification on the TCXO clock on external input. This register has no effect when BYPASS is 0. | RW | 0 | ||
11:10 | RESERVED10 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
9:8 | PEAK_DET_ITRIM | Internal. Only to be used through TI provided API. | RW | 0b00 | ||
7 | RESERVED7 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
6 | BYPASS | Internal. Only to be used through TI provided API. | RW | 0 | ||
5 | RESERVED5 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
4:2 | HP_BUF_ITRIM | Internal. Only to be used through TI provided API. | RW | 0b000 | ||
1:0 | LP_BUF_ITRIM | Internal. Only to be used through TI provided API. | RW | 0b00 |
Address Offset | 0x0000 002C | ||
Physical Address | 0x400C A02C | Instance | 0x400C A02C |
Description | Low Frequency Oscillator Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31:24 | RESERVED24 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 | |||||||||||||||||
23:22 | XOSCLF_REGULATOR_TRIM | Internal. Only to be used through TI provided API. | RW | 0b00 | |||||||||||||||||
21:18 | XOSCLF_CMIRRWR_RATIO | Internal. Only to be used through TI provided API. | RW | 0x0 | |||||||||||||||||
17:10 | RESERVED10 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 | |||||||||||||||||
9:8 | RCOSCLF_RTUNE_TRIM | Internal. Only to be used through TI provided API.
|
RW | 0b00 | |||||||||||||||||
7:0 | RCOSCLF_CTUNE_TRIM | Internal. Only to be used through TI provided API. | RW | 0x00 |
Address Offset | 0x0000 0030 | ||
Physical Address | 0x400C A030 | Instance | 0x400C A030 |
Description | RCOSCHF Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x0000 | ||
15:8 | RCOSCHF_CTRIM | Internal. Only to be used through TI provided API. | RW | 0x00 | ||
7:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 |
Address Offset | 0x0000 0034 | ||
Physical Address | 0x400C A034 | Instance | 0x400C A034 |
Description | RCOSC_MF Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:16 | SPARE16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x0000 | ||
15:9 | RCOSC_MF_CAP_ARRAY | Adjust RCOSC_MF capacitor array. 0x0: nominal frequency, 0.625pF 0x40: highest frequency, 0.125pF 0x3F: lowest frequency, 1.125pF |
RW | 0b000 0000 | ||
8 | RCOSC_MF_REG_SEL | Choose regulator type. 0: default 1: alternate |
RW | 0 | ||
7:6 | RCOSC_MF_RES_COARSE | Select coarse resistor for frequency adjustment. 0x0: 400kohms, default 0x1: 300kohms, min 0x2: 600kohms, max 0x3: 500kohms |
RW | 0b00 | ||
5:4 | RCOSC_MF_RES_FINE | Select fine resistor for frequency adjustment. 0x0: 11kohms, minimum resistance, max freq 0x1: 13kohms 0x2: 16kohms 0x3: 20kohms, max resistance, min freq |
RW | 0b00 | ||
3:0 | RCOSC_MF_BIAS_ADJ | Adjusts bias current to RCOSC_MF. 0x8 minimum current 0x0 default current 0x7 maximum current |
RW | 0x0 |
Address Offset | 0x0000 003C | ||
Physical Address | 0x400C A03C | Instance | 0x400C A03C |
Description | Status 0 This register contains status signals from OSC_DIG |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31 | SPARE31 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | |||||||||||||||||
30:29 | SCLK_LF_SRC | Indicates source for the sclk_lf
|
RO | 0b00 | |||||||||||||||||
28 | SCLK_HF_SRC | Indicates source for the sclk_hf
|
RO | 0 | |||||||||||||||||
27:23 | RESERVED23 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 | |||||||||||||||||
22 | RCOSC_HF_EN | RCOSC_HF_EN | RO | 0 | |||||||||||||||||
21 | RCOSC_LF_EN | RCOSC_LF_EN | RO | 0 | |||||||||||||||||
20 | XOSC_LF_EN | XOSC_LF_EN | RO | 0 | |||||||||||||||||
19 | CLK_DCDC_RDY | CLK_DCDC_RDY | RO | 0 | |||||||||||||||||
18 | CLK_DCDC_RDY_ACK | CLK_DCDC_RDY_ACK | RO | 0 | |||||||||||||||||
17 | SCLK_HF_LOSS | Indicates sclk_hf is lost | RO | 0 | |||||||||||||||||
16 | SCLK_LF_LOSS | Indicates sclk_lf is lost | RO | 0 | |||||||||||||||||
15 | XOSC_HF_EN | Indicates that XOSC_HF is enabled. | RO | 0 | |||||||||||||||||
14 | RESERVED14 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | |||||||||||||||||
13 | XB_48M_CLK_EN | Indicates that the 48MHz clock from the DOUBLER is enabled. It will be enabled if 24 or 48 MHz crystal is used (enabled in doubler bypass for the 48MHz crystal). |
RO | 0 | |||||||||||||||||
12 | RESERVED12 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | |||||||||||||||||
11 | XOSC_HF_LP_BUF_EN | XOSC_HF_LP_BUF_EN | RO | 0 | |||||||||||||||||
10 | XOSC_HF_HP_BUF_EN | XOSC_HF_HP_BUF_EN | RO | 0 | |||||||||||||||||
9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | |||||||||||||||||
8 | ADC_THMET | ADC_THMET | RO | 0 | |||||||||||||||||
7 | ADC_DATA_READY | indicates when adc_data is ready. | RO | 0 | |||||||||||||||||
6:1 | ADC_DATA | adc_data | RO | 0b00 0000 | |||||||||||||||||
0 | PENDINGSCLKHFSWITCHING | Indicates when SCLK_HF clock source is ready to be switched | RO | 0 |
Address Offset | 0x0000 0040 | ||
Physical Address | 0x400C A040 | Instance | 0x400C A040 |
Description | Status 1 This register contains status signals from OSC_DIG |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||||||||||||||||||||
31:28 | RAMPSTATE | AMPCOMP FSM State
|
RO | 0x0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
27:22 | HPM_UPDATE_AMP | XOSC_HF amplitude during HPM_UPDATE state. When amplitude compensation of XOSC_HF is enabled in high performance mode, this value is the amplitude of the crystal oscillations measured by the on-chip oscillator ADC, divided by 15 mV. For example, a value of 0x20 would indicate that the amplitude of the crystal is approximately 480 mV. To enable amplitude compensation, AON_WUC OSCCFG must be set to a non-zero value. |
RO | 0b00 0000 | ||||||||||||||||||||||||||||||||||||||||||||||||||
21:16 | LPM_UPDATE_AMP | XOSC_HF amplitude during LPM_UPDATE state When amplitude compensation of XOSC_HF is enabled in low power mode, this value is the amplitude of the crystal oscillations measured by the on-chip oscillator ADC, divided by 15 mV. For example, a value of 0x20 would indicate that the amplitude of the crystal is approximately 480 mV. To enable amplitude compensation, AON_WUC OSCCFG must be set to a non-zero value. |
RO | 0b00 0000 | ||||||||||||||||||||||||||||||||||||||||||||||||||
15 | FORCE_RCOSC_HF | force_rcosc_hf | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
14 | SCLK_HF_EN | SCLK_HF_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
13 | SCLK_MF_EN | SCLK_MF_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
12 | ACLK_ADC_EN | ACLK_ADC_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
11 | ACLK_TDC_EN | ACLK_TDC_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
10 | ACLK_REF_EN | ACLK_REF_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
9 | CLK_CHP_EN | CLK_CHP_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
8 | CLK_DCDC_EN | CLK_DCDC_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
7 | SCLK_HF_GOOD | SCLK_HF_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
6 | SCLK_MF_GOOD | SCLK_MF_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
5 | SCLK_LF_GOOD | SCLK_LF_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
4 | ACLK_ADC_GOOD | ACLK_ADC_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
3 | ACLK_TDC_GOOD | ACLK_TDC_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
2 | ACLK_REF_GOOD | ACLK_REF_GOOD. | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
1 | CLK_CHP_GOOD | CLK_CHP_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
0 | CLK_DCDC_GOOD | CLK_DCDC_GOOD | RO | 0 |
Address Offset | 0x0000 0044 | ||
Physical Address | 0x400C A044 | Instance | 0x400C A044 |
Description | Status 2 This register contains status signals from AMPCOMP FSM |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:26 | ADC_DCBIAS | DC Bias read by RADC during SAR mode The value is an unsigned integer. It is used for debug only. |
RO | 0b00 0000 | ||
25 | HPM_RAMP1_THMET | Indication of threshold is met for hpm_ramp1 | RO | 0 | ||
24 | HPM_RAMP2_THMET | Indication of threshold is met for hpm_ramp2 | RO | 0 | ||
23 | HPM_RAMP3_THMET | Indication of threshold is met for hpm_ramp3 | RO | 0 | ||
22:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
15:12 | RAMPSTATE | xosc_hf amplitude compensation FSM This is identical to STAT1.RAMPSTATE. See that description for encoding. |
RO | 0x0 | ||
11:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 | ||
3 | AMPCOMP_REQ | ampcomp_req | RO | 0 | ||
2 | XOSC_HF_AMPGOOD | amplitude of xosc_hf is within the required threshold (set by DDI). Not used for anything just for debug/status | RO | 0 | ||
1 | XOSC_HF_FREQGOOD | frequency of xosc_hf is good to use for the digital clocks | RO | 0 | ||
0 | XOSC_HF_RF_FREQGOOD | frequency of xosc_hf is within +/- 20 ppm and xosc_hf is good for radio operations. Used for SW to start synthesizer. | RO | 0 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |