Data Structures
ECDSACC26X1.h File Reference

Detailed Description

ECDSA driver implementation for the CC26X1 family.

============================================================================

This file should only be included in the board file to fill the ECDSA_config struct.

Hardware and Implementation Details

The driver is backed by a software ECC library implementation.

Supported Curves

The driver implementation supports the following curves for ECDSA:

Curves Supported
NISTP256
#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/ECDSA.h>
#include <ti/drivers/TRNG.h>
#include <ti/drivers/trng/TRNGCC26XX.h>
#include <ti/devices/DeviceFamily.h>
#include <DeviceFamily_constructPath(driverlib/rom_ecc.h)>
Include dependency graph for ECDSACC26X1.h:

Go to the source code of this file.

Data Structures

struct  ECDSACC26X1_HWAttrs
 ECDSACC26X1 Hardware Attributes. More...
 
struct  ECDSACC26X1_Object
 ECDSACC26X1 Object. More...
 
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale