180 #ifndef ti_drivers_watchdog_WatchdogCC26XX__include 181 #define ti_drivers_watchdog_WatchdogCC26XX__include HwiP structure.
Definition: HwiP.h:78
void(* Watchdog_Callback)(uintptr_t handle)
Watchdog callback pointer.
Definition: Watchdog.h:291
unsigned int baseAddr
Definition: WatchdogCC26XX.h:228
Watchdog driver interface.
Watchdog hardware attributes for CC26XX.
Definition: WatchdogCC26XX.h:226
Watchdog_Callback callbackFxn
Definition: WatchdogCC26XX.h:240
bool isOpen
Definition: WatchdogCC26XX.h:239
Watchdog_DebugMode
Watchdog debug stall settings.
Definition: Watchdog.h:264
Watchdog Object for CC26XX.
Definition: WatchdogCC26XX.h:237
unsigned long reloadValue
Definition: WatchdogCC26XX.h:229
Watchdog_ResetMode resetMode
Definition: WatchdogCC26XX.h:242
const Watchdog_FxnTable WatchdogCC26XX_fxnTable
Watchdog function table for CC26XX.
Watchdog_DebugMode debugStallMode
Definition: WatchdogCC26XX.h:244
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:360
Watchdog_ResetMode
Watchdog reset mode settings.
Definition: Watchdog.h:277
Hardware Interrupt module for the RTOS Porting Interface.
HwiP_Struct hwi
Definition: WatchdogCC26XX.h:247