rfOADClient
Project Setup using the System Configuration Tool (SysConfig)
The purpose of SysConfig is to provide an easy to use interface for configuring drivers, RF stacks, and more. The .syscfg file provided with each example project has been configured and tested for that project. Changes to the .syscfg file may alter the behavior of the example away from default. Some parameters configured in SysConfig may require the use of specific APIs or additional modifications in the application source code. More information can be found in SysConfig by hovering over a configurable and clicking the question mark (?) next to it's name.
Example Summary
The rfOADClient project, together with the rfOADServer project, illustrates how on-chip over-the-air download works with MCUBoot. The primary slot holds the main image that is run, while the secondary slot is used during the OAD process to temporarily store the new incoming image. This example works by receiving a firmware image from the OAD Server and placing it in the secondary slot. MCUBoot then copies this image into the primary slot, if needed. Upon reset, the new image is now in the primary slot and is run.
Peripherals Exercised
CONFIG_GPIO_GLED
- Toggled when data is transmitted over the RF interfaceCONFIG_GPIO_RLED
- Toggled when data is received over the RF interface
Board Specific Settings
- The default frequency is:
- 433.92 MHz for the CC1350-LAUNCHXL-433 and the CC1352P-4-LAUNCHXL
- 2440 MHz on the CC2640R2-LAUNCHXL and the CC26X2R1-LAUNCHXL
- 868.0 MHz for other launchpads In order to change frequency, modify the ti_radio_config.c file. This can be done using the code export feature in Smart RF Studio, or directly in the file
- On the CC1352P1 the high PA is enabled (high output power) for all Sub-1 GHz modes by default.
- On the CC1352P-2 and CC1352P-4 the high PA operation for Sub-1 GHz modes is not supported
- The CC2640R2 is setup to run all proprietary physical modes at a center frequency of 2440 MHz, at a data rate of 250 Kbps
Required Firmware Images
The rfOADClient example requires two firmware images to be flashed onto the client:
1. MCUBoot Image
* Project: <SDK_INSTALL_DIR>/examples/nortos/<PLATFORM>/mcuboot/mcuboot
* In CCS, after importing the MCUBoot project, modify <mcuboot_project>/flash_map_backend/flash_map_backend.h
to set the desired MCUBoot slot size. It is important that this matches the slot size set in rfOADClient image and in
the imgtool sign command. We recommend setting the slot size to the following values as a starting point:
#define BOOT_PRIMARY_1_SIZE 0x0000D000
#define BOOT_SECONDARY_1_SIZE 0x0000D000
* The slots' base addresses must also be set properly in <mcuboot_project>/flash_map_backend/flash_map_backend.h
depending on the target device family
* CC13x2x7_CC26x2x7
#define BOOT_PRIMARY_1_BASE_ADDRESS 0x00000000
#define BOOT_SECONDARY_1_BASE_ADDRESS 0x00056000
* CC13x4_CC26x4
#define BOOT_PRIMARY_1_BASE_ADDRESS 0x00006000
#define BOOT_SECONDARY_1_BASE_ADDRESS 0x00083000
NOTE: Refer to the Flash Layout section below for more details
* In MCUBoot project, modify <mcuboot_project>/mcuboot_config/mcuboot_config.h
to set MCUBoot's Upgrade Mode to overwrite only mode.
#define MCUBOOT_OVERWRITE_ONLY
// #define MCUBOOT_DIRECT_XIP
2. A Signed rfOADClient Image
* Modify <rfOADClient>/oad/native_oad/oad_config.h
to set the desired MCUBoot slot size. Make sure the value matches what is set in the MCUBoot project
#define MCUBOOT_SLOT_SIZE 0x0D000
* Run imgtool on the rfOADClient image that was built from this example. The imgtool tool will sign the image. Again, make sure the slot size matches
what is set in both MCUBoot project and rfOADClient project.
cd <SDK_INSTALL_DIR>/tools/common/mcuboot
Sign a version 1 of the image
./imgtool sign --header-size 0x20 --align 4 --slot-size 0xD000 --pad --version 1.0.0 --pad-header --key <SDK_INSTALL_DIR>/source/third_party/mcuboot/root-ec-p256.pem <CCS_WORKSPACE>\rfOADClient_<PLATFORM>_tirtos7_ticlang\Debug\rfOADClient_<PLATFORM>_tirtos7_ticlang.hex <CCS_WORKSPACE>\rfOADClient_<PLATFORM>_tirtos7_ticlang\Debug\rfOADClient_<PLATFORM>_tirtos7_ticlang_signed_v1.hex"
After your firmware updates, rebuild the project and sign a version 2 of the image
./imgtool sign --header-size 0x20 --align 4 --slot-size 0xD000 --pad --version 2.0.0 --pad-header --key <SDK_INSTALL_DIR>/source/third_party/mcuboot/root-ec-p256.pem <CCS_WORKSPACE>\rfOADClient_<PLATFORM>_tirtos7_ticlang\Debug\rfOADClient_<PLATFORM>_tirtos7_ticlang.hex <CCS_WORKSPACE>\rfOADClient_<PLATFORM>_tirtos7_ticlang\Debug\rfOADClient_<PLATFORM>_tirtos7_ticlang_signed_v2.hex"
NOTE: This is an example usage of the script. Refer to the ImgTool's README for more information.
Once you have MCUBoot and the signed rfOADClient v1 image, use Uniflash to load both images onto the target device.
Flash Layout
- CC13x2x7_CC26x2x7
+-----------------------+ 0x000B0000
| MCUBoot + CCFG |
| CCFG: 0xAFFA8-0xAFFFF |
+-----------------------+ 0x000AC000
| Padding |
+-----------------------+ BOOT_SECONDARY_1_BASE_ADDRESS + BOOT_SECONDARY_1_SIZE
| |
| |
| Secondary Slot |
| |
| |
+-----------------------+ BOOT_SECONDARY_1_BASE_ADDRESS
| Padding |
+-> +-----------------------+ BOOT_PRIMARY_1_SIZE
| | MCUBoot Trailer |
| +-----------------------+
| | Padding |
| +-----------------------+ Varies
| | |
Primary Slot | Client User App |
| | |
| +-----------------------+
| | OAD Header |
| +-----------------------+
| | Entry Section |
| +-----------------------+
| | MCUBoot Header |
+-> +-----------------------+ 0x00000000
- CC13x4_CC26x4
+-----------------------+ 0x50000800
| CCFG |
+-----------------------+ 0x50000000
| Padding/Holes |
+-----------------------+ BOOT_SECONDARY_1_BASE_ADDRESS + BOOT_SECONDARY_1_SIZE
| |
| |
| Secondary Slot |
| |
| |
+-----------------------+ BOOT_SECONDARY_1_BASE_ADDRESS
| Padding |
+-> +-----------------------+ BOOT_PRIMARY_1_SIZE + 0x00006000
| | MCUBoot Trailer |
| +-----------------------+
| | Padding |
| +-----------------------+ Varies
| | |
Primary Slot | Client User App |
| | |
| +-----------------------+
| | OAD Header |
| +-----------------------+
| | Entry Section |
| +-----------------------+
| | MCUBoot Header |
+-> +-----------------------+ 0x00006000
| Padding |
+-----------------------+ 0x00005800
| MCUBoot |
+-----------------------+ 0x00000000
Example Usage
Once the rfOADClient application starts up, it waits for OAD packets from the OAD Server. On another board then, run the OAD Server example. Refer to rfOADServer README for information on how to use it.
Application Design Details
Init
|
|
+---------> Wait for OAD/Radio Events
| |
| V
| Process OAD Client & Radio Events
| |
| V
| +-----------+----------+---------------------+------------------------+
| | | | |
| V V V V
| Block Rsp FW Version Req Img Identify Req Block Req
| | | | |
| | V V V
| | Send FW Version Send Img Identify Rsp Send Block Req
| | | | |
| V | | |
| Write Img Block | | |
| to Internal Flash | | |
| +---------------------+------------------------+
| |
| V
+-----> Packet RX Packet TX