![]() |
![]() |
|
Z-Stack API Reference
7.40.00.20
|
#include <zstack.h>
Data Fields | |
| bool | enable |
| bool | has_channel |
| uint8_t | channel |
| bool | has_endpoint |
| uint8_t | endpoint |
| bool | has_panID |
| uint16_t | panID |
Structure to send an AF Inter-PAN Control Request.
| uint8_t channel |
InterPan channel
| bool enable |
Set to turn on inter-PAN, Clear to switch back to NIB
| uint8_t endpoint |
Endpoint controller
| bool has_channel |
Rrue if channel is available, false if not
| bool has_endpoint |
True if endpoint is available, false if not
| bool has_panID |
True if panID is available, false if not
| uint16_t panID |
PAN ID