Z-Stack API Reference  7.40.00.20
_zstack_afregisterreq_t Struct Reference

#include <zstack.h>

Data Fields

uint8_t endpoint
 
zstack_SimpleDescriptor_tpSimpleDesc
 
zstack_NetworkLatency latencyReq
 

Detailed Description

Structure to send an AF Register Request.

Field Documentation

§ endpoint

uint8_t endpoint

The endpoint number 1-240 (0 is reserved). This is the subaddress of the node, and is used to receive data.

§ latencyReq

Network Latency Requirements: use zstack_NetworkLatency_NO_LATENCY_REQS

§ pSimpleDesc

Pointer to the Simple Descriptor structure


The documentation for this struct was generated from the following file: