Z-Stack API Reference  7.40.00.20
_zstack_bdbaddinstallcodereq_t Struct Reference

#include <zstack.h>

Data Fields

uint8_t pInstallCode [18]
 
uint8_t pExt [8]
 

Detailed Description

Structure to send a BDB Add Install Code Request.

Field Documentation

§ pExt

uint8_t pExt[8]

Extended address of the joining node

§ pInstallCode

uint8_t pInstallCode[18]

Install Code with CRC, buffer size of 18 bytes (16 bytes install code + 2 bytes CRC)


The documentation for this struct was generated from the following file: