Z-Stack API Reference  7.40.00.20
_zstack_bdbgetattributesrsp_t Struct Reference

#include <zstack.h>

Data Fields

uint32_t bdbSecondaryChannelSet
 
uint32_t bdbPrimaryChannelSet
 
uint16_t bdbCommissioningGroupID
 
uint8_t bdbCommissioningStatus
 
uint8_t bdbCommissioningMode
 
uint8_t bdbNodeCommissioningCapability
 
uint8_t bdbScanDuration
 
bool bdbNodeIsOnANetwork
 

Detailed Description

Structure to send a BDB Get Attribute Request. This is used to retrieve the attributes currently set for bdb commissioning procedures.

Field Documentation

§ bdbCommissioningGroupID

uint16_t bdbCommissioningGroupID

Group ID for Finding and Binding

§ bdbCommissioningMode

uint8_t bdbCommissioningMode

Current commissioning methods in progress (read only)

§ bdbCommissioningStatus

uint8_t bdbCommissioningStatus

Commissioning status from last call.

§ bdbNodeCommissioningCapability

uint8_t bdbNodeCommissioningCapability

Commissioning capabilities (read only)

§ bdbNodeIsOnANetwork

bool bdbNodeIsOnANetwork

Is the device commissioned to a network (read only)

§ bdbPrimaryChannelSet

uint32_t bdbPrimaryChannelSet

Primary Channel Set

§ bdbScanDuration

uint8_t bdbScanDuration

Scan Duration

§ bdbSecondaryChannelSet

uint32_t bdbSecondaryChannelSet

Secondary Channel Set


The documentation for this struct was generated from the following file: