Z-Stack API Reference  7.40.00.20
_zstack_devnwkcheckroutereq_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t dstAddr
 Network address to check if a route exists.
 
bool mtoRoute
 True if you're check for a Many-to-one route.
 

Detailed Description

Structure to send a Device Network Check Route Request.


The documentation for this struct was generated from the following file: