![]() |
![]() |
|
Z-Stack API Reference
7.40.00.20
|
#include <zstack.h>
Data Fields | |
| uint16_t | dstAddr |
| bool | mtoRoute |
| bool | mtoNoCache |
| bool | multicast |
| uint8_t | radius |
Structure to send a Device Network Route Request.
| uint16_t dstAddr |
Network address to discover
| bool mtoNoCache |
True if the concentrator has limited cache (only set if mtoRoute is set)
| bool mtoRoute |
True if you are announcing a concentrator
| bool multicast |
True if the route requested is for a multicast address
| uint8_t radius |
Radius of the message