Z-Stack API Reference  7.40.00.20
_zstack_gpaddrconflict_t Struct Reference

Data Fields

uint16_t nwkAddr
 
uint8_t extAddr [Z_EXTADDR_LEN]
 
bool conflictResolution
 

Field Documentation

§ conflictResolution

bool conflictResolution

Conflict resolution flag

§ extAddr

uint8_t extAddr[Z_EXTADDR_LEN]

Device IEEE address

§ nwkAddr

uint16_t nwkAddr

Nwk address with conclict


The documentation for this struct was generated from the following file: