Z-Stack API Reference  7.40.00.20
_zstack_gpencryptdecryptcommissioningkeyrsp_t Struct Reference

#include <zstack.h>

Data Fields

uint8_t key [SEC_KEY_LEN]
 
uint32_t keyMic
 
uint32_t secFrameCounter
 
uint8_t status
 

Detailed Description

Structure hold the CCM star GPD key result.

Field Documentation

§ key

uint8_t key[SEC_KEY_LEN]

Security Key

§ keyMic

uint32_t keyMic

MIC for the encrypted key

§ secFrameCounter

uint32_t secFrameCounter

Current Security Frame Counter

§ status

uint8_t status

status of CCM star operation


The documentation for this struct was generated from the following file: