![]() |
![]() |
|
Z-Stack API Reference
7.40.00.20
|
#include <zstack.h>
Data Fields | |
| uint16_t | dstAddr |
| uint16_t | nextHop |
| zstack_RouteStatus | status |
| bool | memoryConstrained |
| bool | manyToOne |
| bool | routeRecordRequired |
Structure to hold the information for a single route.
| uint16_t dstAddr |
Destination short address
| bool manyToOne |
A flag indicating that the destination is a concentrator
| bool memoryConstrained |
A flag indicating whether the device is a memory constrained concentrator
| uint16_t nextHop |
Next hop short address
| bool routeRecordRequired |
A flag indicating that a route record command frame should be sent before data
| zstack_RouteStatus status |
Route status