Z-Stack API Reference  7.40.00.20
_zstack_secmgrsetuppartnerreq_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t partNwkAddr
 Partner's Short Address.
 
uint8_t * partExtAddr
 Partner's Extended IEEE Address.
 

Detailed Description

Structure to send a Security Mgr Setup Partner Request.


The documentation for this struct was generated from the following file: