![]() |
![]() |
|
Z-Stack API Reference
7.40.00.20
|
#include <zstack.h>
Data Fields | |
| uint8_t | endpoint |
| uint16_t | profileID |
| uint16_t | deviceID |
| uint8_t | deviceVer |
| uint8_t | n_inputClusters |
| uint16_t * | pInputClusters |
| uint8_t | n_outputClusters |
| uint16_t * | pOutputClusters |
Structure for the Simple Descriptor. Each endpoint must have a Zigbee Simple Descriptor. This descriptor describes the endpoint to the rest of the Zigbee network. Another device can query an endpoint for it simple descriptor and know what kind of device it is. This structure is defined by the application.
| uint16_t deviceID |
This field identifies the Device ID supported on this endpoint. The IDs shall be obtained from the ZigBee Alliance.
| uint8_t deviceVer |
Identifies the version of the relevant Device Description that this device implements on this endpoint. 0x00 is Version 1.0.
| uint8_t endpoint |
The endpoint number 1-240 (0 is reserved). This is the subaddress of the node, and is used to receive data.
| uint8_t n_inputClusters |
This indicates the number of input clusters supported by this endpoint.
| uint8_t n_outputClusters |
This indicates the number of output clusters supported by this endpoint.
| uint16_t* pInputClusters |
Pointer to inputClusters array
| uint16_t* pOutputClusters |
Pointer to outputClusters array
| uint16_t profileID |
This field identifies the Profile ID supported on this endpoint. The IDs shall be obtained from the ZigBee Alliance.