Z-Stack API Reference  7.40.00.20
_zstack_sysresetreq_t Struct Reference

#include <zstack.h>

Data Fields

zstack_ResetTypes type
 
bool newNwkState
 

Detailed Description

Structure to send a system reset request.

Field Documentation

§ newNwkState

bool newNwkState

Set this flag to true to disregard the values stored in non-volatile and restart fresh.

§ type

if the stack doesn't support a type of reset, the type will be ignored and a reset will be performed.


The documentation for this struct was generated from the following file: