Z-Stack API Reference  7.40.00.20
_zstack_sysversionrsp_t Struct Reference

#include <zstack.h>

Data Fields

uint8_t transportRev
 
zstack_BuildTypes product
 Product information - build types.
 
uint8_t majorRel
 Major release number.
 
uint8_t minorRel
 Minor release number.
 
uint8_t maintRel
 Maintenance revision number.
 

Detailed Description

Structure to return the system version response.

Field Documentation

§ transportRev

uint8_t transportRev

Transport protocol revision, this is set to a value of 2


The documentation for this struct was generated from the following file: