Z-Stack API Reference  7.40.00.20
_zstack_zdobeaconnotifyind_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t sourceAddr
 Source address.
 
uint16_t panID
 PAN ID.
 
uint8_t logicalChannel
 Logical channel.
 
bool permitJoining
 Set if joining allowed.
 
bool routerCapacity
 Set if there is router capacity available.
 
bool deviceCapacity
 Set if there is device capacity available.
 
uint8_t protocolVersion
 Protocol version.
 
uint8_t stackProfile
 Stack profile.
 
uint8_t lqi
 LQI.
 
uint8_t depth
 Network depth.
 
uint8_t updateID
 Update ID.
 
zstack_LongAddr_t extendedPANID
 64 bit extended PAN ID
 

Detailed Description

Structure to send a ZDO Beacon Notify Indication.


The documentation for this struct was generated from the following file: