Z-Stack API Reference  7.40.00.20
_zstack_zdoleavecnf_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t dstAddr
 
zstack_LongAddr_t extendedAddr
 
bool removeChildren
 
bool rejoin
 

Detailed Description

Structure to send a ZDO Leave Confirm Indication.

Field Documentation

§ dstAddr

uint16_t dstAddr

Destination address

§ extendedAddr

zstack_LongAddr_t extendedAddr

64 extended address

§ rejoin

bool rejoin

Set if a rejoin is expected, Cleared if not to rejoin network

§ removeChildren

bool removeChildren

Set if remove children option set


The documentation for this struct was generated from the following file: