![]() |
![]() |
|
Z-Stack API Reference
7.40.00.20
|
#include <zstack.h>
Data Fields | |
| uint16_t | dstAddr |
| uint16_t | nwkAddrOfInterest |
| uint16_t | profileID |
| uint8_t | n_inputClusters |
| uint16_t * | pInputClusters |
| uint8_t | n_outputClusters |
| uint16_t * | pOutputClusters |
Structure to send a ZDO Match Descriptor Request.
| uint16_t dstAddr |
Destination address
| uint8_t n_inputClusters |
Number of input clusters
| uint8_t n_outputClusters |
Number of output clusters
| uint16_t nwkAddrOfInterest |
The network address of the destination device being queried.
| uint16_t* pInputClusters |
Pointer to array of input clusters
| uint16_t* pOutputClusters |
Pointer to array of output clusters
| uint16_t profileID |
The profile ID of the device