Z-Stack API Reference  7.40.00.20
_zstack_zdomatchdescrspind_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t srcAddr
 Source address.
 
zstack_ZdpStatus status
 Response status.
 
uint16_t nwkAddrOfInterest
 Nwk address of this this descriptor.
 
uint8_t n_matchList
 Number of matching endpoints.
 
uint8_t * pMatchList
 Array of matching endpoints (uint8_t)
 

Detailed Description

Structure to send a ZDO Match Descriptor Response Indication.


The documentation for this struct was generated from the following file: