![]() |
![]() |
|
Z-Stack API Reference
7.40.00.20
|
#include <zstack.h>
Data Fields | |
| uint16_t | dstAddr |
| uint16_t | nwkAddrOfInterest |
| uint8_t | n_userDescriptor |
| uint8_t * | pUserDescriptor |
Structure to send a ZDO User Decriptor Set Request.
| uint16_t dstAddr |
Destination address
| uint8_t n_userDescriptor |
Length of of the User Descriptor (16 max)
| uint16_t nwkAddrOfInterest |
The network address of the destination device being queried.
| uint8_t* pUserDescriptor |
Pointer to the descriptor