Z-Stack API Reference  7.40.00.20
_zstackmsg_HDR_t Struct Reference

#include <zstackmsg.h>

Data Fields

uint8_t event
 
uint8_t status
 

Detailed Description

Event message header. This is to support ICALL_CMD_EVENT

Field Documentation

§ event

uint8_t event

event

§ status

uint8_t status

Will hold the default response status field.


The documentation for this struct was generated from the following file: