Z-Stack API Reference  7.40.00.20
_zstackmsg_bdbaddinstallcode_t Struct Reference

#include <zstackmsg.h>

Data Fields

zstackmsg_HDR_t hdr
 
zstack_bdbAddInstallCodeReq_tpReq
 

Detailed Description

Send this message to the ZStack Thread to add an install code in the coordinator. This install code will be used with the device indicated by the IEEE address during joining. The command ID for this message is zstackmsg_CmdIDs_BDB_ADD_INSTALL_CODE_REQ.

Field Documentation

§ hdr

message header
event field must be set to zstack_CmdIDs

§ pReq

Message command fields


The documentation for this struct was generated from the following file: