Z-Stack API Reference  7.40.00.20
_zstackmsg_bdbcbketclinkkeyexchangeattempt_t Struct Reference

#include <zstackmsg.h>

Data Fields

zstackmsg_HDR_t hdr
 
zstack_bdbCBKETCLinkKeyExchangeAttemptReq_tpReq
 

Detailed Description

Send this message to the ZStack Thread to report the stack if the default Trust Center Link Key exchange has to be done (report fail on this) or it has been done by application means (report Success on this). The command ID for this message is zstackmsg_CmdIDs_BDB_CBKE_TC_LINK_KEY_EXCHANGE_ATTEMPT_REQ.

Field Documentation

§ hdr

message header
event field must be set to zstack_CmdIDs

§ pReq

Message command fields


The documentation for this struct was generated from the following file: