Z-Stack API Reference  7.40.00.20
_zstackmsg_bdbfilternwkdesccomplete_t Struct Reference

#include <zstackmsg.h>

Data Fields

zstackmsg_HDR_t hdr
 

Detailed Description

Send this message to the ZStack Thread to indicate the stack that all networks that remains in the list of networks found can be attempted. This must be call even if there are no network descriptors in the list to allow the stack finish Steering process. The command ID for this message is zstackmsg_CmdIDs_BDB_FILTER_NWK_DESC_COMPLETE_REQ.

Field Documentation

§ hdr

message header
event field must be set to zstack_CmdIDs


The documentation for this struct was generated from the following file: