Z-Stack API Reference  7.40.00.20
_zstackmsg_bdbrecovernwk_t Struct Reference

#include <zstackmsg.h>

Data Fields

zstackmsg_HDR_t hdr
 
void * pReq
 
zstack_bdbRecoverNwkRsp_tpRsp
 

Detailed Description

Send this message to the ZStack Thread to trigger the rejoin mechanism for End Devices that has lost its parent. The command ID for this message is zstackmsg_CmdIDs_BDB_RECOVER_NWK_REQ.

Field Documentation

§ hdr

message header
event field must be set to zstack_CmdIDs


The documentation for this struct was generated from the following file: