Z-Stack API Reference  7.40.00.20
_zstackmsg_bdbresetlocalaction_t Struct Reference

#include <zstackmsg.h>

Data Fields

zstackmsg_HDR_t hdr
 
void * pReq
 

Detailed Description

Send this message to the ZStack Thread to request the stack to perform a factory new reset. This will erase all Zigbee network parameters but WILL NOT ERASE Application data, that is up to the application. The command ID for this message is zstackmsg_CmdIDs_BDB_RESET_LOCAL_ACTION_REQ.

Field Documentation

§ hdr

message header
event field must be set to zstack_CmdIDs


The documentation for this struct was generated from the following file: