Z-Stack API Reference  7.40.00.20
_zstackmsg_bdbsetepdesclisttoactiveendpoint_t Struct Reference

#include <zstackmsg.h>

Data Fields

zstackmsg_HDR_t hdr
 
void * pReq
 
zstack_bdbSetEpDescListToActiveEndpointRsp_tpRsp
 

Detailed Description

Send this message to the ZStack Thread to Set the endpoint list to the active endpoint selected by the application for F&B process The command ID for this message is zstackmsg_CmdIDs_BDB_SET_EP_DESC_LIST_ACTIVE_EP.

Field Documentation

§ hdr

message header
event field must be set to zstack_CmdIDs

§ pRsp

Message command fields


The documentation for this struct was generated from the following file: