Z-Stack API Reference  7.40.00.20
_zstackmsg_bdbtouchlinktargetenableind_t Struct Reference

#include <zstackmsg.h>

Data Fields

zstackmsg_HDR_t hdr
 
uint8_t Enable
 

Detailed Description

Message send from the ZStack Thread to notify a change in the state of TouchLink as target (enabled or disabled) The command ID for this message is zstackmsg_CmdIDs_BDB_TOUCHLINK_TARGET_ENABLE_IND.

Field Documentation

§ Enable

uint8_t Enable

Message command fields

§ hdr

message header
event field must be set to zstack_CmdIDs


The documentation for this struct was generated from the following file: