Z-Stack API Reference  7.40.00.20
zstack_gpcommissioningsuccess_t Struct Reference

#include <zstack.h>

Data Fields

uint16_t index
 
uint16_t alias
 
gpdID_t gpdID
 

Detailed Description

Structure hold the gp commissioning success.

Field Documentation

§ alias

uint16_t alias

GPD alias nwk address

§ gpdID

gpdID_t gpdID

Green power device ID parameters

§ index

uint16_t index

Sink Table Index


The documentation for this struct was generated from the following file: